Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Having trouble making library parts from others
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 189 subscribers
  • Views 715 views
  • Users 0 members are here
Related

Having trouble making library parts from others

rickford66
rickford66 over 14 years ago

Hi,

I'm trying to understand how to make a library part from another library part.  I can do it 1 piece at a time, but there should be a way to do it with the whole device, as shown on page 268-9 of the Eagle Version 6 manual.  I use the command line COPY 'AD712@C:\Program Files\EAGLE-6.1.0\lbr\analog-devices.lbr' AD8572NEW, but I get an error saying that it cannot find the part or library.  that is, "cannot find 'AD712@C:\Program Files\EAGLE-6.1.0\lbr\analog-devices.lbr'.  There must be a good way to do this.  I thought the manual was clear, until it didn't work.  Youtube has some videos on this but I wonder if they are from earlier versions of Eagle.  Ideally, I'd like to copy the entire device, including package variants if possible.  Any ideas on what I may be doing wrong?

Thanks.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 1/25/2012 4:50 PM, Mike Fields wrote:

    Not sure in 6, but in 5.12, you don't even need to go through the copy menu

    - you can simply open the destination library (and have at least part of it

    visible on the screen), then expand the library tree to find the one you

    want, left click and drag it to the open destination library.  Seems to

    work fine for me (I forget where I found a tutorial on that method).

     

    mikey

     

     

    Hi Mike,

     

    That works, too but I just find it easier to explain with the context

    menu. I've had users get confused when I mention drag and drop.

     

    It's in the manual near the end of Chp 8.

     

    Best Regards,

     

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Not sure in 6, but in 5.12, you don't even need to go through the copy menu

    - you can simply open the destination library (and have at least part of it

    visible on the screen), then expand the library tree to find the one you

    want, left click and drag it to the open destination library.  Seems to

    work fine for me (I forget where I found a tutorial on that method).

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rickford66
    rickford66 over 14 years ago in reply to rickford66

    Nevermind, found it.  Duh.  haha

    Thanks all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    I had the same problem, don't use the path name for the library, and the part name is case sensitive

    do COPY AD712@analog-devices

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rickford66
    rickford66 over 14 years ago in reply to e14 Contributor

    That worked perfectly.  Now how do I rename it in the new library?

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    rickford66 wrote:

    Hi,

    I'm trying to understand how to make a library part from another

    library part. I can do it 1 piece at a time, but there should be a

    way to do it with the whole device, as shown on page 268-9 of the

    Eagle Version 6 manual. I use the command line COPY 'AD712@C:\Program

    (mailto:'AD712@C:\Program) Files\EAGLE-6.1.0\lbr\analog-devices.lbr'

    AD8572NEW, but I get an error saying that it cannot find the part or

    library. that is, "cannot find 'AD712@C:\Program

    (mailto:'AD712@C:\Program) Files\EAGLE-6.1.0\lbr\analog-devices.lbr'.

    There must be a good way to do this. I thought the manual was clear,

    until it didn't work. Youtube has some videos on this but I wonder if

    they are from earlier versions of Eagle. Ideally, I'd like to copy

    the entire device, including package variants if possible. Any ideas

    on what I may be doing wrong? Thanks.

     

    Cannot comment on v6 as I have discontinued using it. I recommend new users

    revert to v5.12  as many issues exist with v6 and you may have run into yet

    another.

    The following is the easy way to do what you want,.Try it in your version.

     

    Open your target library.

    Go into the control panel,  locate the device you wish to copy and

    right-click

    Context dialog opens, select "Copy to Library" .

     

    The device and all its variants are now in your new library

     

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 1/25/2012 1:47 PM, rickford66 wrote:

    Hi,

    I'm trying to understand how to make a library part from another library part.  I can do it 1 piece at a time, but there should be a way to do it with the whole device, as shown on page 268-9 of the Eagle Version 6 manual.  I use the command line COPY 'AD712@C:\Program (mailto:'AD712@C:\Program) Files\EAGLE-6.1.0\lbr\analog-devices.lbr' AD8572NEW, but I get an error saying that it cannot find the part or library.  that is, "cannot find 'AD712@C:\Program (mailto:'AD712@C:\Program) Files\EAGLE-6.1.0\lbr\analog-devices.lbr'.  There must be a good way to do this.  I thought the manual was clear, until it didn't work.  Youtube has some videos on this but I wonder if they are from earlier versions of Eagle.  Ideally, I'd like to copy the entire device, including package variants if possible.  Any ideas on what I may be doing wrong?

    Thanks.

     

     

    Hi Rick,

     

    There's several ways to copy components from one library to another.

    Here's the one I find the simplest.

     

    1. Open the destination library(the one you're going to copy into). The

    library editor should open.

    2. Go to the EAGLE control panel,expand the libraries tree and find the

    device or package you would like to copy.

    3. Right-click on said device or package and select copy to Library. The

    part will now be in your personal library.

     

    When you copy a device, all packages associated with it as well as the

    symbol get copied to your library. When you copy a package, that's all

    that gets copied the package.

     

    Let me know if there's anything else I can do for you.

     

    hth,

    Jorge Garcia