Hi,
I'm a new Eagle user, but I suspect this is actually a more complicated question.
I have traces that will carry up to 2 amps. Those traces also control various FETs and other signals. If I set that net node to the trace width for the high current, all of the net gets set to that width and I don't have room to route my board. I've already re-arranged all my components so that the wide traces are short and the pins near each other. I've even gone from 4 layers to 6 layers. (The board routes just fine with 4 layers by 7 mil traces.)
I don't see a way to set the width of signals before routing, and after routing is too late. One idea is to isolate the low current part of the net from the high current with a 0 ohm resistor, then after routing fill in will a trace. But even that seems a little clumsy.
I'm considering going to thicker copper layers so that I can reduce the trace width, but I haven't tried that yet.
Does anyone have any ideas on how I might solve this problem?
Thanks,
Dave