Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21292 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • anishkgt
    0 anishkgt over 10 years ago

    So if i understand correct, the triac, when used with an inductive load such as the MOT does not switch off the load at the zero cross but after 10ms on 240VAC 50Hz.

     

    I was reading about commutaion TRAIC and came across this high commutation TRIAC, would this be ok with.

     

    http://www.mouser.com/ds/2/302/BTA216_SERIES_B-353015.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 12/09/16 14:00, George Thomas wrote:

    So if i understand correct, the triac, when used with an inductive load such as the MOT does not switch off the load at the zero cross but after 10ms on 240VAC 50Hz.

     

    Not quite. The triac turns off at the zero crossing of the current, not

    the voltage. With a resistive load, these occur at the same time. With

    an inductive load, the current lags behind by (up to) one quarter cycle,

    or 5ms on UK (50Hz) mains (~4ms in US).

     

    However, when the triac attempts to turn off this late in the cycle, the

    voltage is at its peak, and the act of turning off causes the voltage

    across the triac to rise extremely rapidly. This high dV/dt can cause

    false triggering of the triac, meaning it fails to turn off at all. At

    minimum, this results in one extra half cycle of conduction. But at the

    end of that half cycle the conditions for a commutation failure are

    repeated, with the risk that it fails to turn off again... and again...

    and again...

     

    I was reading about commutaion TRAIC and came across this high commutation TRIAC, would this be ok with.

     

    http://www.mouser.com/ds/2/302/BTA216_SERIES_B-353015.pdf

     

    I'm sure Rachael would object to the 0.1" pin spacing. I'd certainly

    prefer the wider spacing of a TO3-P too. However, the datasheet does

    give figures that look OK in terms of ratings.

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to autodeskguest

    CadSoft Guest wrote:

    I was reading about commutaion TRAIC and came across this high commutation TRIAC, would this be ok with.

     

    http://www.mouser.com/ds/2/302/BTA216_SERIES_B-353015.pdf

     

    I'm sure Rachael would object to the 0.1" pin spacing. I'd certainly prefer the wider spacing of a TO3-P too. However, the datasheet does give figures that look OK in terms of ratings.

     

     

     

    Yes its figures do look fine in terms of ratings for the normal operation of the design but you are right, I wouldn't be overly happy with the 0.1" pin spacing if this were my design. The need for increased spacing is for improved creepage/clearance. Now, given this is for a spot welder, I assume this may be used in a potentially dusty / damp environment such as a shed or garage, and the environment can play a big part in whether this carries on working reliably even under normal voltage conditions let alone abnormal conditions like voltage surges. In general if the environment is dusty / damp then the required creepage and clearance values are much larger than for equipment used in a nice clean and dry environment.

     

    See this link for a reasonable overview of things that should be considered for high voltage designs: http://www.infineon.com/dgdl/Infineon+-+Application+Note+-+PowerMOSFETs+-+CoolMOS%E2%84%A2+-+Electrical+Safety+and+Isolation+in+high+voltage+Applications.pdf?fileId=db3a30433d1d0bbe013d20e0cbf017fe

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rachaelp
    0 rachaelp over 10 years ago in reply to autodeskguest

    CadSoft Guest wrote:

    I was reading about commutaion TRAIC and came across this high commutation TRIAC, would this be ok with.

     

    http://www.mouser.com/ds/2/302/BTA216_SERIES_B-353015.pdf

     

    I'm sure Rachael would object to the 0.1" pin spacing. I'd certainly prefer the wider spacing of a TO3-P too. However, the datasheet does give figures that look OK in terms of ratings.

     

     

     

    Yes its figures do look fine in terms of ratings for the normal operation of the design but you are right, I wouldn't be overly happy with the 0.1" pin spacing if this were my design. The need for increased spacing is for improved creepage/clearance. Now, given this is for a spot welder, I assume this may be used in a potentially dusty / damp environment such as a shed or garage, and the environment can play a big part in whether this carries on working reliably even under normal voltage conditions let alone abnormal conditions like voltage surges. In general if the environment is dusty / damp then the required creepage and clearance values are much larger than for equipment used in a nice clean and dry environment.

     

    See this link for a reasonable overview of things that should be considered for high voltage designs: http://www.infineon.com/dgdl/Infineon+-+Application+Note+-+PowerMOSFETs+-+CoolMOS%E2%84%A2+-+Electrical+Safety+and+Isolation+in+high+voltage+Applications.pdf?fileId=db3a30433d1d0bbe013d20e0cbf017fe

     

    Best Regards,

     

    Rachael