Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle Dimension and Clearance
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 189 subscribers
  • Views 1829 views
  • Users 0 members are here
  • eagle
  • and
  • error
  • clearance
  • dimension
Related

Eagle Dimension and Clearance

e14 Contributor
e14 Contributor over 13 years ago

I ran a test and I hot two errors, 'Dimension' and 'Clearance'. Not too sure what the problem is with the clearance one as its showing on near enough every via ive made ontop of traces to allow for my capcitors

 

Clearance pic

http://tinypic.com/r/2u4hlia/4

 

 

Dimension pic

http://tinypic.com/r/nd4iz5/4

 

The dimension pic I understand it is close to the edge. (1mm) I guess this is abit to close, what kind of distance should I be keeping away from the board?

 

 

 

I uploaded my .brd file for people to have a look at! and maybe look for other errors (which I think/hope there isnt any!!!!) haha

 

Thanks for your time image

Attachments:
Half omni copy.brd.zip
  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    But then I need to add a capcitor between pinheader 1 & 2 on the traces. I was under the understanding that this wouldnt be done in the shematic and its to do with the traces on the board which you need to lay down first before being able to place a via ontop.

     

    Hi Matt,

     

    All components (i.e. the capacitor in this case) are placed on the schematic. It's a logical representation, like a metro/tube map. While working on the

    schematic, keep the board view open, but don't do anything with it.

     

    Once you are satisfied it is correct, then work on the board which is the physical view. You can drag the capacitor close to the pin header on the board view.

    All this is explained in the EAGLE manual (chapter 6,"From Schematic to Finished Board").

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to autodeskguest

    Thanks Rob, I understand its a error on eagle but would it acctaully result in a phical error once the board is prinited?

     

    My componets and pads are all fine on the shematic but im not sure if I should add via's on the shematic? Could you take this example and explain how you would go about adding a via;

     

    All analog potemeters traced to a pin header on the shematic. But then I need to add a capcitor between pinheader 1 & 2 on the traces. I was under the understanding that this wouldnt be done in the shematic and its to do with the traces on the board which you need to lay down first before being able to place a via ontop.

     

    Thanks again

     

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to e14 Contributor

    On 28/04/13 15:39, Matt Porta wrote:

    @ Paul. So this error is only acutally to do with the net/names

    whatever. Not acually to do with a physical error on the baord which

    will affect when getting made?

     

    It's to do with you abusing Eagle in a way you shouldn't. You said the

    error is "on near enough every via ive made ontop of traces to allow for

    my capcitors", but that wording tells me you've omitted those VITAL

    COMPONENTS from the schematic! If you'd designed the schematic right you

    wouldn't be adding vias - there would be the correct components,

    complete with pads, correctly connected to the right nets, ALREADY THERE

    and without any such errors.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to autodeskguest

    @ Paul. So this error is only acutally to do with the net/names whatever. Not acually to do with a physical error on the baord which will affect when getting made?

     

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago

    On 04/25/2013 03:44 PM, Matt Porta wrote:

    The dimension pic I understand it is close to the edge. (1mm) I guess

    this is abit to close, what kind of distance should I be keeping away

    from the board?

     

    The distance you must keep copper from the edge of the board depends on

    who is fabricating the board. For example, PCB-Pool wants a minimum of

    0.3mm (12mil). AP Circuits wants 0.38mm (15mil). Sunstone Circuits wants

    0.5mm (20mil). If you can, allow more room, as this reduces the failure

    rate. 1mm seems safe, but always consult with the board house before

    committing to a layout -- many post their capabilities on their websites.

     

    -Reece

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bmoe
    0 bmoe over 13 years ago

    Hi.

     

    Regarding the distance from the board edge to copper I have used as little as 0.1mm and have seen no problem.

    This can be set in menu Tools - DRC, and in the Distance tab change the Copper/Dimension value.

     

    /Matias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago

    On 04/25/2013 03:44 PM, Matt Porta wrote:

    I ran a test and I hot two errors, 'Dimension' and 'Clearance'. Not too

    sure what the problem is with the clearance one as its showing on near

    enough every via ive made ontop of traces to allow for my capcitors

    A guess is you just added a via and did not connect it to the net.

     

    If you need a test point or test pad add it to the sch.

    The fix is to name the via the net name you want it to connect to.

    Paul R.