element14 Community
element14 Community
    Register Log In
  • Site
  • Search
  • Log In Register
  • Community Hub
    Community Hub
    • What's New on element14
    • Feedback and Support
    • Benefits of Membership
    • Personal Blogs
    • Members Area
    • Achievement Levels
  • Learn
    Learn
    • Ask an Expert
    • eBooks
    • element14 presents
    • Learning Center
    • Tech Spotlight
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
    • element14 presents Projects
    • Project14
    • Arduino Projects
    • Raspberry Pi Projects
    • Project Groups
  • Products
    Products
    • Arduino
    • Avnet Boards Community
    • Dev Tools
    • Manufacturers
    • Multicomp Pro
    • Product Groups
    • Raspberry Pi
    • RoadTests & Reviews
  • Store
    Store
    • Visit Your Store
    • Choose another store...
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
  • Settings
Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Making a device, packages are not selectable
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 172 subscribers
  • Views 765 views
  • Users 0 members are here
Related

Making a device, packages are not selectable

Former Member
Former Member over 11 years ago

I am trying to create a new library part. In the final steps of the process, combining the symbol with the package, I am unable to select the package from the list. Its on the list, but is a lighter gray color and not selectable.

 

Can any instructors offer a suggestion on getting over this hurdle?

 

I have noticed this in other library's I didn't create, also

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 5/5/2014 3:18 PM, Daniel Bowler wrote:

    I am trying to create a new library part. In the final steps of the

    process, combining the symbol with the package, I am unable to select

    the package from the list. Its on the list, but is a lighter gray color

    and not selectable.

     

     

    Hi Daniel,

     

    This implies that there are more pins in the symbol than pads in the

    package. Double check your symbol and make sure that you don't

    accidentally have two pins on top of each other.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 05/05/14 20:18, Daniel Bowler wrote:

    I am trying to create a new library part. In the final steps of the

    process, combining the symbol with the package, I am unable to select

    the package from the list. Its on the list, but is a lighter gray color

    and not selectable.

     

    Can any instructors offer a suggestion on getting over this hurdle?

     

    Well, I'm certainly not an "instructor" but as this is a public NNTP

    group...

     

    The greying out (which was added at V5, I think) indicates that the

    package is unsuitable for use on your device, most likely because it

    does not have enough pads for the number of pins on the symbols in the

    device. You need to check that you've got enough pads on your package,

    that your symbol doesn't have stray pins and that your device doesn't

    contain any stray extra symbols.

     

    HTH,

    Rob

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Thanks guys,

     

    That was it.

     

    Now what happen when you have something like a voltage regulator that comes in different packages that have less pin or features? Do you have to create a separate symbols for this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    On 05/05/14 21:36, Daniel Bowler wrote:

    Now what happen when you have something like a voltage regulator that

    comes in different packages that have less pin or features? Do you have

    to create a separate symbols for this?

     

    Traditionally yes, you would. I think something was done on V6 but as

    I'm still (mostly) using V4 I'm accustomed to different devices for the

    78xx in SO-8 vs. TO92

     

    It was never an issue for devices where the TSSOP-20 merely had two

    extra N/C pins compared to the SO-18 but where it had a doubled-up

    ground pin they would have to be separate devices. The symbol would also

    have to be different unless the extra pins are "implied" or "hidden"

    such as supply pins, and the device could include them as "on-demand"

    symbols.

     

    Again, this is for V5 and earlier, it may not be true of V6. However, if

    you're talking "less feature" then it's a change of visible pins on the

    schematic too, so that would still be a different device.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 11 years ago in reply to Former Member

    On 05/05/2014 04:36 PM, Daniel Bowler wrote:

    Thanks guys,

     

    That was it.

     

    Now what happen when you have something like a voltage regulator that

    comes in different packages that have less pin or features? Do you have

    to create a separate symbols for this?

     

    If the symbol is exactly the same, you can use multiple packages.  In

    such cases, the extra pins may have a common internal connection.  An

    example of this is where you have a FET in an 8-pin package.  Three of

    the pins may be connected to the source, one for the gate, and four for

    the drain.  In other cases, the extra pins are left unconnected.  The

    datasheet will tell.

     

    In v6, it is possible to connect multiple pads (on the package) to a

    single pin (on the symbol).  The connections can be ANY or ALL.  In the

    case of ANY, the the connecting net can be routed to any of the pins for

    that signal.  In the case of ALL, the connecting net must be routed to

    all of the pins for that signal.

     

    If the regulator has an extra feature, such as an enable pin, you will

    have to create a different symbol to accommodate this and connect pins

    and pads appropriately.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.