EAGLE User Support (English) Straition lines printing in filled areas
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
  • State Not Answered
  • Replies 22 replies
  • Subscribers 183 subscribers
  • Views 3574 views
  • Users 0 members are here
  • lines
  • fill
Related

Straition lines printing in filled areas

Former Member
Former Member over 10 years ago

OS= Win 8.1

Eagle = 7.2

 

I have a direct to board print setup. That is, I print directly on the copper clad, straight out of Eagle. I have noticed that the fill lines are showing. I have found where others have had this issue, but I have not understood what to do to resolve the problem. This problem also occurs when I print the PCB to pdf format. I have read that it has to do with Eagle using lines to cover the filled area and that changing the line width and the fill style might be helpful. But, then, there are no instructions on how to do these operations and no feedback as to whether it worked, or not. Would someone please be so kind as to tell me the definitive cure and the steps to complete the task? I would be very grateful. Eagle files and libraries are attached. The problem is very clear in the pdf format. Thank you very much for your help.

Attachments:
Oscilloscope.zip
  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +1
    Maybe you need to do a Polygon command setting the color. See PCB Creation with Eagle for Beginners : The Ground Plane There is more about polygon HOW-TO: Polygons and ground fills for PCBs in Eagle |…
  • balearicdynamics
    balearicdynamics over 10 years ago +1
    t1d I have downloaded the attached zip file and opened it on eagle checking for the schematics you included in PDF. The point is that the pdf is different than the schematics you attached, as in the image…
  • Bertl
    Bertl over 10 years ago in reply to balearicdynamics +1
    If you press the button "Ratsnest" (first one in the last button section, the one with the connected nodes), you will see that the area enclosed by the dashed line will fill up (flood) the free space around…
Parents
  • Former Member
    0 Former Member over 10 years ago

    I have not discovered the definitive answer, so I am bumping up the queue, to keep the thread fresh.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 28/05/2015 9:34 a.m., Tee Dunn wrote:

    I have not discovered the definitive answer, so I am bumping up the

    queue, to keep the thread fresh.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/150912

     

     

     

    In the print dialog, when you select 'black', you should also select

    'solid'. If you fail to do that and your layer setup does not have a

    solid fillstyle then you can get the light and dark stripes.

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 28.05.2015 12:05, warrenbrayshaw wrote:

    On 28/05/2015 9:34 a.m., Tee Dunn wrote:

    I have not discovered the definitive answer, so I am bumping up the

    queue, to keep the thread fresh.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/150912

     

     

    In the print dialog, when you select 'black', you should also select

    'solid'. If you fail to do that and your layer setup does not have a

    solid fillstyle then you can get the light and dark stripes.

     

     

    I suppose this only prints non solid fillstyle lines as solid? This is

    not about that.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 28.05.2015 12:05, warrenbrayshaw wrote:

    On 28/05/2015 9:34 a.m., Tee Dunn wrote:

    I have not discovered the definitive answer, so I am bumping up the

    queue, to keep the thread fresh.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/150912

     

     

    In the print dialog, when you select 'black', you should also select

    'solid'. If you fail to do that and your layer setup does not have a

    solid fillstyle then you can get the light and dark stripes.

     

     

    I suppose this only prints non solid fillstyle lines as solid? This is

    not about that.