Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) BC184L transistor component
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 189 subscribers
  • Views 5135 views
  • Users 0 members are here
Related

BC184L transistor component

Andy Betts
Andy Betts over 10 years ago

I'm taking my first baby steps into circuit design, with the intention of making guitar effect pedals that are as close to the original vintage spec as possible... Here's my issue.

 

I'm laying out the schematic for the circuit, and went to the library to pull out a BC184L transistor and there wasn't one. The closest to it I could find was a BC109, however I would really like the 184L as that's the correct one for the circuit. can I just create a new one in the library from an existing component that's virtually the same, or is there a resource for obtaining the correct library file, or am I missing something blatantly obvious as a newbie.

 

 

Thanks for your patience in advance...

 

Andy

  • Sign in to reply
  • Cancel
Parents
  • Andy Betts
    Andy Betts over 10 years ago

    Hi guys.

     

    Thank you all for your help, and comments. I've checked the schematic and that says that the 3 trannies in the circuit are BC169C, BC184C & BC109. However, I'm also working from an original photograph of the circuit and the trannies are ALL BC184L so I'll be going with that. The pin outs are the same on all those transistors I believe so i'll use the 109 from the library and rename it... Simples!! :-)

     

    For your interest, I'm recreating a Colorsound Power Boost version 2. The board will be the same, with board mounted pots, I just need to lay the circuit out in eagle and get the design as close to the trace as possible. I could manually trace the layout from the photo below, but it's a bit messy, and using Eagle to re-draw the circuit and create the board will ensure I don't make any ***-ups along the way as regards the circuit. I'm also sourcing (where practical) original components, so I've just received a delivery of NOS Mullard tropical fish caps the same as in the photo. all resistors are the same, I have however had to compromise with the axial electrolytic caps... I've gone with Vishay caps, a good brand and the same as what's used in the current power boost reissues.

     

    The photos below show a version 1 power boost, which had an extra 10k resistor which the version 2 didn't have. Apart from that they were identical.

    . imageimage

     

      imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 10 years ago in reply to Andy Betts

    Groovy! Boost that power, man!

     

    Made in London, too.

     

    What does it do to the sound? It looks like it's a just preamp and a tone control. Do the bass and treble cut as well, or is it just boost? Nice colour and love the graphics.

    [In the time I took to write this you've added the schematic and answered my question.]

     

    The BC184L has the base at one end, the BC109 in the middle. I vaguely seem to remember that there was a non-L version with a different pinout (it's the kind of thing that causes no end of confusion because it's inevitable that eventually somebody doing the buying will get offered a great deal on the wrong part).

     

    Also, the pins of the BC184 are in-line, whereas those of the BC109 were in a triangular shape. It was quite normal to bend the centre pin out to form the triangle shape when you had an in-line part. We were producing industrial equipment, so we used small plastic formers that the parts sat on and that guided and supported the legs, but this is the cheap and cheerful end of the market and you can see they've just stuffed the transistors in any old how.

     

    Do the BC184s have a letter at the end? Either BC184LB or BC184LC? The manufacturers grade transistors and offer them in a narrower range of gains than you'd get if you just had them from the end of the production line. If it has C parts, you probably want to match it - that was the higher gain bucket and they wouldn't have paid the extra if they didn't need them for the circuit operation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andy Betts
    Andy Betts over 10 years ago in reply to jc2048

    The guy that owns that particular power boost has told me that ALL the transistors are BC184L's.

     

    Also the axial caps are 22uf (The big ones), however the actual powerboost has different smaller axial caps than the schematic... the owner has listed the caps as follows:

     

    "the small blue caps are 6.4µF, the small green one is probably a 4.7µF and the large green one is a 22µF." However the schematic lists them as 220pf & 10uf......

     

    As regards the sound. it is a pre-amp, with a treble and bass boost... It's only when you get to about 3/4 on the volume knob does it start to break up into an overdrive. Used extensively by David Gilmour throughout the 70's with a fuzz box, he used the power boost and a big muff fuzz for the classic comfortably numb solo. he also used it on the Animals album and on the solos in Shine on.

     

    Any help with identifying caps and stuff would be greatly appreciated.

     

    here's more pics

     

    imageimage

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to Andy Betts

    Am 30.07.2016 um 14:31 schrieb Andy Betts:

    Do I detect an essence of sarcasm?? image

     

    I'm qualified in using AutoCAD, have been using it for years... And I have to say that designing in Eagle is "clunky" to say the least and not at all intuitive. I will design my own devices if I have to.. but if there's something already there that just needs a tweak I'll do that. why try and reinvent the wheel when somebody has already done it. As a CAD program eagle is not a good program, and designing simple things takes thought... I'm used to using absolute coordinates.. Eagle doesn't appear to use that.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/202727

     

     

    Do I detect someone comparing apples with pears?

    Eagle is a layout program autocad is not, so your argumentation is for

    the birds.

    Imho this thread is by far too long just for modifying a lousy transistor.

    And I see your qualification: This little work took you a week...

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to Andy Betts

    Andy Betts wrote on Sat, 30 July 2016 08:31

    why try and reinvent the wheel when somebody has already done it.

     

     

    In the case of ECAD library parts, that's already been answered.

     

    Quote:

    designing simple things takes thought

     

    OMG!  You mean in engineering I have to use my brain!!?  I just wanted to

    plug dis inta dat.  Now I have to add things and think and stuff?  Let me

    outta here!!

     

    Quote:

    I'm used to using absolute coordinates.. Eagle doesn't appear to use

    that.

     

     

    This shows you haven't even tried to learn, let a alone experiment with

    Eagle.  Just about everything in Eagle uses absolute coordinates.  One of

    the first things I do when designing a footprint is to pick a origin and

    determine the absolute coordinates of things to that origin.

     

    Oh, right, that requires adding things and thinking, and a even more

    advanced concept called subtraction.  Nevermind.

     

    You're right. Eagle and any kind of engineering isn't for you.  Perhaps you

    can go into politics, or practise really hard and get good as asking "Do

    you want fries with that?".

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to Andy Betts

    Andy Betts wrote on Sat, 30 July 2016 08:31

    why try and reinvent the wheel when somebody has already done it.

     

     

    In the case of ECAD library parts, that's already been answered.

     

    Quote:

    designing simple things takes thought

     

    OMG!  You mean in engineering I have to use my brain!!?  I just wanted to

    plug dis inta dat.  Now I have to add things and think and stuff?  Let me

    outta here!!

     

    Quote:

    I'm used to using absolute coordinates.. Eagle doesn't appear to use

    that.

     

     

    This shows you haven't even tried to learn, let a alone experiment with

    Eagle.  Just about everything in Eagle uses absolute coordinates.  One of

    the first things I do when designing a footprint is to pick a origin and

    determine the absolute coordinates of things to that origin.

     

    Oh, right, that requires adding things and thinking, and a even more

    advanced concept called subtraction.  Nevermind.

     

    You're right. Eagle and any kind of engineering isn't for you.  Perhaps you

    can go into politics, or practise really hard and get good as asking "Do

    you want fries with that?".

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.