Weller
  • Products & Partners
  • Manufacturers
  • Weller
  • More
  • Cancel
Weller
Forum Remove a castellated PCB with Weller WRK SMD reflow set
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Weller to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 9 subscribers
  • Views 2458 views
  • Users 0 members are here
  • weller
  • WRK
Related

Remove a castellated PCB with Weller WRK SMD reflow set

Jan Cumps
Jan Cumps over 2 years ago

Removing castellated PCBs, once soldered, can be a tricky task. It's not easy to get the solder on all castellations heated up at the same time. 

I had to replace the XIAO RP2400 board on my  Pi Pico Eurocard Development Board. Doing this with a high capacity iron, or with hot air isn't easy. By the time you get to pin 14, pin 1 has gone solid again.
You may get away with prying under the board while attacking each castellation, but chances are that you 'll tear off the pads from the motherboard.

image

One possible solution is to ply a thick copper wire in such a way that it surrounds the PCB and touches all castellations. Then, with a decent iron and a lot of flux, heat up that wire.
I decided to try removing the IC with a Weller WRK SMD reflow kit.

image

This kit has little ovens that you can put on top of something. And it has a vacuum-actioned suction cup that you can stick on top of the device that needs to be removed.

image

When you then put a hot air pencil in the little oven's opening, the inside gets hot very fast. No risk of burning the neighbour components. And very efficient heat usage.

When I tried this at 380° C, the castellated board lifted off in 20-30 seconds. Without any damage.

This is the motherboard after the action:

image

And the castellated board survived too:

image

There is a little alchemy and experience involved. In my case, the XIAO used lead-free solder, and the castellated board was placed with leaded.
That meant that the castellations melted faster than the components on the XIAO. And when the lift-off happened, the whole board came off.
It's not that easy in every case.

But you can prepare for this. In case the castellated board is placed with lead-free, You can first wick off most of that, and replace it with leaded solder (or even lower melting point specialised products). Then use the oven to remove everything.

Anyways, after this exercise, I cleaned up the motherboard and put on a new XIAO RP2040.

image

Thanks for reading.

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 2 years ago +2
    That tool is really useful. Good job desoldering. I usually do it quite badly, using the technique you indicate with the thick wire, but many times I end up ruining a track.
  • DAB
    DAB over 2 years ago +2
    Good post Jan.
  • scottiebabe
    scottiebabe over 2 years ago +2
    Bismuth solder is a miracle worker when your desperate...
Parents
  • Jan Cumps
    Jan Cumps over 1 year ago

    another year, another victim Slight smile

    image

    image

    That rework set proves to be helpful. 2nd time that I replace the XIAO debugger on this board, and all the copper pads survived. After the last repair, I used lead-free. So I had to up the temperature a little. I used 350°C.

    This time, I think  I'll place headers instead of soldering the new XIAO direct on the PCB.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 1 year ago in reply to Jan Cumps

    Did your XIAO fail?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to scottiebabe

    yes. It's used as a PicoProbe. I made a mistake when connecting both Xiao and Pico to USB, and lost a GPIO

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to scottiebabe

    Back in business. The most difficult part was to transfer shabaz ' debugger sticker without damaging it Slight smile.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to scottiebabe

    Back in business. The most difficult part was to transfer shabaz ' debugger sticker without damaging it Slight smile.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • scottiebabe
    scottiebabe over 1 year ago in reply to Jan Cumps

    great work! I don't want to jinx it, but so far I haven't had an rp2040 fail

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to scottiebabe

    In total, I have 3 victims:

    • 2 XIAOs that I killed in virtually the same fashion, while serving as PicoProbes
    • a Pico 1 lost a GPIO pin while I was playing with stepper motor drivers.

    I have to admit that I'm not careful. In particular with the XIAOs. I ordered a batch of 14, and that makes me a bit reckless.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to Jan Cumps

    I was wondering if the Xiao might not have ESD protection on the USB connector, but according to the circuit diagram it does:

    image

    Maybe due to the tiny size of it, minute flexing on the socket could cause a capacitor to crack or something : (

    There's a load of tiny resistors in a line, but there's also a capacitor (C2) which is across the 3.3V rail, so it's possible it could have shorted. It's 0201 sized which is insanely tiny of course : ( If it's possible to pull that part off (it's the second part in that row, see the yellow arrow), if it was indeed faulty then the XIAO might start working perhaps. Anyway this is all just speculation, it might be something completely different. I've never used an 0201 part, all I know is that those small parts (0402 too, which I've experienced this with) are so easy to crack, especially with hot air tools too.

    (btw I looked at a slightly older revision in EAGLE, because I happened to have downloaded the XIAO files in the past, I didn't download the most reccent ones).

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to shabaz

    The USB still works. And the rp2040 cores too. I can still program it. I lost a gpio.