Würth Elektronik
  • Products & Partners
  • Manufacturers
  • Würth Elektronik
  • More
  • Cancel
Würth Elektronik
Blog Isolated MagI³C Power Module Mastering the 24V Industry Bus II
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Würth Elektronik to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Würth Elektronik
  • Date Created: 5 Dec 2023 6:53 AM Date Created
  • Views 407 views
  • Likes 4 likes
  • Comments 0 comments
  • technical insights
  • würth elektronik
  • magi³c_power_module
Related
Recommended

Isolated MagI³C Power Module Mastering the 24V Industry Bus II

Würth Elektronik
Würth Elektronik
5 Dec 2023
Isolated MagI³C Power Module Mastering the 24V Industry Bus II

Isolated MagI³C Power Module Mastering the 24V Industry Bus

Wide Voltage Range – Input Voltage Limits

Author: Timur Uludag / Editor: Gerhard Stelzer

In the industrial environment, 24 V bus systems are widely used to supply a wide range of field devices. Part 1 explained selection criteria for power modules and typical voltage ranges. Part 2 now elaborates on the issues with input voltage limits.

Initially it is helpful to have a common understanding of the structure of an industrial application, such as which voltages are present and why.

Industrial applications are known for long connecting lines between the separated parts of the application. Due to the spatial extensions the length of these connecting lines can be in the range of tens of meters.

Figure 1 shows the basic structure of an industry plant. Nowadays, the electrical supply is realized through cabinets with switched mode power supplies or transformer power supplies. Transformer power supplies are still common for higher power supply. The separated parts of the applications are supplied through a DC bus. On site, every separated electrical load is connected via a sub distribution with 24V. It is easier to generate the 24V in a centralized cabinet and distribute the voltage through a DC bus than to distribute the hazardous 230Vac / 400Vac. This also reduces the number of separate power supplies.

Based on that structure there are three main influencing phenomena to the DC bus voltage:

  • The voltage from the electrical supply
  • Disturbances to the DC bus from running cables that are placed in parallel
  • Voltage drops due to current flow

This article series is being continued with “Minimum input voltage – lower limit”.

 image

 

Figure 1. Typical industrial set-up of power supplies.