Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Pico low jitter PID controller
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 24 Oct 2026 11:35 AM Date Created
  • Views 287 views
  • Likes 7 likes
  • Comments 7 comments
Related
Recommended
  • pico2
  • pico
  • c++26
  • pico_eurocard
  • pico c sdk
  • pid_controller
  • c++

Pico low jitter PID controller

Jan Cumps
Jan Cumps
24 Oct 2026

In my blog  Pico PID controller without floating point using DSP C++ fixed point API , I created a low footprint Pico PID example. 
In this post, I reduce jitter by making sample clock steady, and let that drive the PID loop execution.

image

I used Google AI in this blog post to help explain jitter aspects, and help to set up ADC timer and trigger code.
All narrative is written by me, except where explicitly stated.

In a PID control loop, an inconsistent sample time can introduce jitter in the regulation. By letting a clock drive the exact ADC timing, the sample cadence becomes deterministic.

This content is AI generated by Google Gemini:

image

PID loop scheduling vs ADC sample scheduling: impact on firmware

image

In the code of the previous post, a Pico timer generated an interrupt. That interrupt was the driver of executing a full PID loop:

  • sample the output
  • let PID calculate ideal PWM duty cycle, to have output match desired output
  • set the PWM

In the deterministic sample design, there is no longer a clock that makes the PID tick.
The ADC clock ticks the sample time,
ADC ready interrupt pushes the regulation

  • ADC clock initiates sample
  • ADC raises interrupt when sample done

When the interrupt happens:

  • let PID calculate ideal PWM duty cycle, to have output match desired output
  • set the PWM (see end of this post: I replaced the PWM API call by a CPU-less DMA approach).

Real time startup behaviour, set to regulate output to 50%:

image

slomo 4X:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Source Code

#include "fixed_point.hpp"

#include "hardware/adc.h"
#include "hardware/gpio.h"
#include "hardware/pwm.h"
#include "hardware/irq.h"
#include "hardware/clocks.h"

import pid;

using namespace arm_cmsis_dsp;

using fp_t = Q15;
constexpr Q15 operator""_fp(long double val) {
        return operator""_q15(val);
}

using pid_controller_t = pid::pid<fp_t>;

// ADC and PWM declarations
// Pico SDK types are used here:
const uint ADC_PIN = 26;
const uint PWM_PIN = 0;
const uint PWM_CHANNEL = 0;

// frequency of PWM will be 125 MHz (on Pico1, 150 on Pico2) / (PWM_MAX * CKDIV)
// i.e. about 30.5 kHz for PWM_MAX = 4095
const uint PWM_MAX = 4095;
const float CKDIV = 1; // set CKDIV to 1 for approx 30.5 / 36.62 kHz PWM frequency if PWM_MAX is 4095
const uint32_t pwm_frequency = clock_get_hz(clk_sys) / (PWM_MAX * CKDIV);

const uint32_t adc_frequency = pwm_frequency / 10; // 3.663 kHze PID loop rate, 1/10 of PWM frequency
const float adc_clock_div = clock_get_hz(clk_adc) / adc_frequency;

// PID variables and objects
fp_t feedback;
constinit fp_t target_command = 0.66_fp; // Example target command in fixed point per-unit (0.0 to 1.0)
constinit fp_t output_pid = 0.0_fp; // Initialize output_pid to 0.0 in fixed point per-unit
pid_controller_t controller(0.1_fp, 0.01_fp, 0.05_fp); // Example PID gains for voltage control

// GPIO pin, to measure duration of a PID loop
const uint GPIO_PIN = 22; // happens to be the Pico Eurocard LED

void __not_in_flash_func(adc_pid_handler)() {
    gpio_xor_mask(1u << GPIO_PIN); // toggle
    feedback.v = static_cast<int16_t>((adc_fifo_get()) << 3); // Direct to 0.0 - 1.0 per-unit in Q15!

    output_pid = controller.compute(target_command, feedback);

    // Convert Q15 per-unit (0.0 to 1.0 excluded) to raw timer counts (0 to 65535)
    // the level will be 0 - 4095, 12 bits
    pwm_set_chan_level(slice_num, PWM_CHANNEL, static_cast<std::uint16_t>(output_pid.v >> 3)); // set PWM value
    gpio_xor_mask(1u << GPIO_PIN); // toggle
}

void init_adc() {
    adc_init();
    adc_gpio_init(ADC_PIN);
    adc_select_input(0);

    adc_fifo_setup(true, false, 1, false, false);
    adc_fifo_setup(true, false, 1, false, false);

    irq_set_exclusive_handler(ADC_IRQ_FIFO, adc_pid_handler);
    irq_set_enabled(ADC_IRQ_FIFO, true);
    adc_irq_set_enabled(true);

    adc_set_clkdiv(adc_clock_div);
}

void init_pwm() {
    gpio_set_function(PWM_PIN, GPIO_FUNC_PWM);
    slice_num = pwm_gpio_to_slice_num(PWM_PIN);
    pwm_set_clkdiv(slice_num, CKDIV);
    pwm_set_wrap(slice_num, PWM_MAX-1);
    pwm_set_chan_level(slice_num, PWM_CHANNEL, 0);
    pwm_set_enabled(slice_num, true);
}

void init_gpio() {
    gpio_init(GPIO_PIN);
    gpio_put(GPIO_PIN, 0);
    gpio_set_dir(GPIO_PIN, true);
}

int main() {
    init_gpio();
    init_pwm();
    init_adc();

    adc_run(true);

    while (true) {
        tight_loop_contents(); 
    }    
}

CMake script

cmake_minimum_required(VERSION 3.28)

set(CMAKE_C_STANDARD 11)
set(CMAKE_CXX_STANDARD 26)
set(CMAKE_EXPORT_COMPILE_COMMANDS ON)
set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -fmodules-ts -fcommon -fno-rtti -fno-exceptions")
set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -mthumb -mfpu=fpv5-sp-d16")
set(CMAKE_CXX_STANDARD_REQUIRED ON)

message("CMAKE_BUILD_TYPE is set to '${CMAKE_BUILD_TYPE}'")
string(TOUPPER "${CMAKE_BUILD_TYPE}" uppercase_CMAKE_BUILD_TYPE)
if(uppercase_CMAKE_BUILD_TYPE STREQUAL "DEBUG")
    set(PICO_DEOPTIMIZED_DEBUG 1)
    message(STATUS "Debug configuration detected. Switch PICO_DEOPTIMIZED_DEBUG on.")
else()
    set(PICO_DEOPTIMIZED_DEBUG 0)
    message(STATUS "Debug configuration not detected. Swith PICO_DEOPTIMIZED_DEBUG off.")
endif()
message(STATUS "PICO_DEOPTIMIZED_DEBUG is set to '${PICO_DEOPTIMIZED_DEBUG}'")

# This block automatically detects the active selection in VS Code
if(CMAKE_CXX_COMPILER_ID STREQUAL "GNU" OR CMAKE_CXX_COMPILER_ID STREQUAL "Clang")
    
    # 1. If you select "Debug" in VS Code:
    set(CMAKE_CXX_FLAGS_DEBUG "-O0 -g -gstrict-dwarf -gdwarf-3" CACHE STRING "Debug flags" FORCE)
    
    # 2. If you select "Release" in VS Code:
    set(CMAKE_CXX_FLAGS_RELEASE "-O3" CACHE STRING "Release flags" FORCE)

endif()

add_compile_options(-march=armv8-m.main+fp+dsp)


# path to PICO utilities (if needed)
if (NOT DEFINED ENV{PIOASM_DIR})
        message("PIOASM: set PIOASM_DIR env variable if you use PIO")
else()
        message("PIOASM: PIOASM_DIR env variable is set to '$ENV{PIOASM_DIR}'")
        set(pioasm_DIR $ENV{PIOASM_DIR})
endif()
if (NOT DEFINED ENV{PICOTOOL_DIR})
        message("PICOTOOL: set PICOTOOL_DIR env variable if you create uf2 output with pico_add_extra_outputs()")
else()
        message("PICOTOOL: PICOTOOL_DIR env variable is set to '$ENV{PICOTOOL_DIR}'")
        set(picotool_DIR $ENV{PICOTOOL_DIR})
endif()

# set(PICO_PLATFORM rp2350-riscv CACHE STRING "Pico Platform")
set(PICO_PLATFORM rp2350-arm-s CACHE STRING "Pico Platform")
set(PICO_BOARD pico2 CACHE STRING "Board type")


include(pico_sdk_import.cmake)

project(pico_pid_template C CXX ASM)

pico_sdk_init()

include(FetchContent)

# CMSIS DSP fixed point c++ library dsppp
FetchContent_Declare(dsp_fixed_point
  GIT_REPOSITORY "https://github.com/ARM-software/CMSIS-DSP.git"
  GIT_TAG HEAD
  GIT_SHALLOW OFF # needed to find the commit HEAD
  # prevent makefile execution (if any)
  SOURCE_SUBDIR =
)
FetchContent_MakeAvailable(dsp_fixed_point)

# PID embedded C++ library
FetchContent_Declare(pid_embedded
  GIT_REPOSITORY "https://github.com/jancumps/pid_embedded_cpp.git"
  GIT_TAG origin/main
  # prevent makefile execution (if any)
  SOURCE_SUBDIR =
)
FetchContent_MakeAvailable(pid_embedded)

include_directories( # this project uses CMSIS DSP fixed point library, so include the path to the CMSIS DSP headers
    ${PICO_SDK_PATH}/src/rp2_common/cmsis/stub/CMSIS/Core/Include
    ${dsp_fixed_point_SOURCE_DIR}/dsppp/Include/dsppp
)


add_executable(${CMAKE_PROJECT_NAME})

target_compile_definitions(${CMAKE_PROJECT_NAME} PRIVATE 
    ARM_MATH_CM33=1
)

target_sources(${CMAKE_PROJECT_NAME}
        PUBLIC
        ${CMAKE_CURRENT_SOURCE_DIR}/main.cpp
)
target_sources(${CMAKE_PROJECT_NAME}
        PUBLIC
        FILE_SET cxx_modules TYPE CXX_MODULES FILES
        ${pid_embedded_SOURCE_DIR}/source/pid_template.cpp
)

target_link_libraries( ${CMAKE_PROJECT_NAME}
        pico_stdlib
        hardware_adc
        hardware_gpio
        hardware_pwm
)

pico_add_extra_outputs(${CMAKE_PROJECT_NAME} )

CMake edits to make it build for Pico RP2040:

# set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -mfpu=fpv5-sp-d16") # TODO: enable for Pico2
# add_compile_options(-march=armv8-m.main+fp+dsp) # TODO: enable for Pico2
add_compile_options(-march=armv6-m)
# set(PICO_PLATFORM rp2350-arm-s CACHE STRING "Pico Platform") # TODO: enable for Pico2
# set(PICO_BOARD pico2 CACHE STRING "Board type") # TODO: enable for Pico2
set(PICO_PLATFORM rp2040 CACHE STRING "Pico Platform")
set(PICO_BOARD pico CACHE STRING "Board type")
    # ARM_MATH_CM33=1 # TODO: enable for Pico2
    ARM_MATH_CM0PLUS

Timings

Single execution: The PID loop lasts 560 ns with full optimisation on. 

image

After I wrote this bog, I optimised the loop further, using DMA.

Instead of setting the PWM duty cycle right after the PID loop, I wrote the requested duty cycle to a variable, and flagged DMA that it needs to do its job.
At program startup, I associate both the variable, and the PWM duty cycle register, with a DMA channel.
After the PID results are stored in the variable, I flag to the DMA that new data is ready.
At the start of the PWM period, that duty cycle is applied to the PWM signal.

For the CPU, this flagging is cheaper than setting the duty cycle directly via an SDL call.

The result is that the PID loop now takes 460 ns instead of 560 ns, on a Pico 2 / RP2350 ARM at 150 MHz.
The same DMA design, on a Pico 1 / RP2040 at 125 MHz, takes 1.140 µs.
And on a Pico 2 / RP2350 RISC at 150 MHz:

  • with fmp fixed point lib (similar Q15 data type), 640 ns.
  • with cnl fixed point lib (again similar Q15 type, 496 ns.

code snippet:

    //  ADC 12 bits to Q15 conversion, using efficient bit shift
    feedback.v = static_cast<int16_t>((adc_fifo_get()) << 3); // Direct to 0.0 - 1.0 per-unit in Q15!

    // Convert Q15 per-unit (0.0 to 1.0 excluded) to raw timer counts (0 to 65535)
    // the level will be 0 - 4095, 12 bits
    duty = static_cast<std::uint16_t>(controller.compute(target_command, feedback).v >> 3); // set PWM value
    dma_channel_set_trans_count(dma_chan, 1, true);

The samples happen clock steady every 276 µs.


image

Measurements done on a Pico 2 / RP2350 ARM, at the default 150 MHz.
I used a GPIO pin to measure both times, toggled in the ADC interrupt handler.
It's not an exact representation of when the sample happens, and when the PID is finished. But I think this is a reasonable way to validate timings.

references:

Development kit:  Pi Pico Eurocard Development Board 

Previous Pico PID blog:   Pico PID controller without floating point using DSP C++ fixed point API 

PID class GitHub repository

VS Code project - with DMA. Configured for Pico 2 / RP3250 ARM. Check the CMake section above to configure for an RP2040. The non-dma source is available as main.cpp.pidtimer: pico_pid_template_dma_20261024 (2).zip

VS Code project - with DMA. Configured for Pico 2 / RP3250 RISC pico_pid_template_20261025_riscv.zip.

Thank you for reading

  • Sign in to reply
  • Jan Cumps
    Jan Cumps 17 days ago in reply to Jan Cumps

    When I use a different fixed point library, https://github.com/johnmcfarlane/cnl, I get a faster loop: 496 ns. So it pays off to check out the options.

    Because fmp and cnl libs both support C++ standard numeric behaviour, exchanging is easy.

    • adapt make file to retrieve the code.
    • use different include
    • adapt your data type declaration:

    fmp: (640 ns)

    #include "fixed.hpp"
    using fp_t = fpm::fixed<int16_t, int32_t, 15>;
    constexpr fp_t operator""_fp(long double v) noexcept {
        return fp_t(v);
    }

    cnl: (496 ns)

    #include "cnl/all.h"
    using fp_t = cnl::scaled_integer<int16_t, cnl::power<-15>>;
    constexpr fp_t operator""_fp(long double v) noexcept {
        return static_cast<fp_t>(v);
    }

    If you also provide conversion functions for the library you use, you likely don't have to change any other code, when switching out libraries

    template <typename T>
    using underlying_type_t = typename std::remove_reference<decltype(cnl::unwrap(std::declval<T>()))>::type;
    template <typename T>
    constexpr auto to_12bit_uint32_t(T&& val) -> underlying_type_t<T> {
    return static_cast<uint32_t>(cnl::unwrap(std::forward<T>(val)) >> 3);
    }
    constexpr auto from_12bit_uint16_t = [](auto raw_bits) {
    return cnl::from_rep<fp_t, std::int16_t>{}(static_cast<std::int16_t>(raw_bits << 3));
    };
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 18 days ago in reply to Jan Cumps

    RISC update:

    So I found a fixed floating point library that works with RISK: https://github.com/MikeLankamp/fpm/blob/master/include/fpm/fixed.hpp

    Now that I can make the RISC CPU do the calculation in fixed floating point , without any float calculations in the loop,
    the RP2350 runs a PID loop at 640 ns. That's 200 ns slower than the ARM core, but 500 ns faster than RISC with a float.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 18 days ago

    I tried this same example, on the RISC-V cores of the RP2350

    The comparison is unfair at the moment because:

    • I don't have a fixed point library for the RISC family (yet), so I have to use floating point math
    • the RISC cores don't have an FPU, They can't use the ARM FPU, so have to do all floating point math in C on the CPU, that doesn't have floating point instructions.

    The PID loop time is 11 µs. 

    I'll try to find q fixed floating point lib for the RISC, either a Q15 or Q31 version. The results should be fairly similar to ARM then.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 18 days ago in reply to Jan Cumps
    • Using DMA to control PWM, instead of calling the PWM APIs, reduced total loop to 460 ns.

    On a Pico 1 / RP2040, running at 125 MHz, the loop takes 1140 ns.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 19 days ago in reply to Jan Cumps

    correction, can't update:

    typo:  That's a run each 273 ms. 

    should be:  That's a run each 273 µs. 

    the percentage is correct.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>