Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Raspberry Pi Operating Temperature Comparison (A+, B+, Zero, Pi 2, Pi 3)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: cstanton
  • Date Created: 2 Mar 2016 12:57 PM Date Created
  • Views 9004 views
  • Likes 10 likes
  • Comments 20 comments
Related
Recommended
  • b+
  • heat
  • raspberry pi 2
  • raspberry pi operating temperature
  • a+
  • raspberry pi
  • model a+
  • model b+
  • raspberry pi heat
  • raspberry pi 3
  • model b
  • raspberry pi 1
  • raspberry pi temperature

Raspberry Pi Operating Temperature Comparison (A+, B+, Zero, Pi 2, Pi 3)

cstanton
cstanton
2 Mar 2016

Thanks to Gareth Halfacree, whom took a series of photographs of the Raspberry Pi processor under heavy load, I think. Note there's no load on the GPU in these photographs. You can see how potentially hot each processor chip of the Raspberry Pi get. These are at stock processing speeds with no overclock and using sysbench to push the CPU.

 

element14 does sell Raspberry Pi HeatsinksRaspberry Pi Heatsinks

 

{gallery} Raspberry Pi Operating Temperatures Individual Scaling

image

Raspberry Pi 1 Model A+: 13.5degC to 28.8degC

image

Raspberry Pi Zero: 13.1degC to 44.1degC

image

Raspberry Pi 1 Model B+: 14.9degC to 32.5degC

image

Raspberry Pi 2 Model B: 12.4degC to 49.4degC

image

Raspberry Pi 3 Model B: 16degC to 87.6degC

image

Raspberry Pi 3 Model B Close up: 45.1degC to 101.3degC

{gallery} Raspberry Pi Operating Temperatures Normalised Scale

image

Raspberry Pi 1 Model A+: Normalised Temperature View

image

Raspberry Pi Zero: Normalised Temperature View

image

Raspberry Pi 1 Model B+: Normalised Temperature View

image

Raspberry Pi 2 Model B: Normalised Temperature View

image

Raspberry Pi 3 Model B: Normalised Temperature View

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 10 years ago in reply to clem57 +3
    Hi Clem, It will be guesswork, because not all characteristics are know, but this online tool is useful: Calculating heat sinks Usually I plug in approximate values if they are not known (there are some…
  • bwelsby
    bwelsby over 10 years ago in reply to cstanton +2
    Christopher Stanton wrote: HAT add on boards will likely also be affected due to vertical clearance, or lack of. yes that's a problem, maybe something like this is better : MPC151525T - AMEC THERMASOL…
  • shabaz
    shabaz over 10 years ago in reply to bwelsby +2
    That's actually really good. Those ceramic heatsinks are (literally) cool : ) I actually have one here for another project, but unfortunately 22x22mm : ( will see if it fits. ( MPC222225T - AMEC THERMASOL…
  • bwelsby
    bwelsby over 10 years ago in reply to shabaz

    You shouldn't have a problem with 22x22 there's a few tiny black specs around the SOC, I think they call them resistors image  The SOC is higher and the ceramic heatsink is non-conductive anyway.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to clem57

    Hi Clem,

     

    Correct, the BCM.. chip is only about 14x14mm as Brian mentions.

    I've just opened up the Pi 3 box, and looks like the BCM.. chip is not as low-profile as I thought it might be. It is higher than surrounding components, so a 22x22mm should fit too, since that is only an additional 4mm overhang on each edge.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to shabaz

    This is a bigger square. Right?shabaz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to bwelsby

    That's actually really good. Those ceramic heatsinks are (literally) cool : )  I actually have one here for another project, but unfortunately 22x22mm : ( will see if it fits.

    ( MPC222225T - AMEC THERMASOL - Heat Sink, Square, Micro Porous, 10.21 °C/W, 2.5 mm, 22 mm, 22 mm | Farnell element14  )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to cstanton

    Christopher Stanton wrote:

     

    HAT add on boards will likely also be affected due to vertical clearance, or lack of.

    yes that's a problem, maybe something like this is better : MPC151525T - AMEC THERMASOL - Heat Sink, Square, Micro Porous, 10.21 °C/W, 2 mm, 15 mm, 15 mm | Farnell element14  it's only 2mm thick and at 15mm square is about the same size as the SOC

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>