Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Raspberry Pico as USB test device - part 1: the TinyUSB USBTMC profile
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 29 Jan 2023 3:20 PM Date Created
  • Views 9440 views
  • Likes 14 likes
  • Comments 14 comments
Related
Recommended
  • raspberry
  • pico_usbtmc_scpi
  • pico
  • scpi

Raspberry Pico as USB test device - part 1: the TinyUSB USBTMC profile

Jan Cumps
Jan Cumps
29 Jan 2023
Raspberry Pico as USB test device - part 1: the TinyUSB USBTMC profile

There's a standard profile for USB test devices, called USBTMC. If your instrument supports it, it becomes a plug-and-play device for the likes of LabVIEW. The Raspberry Pico examples come with a set of TinyUSB profile examples, and USBTMC is one of them. In this post, I run the example on a Pico and check if my operating system and the LabVIEW utilities recognise it. 

image

This started as a blog to investigate if the Pico + TinyUSB Test and Measurement protocol example renders a device that's recognised by LabVIEW. But I had a bit of tailwind. At the end of the blog you'll find the source for a first shot at a real USBTMC lab programmable instrument.

Check if the instrument is detected upon plugin via Zadig

The example does not implement an instrument, but it enables USB and makes itself known as a usbtmc. When the firmware is loaded and running, the first test should be if the device is recognised. I use the Zadig log screen for that. Good news immediately:

image

Check if the usbtmc device driver is loaded

This one is obvious from the Zadig screen (Usbtmc driver version 16.x loaded), but let's look at the device manager:

image

More success. The appropriate driver - exactly the same one as used for my usbtmc compatible Keatley meter - is loaded. You recognise the properties that Zadig logged earlier.

Test if NI-Visa recognises it

If a device enumerates as usbtmc, the NI-Visa tools should detect it. The easiest way to see that is by starting NI-MAX, the NI instrument explorer.

image

That completes this test. The device does not have any intelligence, but is able to make itself known as a usbtmc. And software recognises that after plugging it in a USB bus. This 'll be my first step to try and write a Pico "native" test instrument with the C-SDK.

Preview of a working project

I made a SCPI Pico instrument that worked via USB-serial before. I've ported it to the USBTMC profile. It is working, but barely. The same commands are supported,

Here's the VSCode project. Use it for an initial view only. The reply engine isn't working stable yet (activity for the next blog post).
Don't forget to add these two variables to your VSCode user environment:

image

scpi_switch_usbtmc_20230129.zip

link to all posts

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 3 years ago +1
    One minute extra quality time, and I got it working: I'm attaching the current VSCode project to the blog
  • Jan Cumps
    Jan Cumps over 3 years ago +1
    One of the advantages using USBTMC is that this Pico will enumerate identical to commercial instruments. A Keithley meter, Rigol power supply and the Pico are connected. For LabVIEW (and PyVISA), they…
Parents
  • Jan Cumps
    Jan Cumps over 3 years ago

    One of the advantages using USBTMC is that this Pico will enumerate identical to commercial instruments. 

    image

    A Keithley meter, Rigol power supply and the Pico are connected. For LabVIEW (and PyVISA), they are immediately recognised as VISA instruments.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 3 years ago

    One of the advantages using USBTMC is that this Pico will enumerate identical to commercial instruments. 

    image

    A Keithley meter, Rigol power supply and the Pico are connected. For LabVIEW (and PyVISA), they are immediately recognised as VISA instruments.