Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Stepper Motor Control with Raspberry Pico PIO and DRV8711 driver- Part 2: SPI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 30 Mar 2025 5:18 PM Date Created
  • Views 1153 views
  • Likes 8 likes
  • Comments 2 comments
Related
Recommended
  • pico_eurocard
  • PIO

Stepper Motor Control with Raspberry Pico PIO and DRV8711 driver- Part 2: SPI

Jan Cumps
Jan Cumps
30 Mar 2025

The Pico has a set of PIO co-processors. They are real-time controllers that can execute logic with deterministic timing. Ideal to run strict-timed sequences and state machines. And to implement extra peripherals.
In this series, I'm trying to use the PIO to control a TI DRV8711 stepper motor controller.

image

Follow up of  Stepper Motor Control with Raspberry Pico PIO and DRV8711 driver- Part 1: Hardware Provisioning 

SPI requirements and setup

The TI DRV8711 stepper motor driver, that we use in this project, relies on pre-configuration via SPI.

These are the Pico resources I reserve:

signal DRV8711 Pico
SPI CLK SCLK default SCLK  IO18
SPI CS SCS default CS* IO17
SPI MISO sdato default MISO** IO16
SPI MOSI sdati default MOSI IO19
SPI default spi0

SPI settings:

baud 1000 * 1000
message size 16 bits


* DRV8711 uses a chip select that's active high. Pico's SPI library doesn't support that, so I will bit bang that pin.
** DRV8711 uses open collector for outputs. Pico will have to provide the rail via a pull-up.

The setup code isn't complex. You 'll recognise the special cases mentioned below:

void init_drv8711_spi_hw() {
    // Enable SPI 0 at 1 MHz and connect to GPIOs
    spi_init(spi_default, 1000 * 1000);
    spi_set_format(spi_default, 16, SPI_CPOL_0, SPI_CPHA_0, SPI_MSB_FIRST); // 16 bit registers
    gpio_set_function(PICO_DEFAULT_SPI_RX_PIN, GPIO_FUNC_SPI);
    gpio_set_pulls(PICO_DEFAULT_SPI_RX_PIN, true, false); // drv8711 outputs are open drain
    gpio_set_function(PICO_DEFAULT_SPI_SCK_PIN, GPIO_FUNC_SPI);
    gpio_set_function(PICO_DEFAULT_SPI_TX_PIN, GPIO_FUNC_SPI);
    // CS is active-high, invert pin action
    gpio_set_function(cs_, GPIO_FUNC_SPI);
    gpio_set_outover(cs_,GPIO_OVERRIDE_INVERT );
}

I provided a helper for bit write (the width of the DRV8711 registers):

static void spi_write(const uint16_t &data) {
    spi_write16_blocking(spi_default, &data, 1);
}

Here's an example of a register structure, with a convert-to-16-bit operator. This code sits in a DRV8711 driver that I wrote for this project.

struct CTRL {
                            // address 14-12
    unsigned int dtime;		// 11-10
    unsigned int isgain;	// 9-8
    unsigned int exstall;	// 7
    unsigned int mode;		// 6-3
    unsigned int rstep;		// 2
    unsigned int rdir;		// 1
    unsigned int enbl;		// 0
    inline operator uint16_t() const {
        return (0x0000 << 12) | (dtime << 10) | (isgain << 8) |(exstall << 7) | (mode << 3) | (rstep << 2) | (rdir << 1) | (enbl);
    }
};

Then the declaration of an object of that type, with initialisation. This allows the linker / loader to fill this structure straight away at firmware loading. Not a single clock tick of runtime code is involved in this construct:

drv8711::CTRL reg_CTRL {
    0x0003, // DTIME
    0x0003, // ISGAIN
    0x0000, // EXSTALL
    0x0003, // MODE 8 microsteps
    0x0000, // RSTEP
    0x0000, // RDIR
    0x0001  // ENBL
};

I have that mechanism for all DRV8711 registers. Here's the code to actually write the setup to the IC:

void init_drv8711_settings() {
    // Set Default Register Settings
    spi_write(reg_CTRL);
    spi_write(reg_TORQUE);
    spi_write(reg_OFF);
    spi_write(reg_BLANK);
    spi_write(reg_DECAY);
    spi_write(reg_STALL);
    spi_write(reg_DRIVE);
    spi_write(reg_STATUS);
}

The full code will be attached when I'm a bit further into this project. Next post will focus on provisioning the non-SPI pins.

Meanwhile: here's the full conversation from Pico to DRV8711:

image

  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 1 year ago

    Little follow up:  Stepper Motor Control with Raspberry Pico PIO and DRV8711 driver- Part 3: GPIO 

    just documenting the digital pins used. Nothing exciting

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 1 year ago

    Well done Jan.