Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Triggered Sound FX: On-the-Fly Sound Mixing with Pi Pico
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 5 Jan 2024 11:04 PM Date Created
  • Views 5972 views
  • Likes 11 likes
  • Comments 33 comments
Related
Recommended
  • audio dac
  • audio
  • rpibeginner
  • sound
  • sound effects
  • pi pico

Triggered Sound FX: On-the-Fly Sound Mixing with Pi Pico

shabaz
shabaz
5 Jan 2024
Triggered Sound FX: On-the-Fly Sound Mixing with Pi Pico

Table of Contents

  • Introduction
  • How Does it Work?
  • Using the Ready-Built Code
  • Source Code
  • Changing the Sounds
  • Summary


Introduction

This short project can be used to output WAV format sound effects for animatronic displays (such as at model train exhibitions), but it could have other applications, too. It was created after a requirement was mentioned by colporteur . The requirement was to be able to generate farm animal sounds in synchronization with the physical movements that the animals make.

This project uses a Pi Pico with up to 8 (for now) trigger inputs to accept when a sound needs to be played out. The sound recordings (recorded in WAV format) are then played through a speaker. Since all animals are equal, the Pi Pico will mix the WAV recordings on-the-fly, so you can have a whole menagerie of animals all making their sounds whenever required.

The entire project is through-hole soldered because it relies on using ready-made modules. It is a quick-to-solder project because I originally designed the board for construction by kids in a project described here:  Pocket Scarface – Pi Pico Python Based MP3 Clip Player 

This new project reuses all the same hardware from that earlier project; only software changes were required!

There is a quick video demo here; it’s a bit repetitive because it was tempting to keep hitting buttons on it!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

How Does it Work?

The general idea is simple; there are a bunch of inputs on a Pi Pico microcontroller, and whenever they are activated (the precise method of activation is for further study! For now, I used buttons), then the Pico will output digital sound information (in 24kbit/sec mono format for now) to an audio DAC module which plays it out. That’s it for the hardware; all the interesting stuff happens in software.

image


The PCB layout below shows how everything fits on the board. As mentioned, this board was used for an earlier project, so the PCB and circuit won’t be described here since there’s zero hardware difference from the earlier project. You can refer to that earlier blog to build the board if desired. The only difference is the software, which will be discussed next.

image

The way the software works is that it continually fills a buffer array with sound samples whenever a memory buffer is free. The Pico’s low-level PIO functionality uses the buffer content to clock out data in I2S format to the DAC. All the main.c file code has to do is figure out what to put in the buffer! The way that is achieved, is that whenever a trigger is activated, the sample values for the WAV sound get added to the sample values for whatever other trigger sounds have been activated. Up to 8 sounds can be played simultaneously (or 'voiced') in this way. The same trigger can occur repeatedly if desired (e.g., hitting the same button quickly repeatedly), because, as long as at least one voice is free, then sound samples can be assigned to it. The C code merely sums up the 8 voice samples to create a single output sample and repeats until the buffer is full.


Using the Ready-Built Code

If you already have a Pi Pico and an I2S DAC board (it doesn't have to be the same board as I used, but that is tried-and-tested), then all you need to do is wire them up (there are three wires which make up the I2S interface, plus GND), and then you’re ready to use the code.

image

With the board unpowered (no 9-12V source) hold down the BOOTSEL button on the Pi Pico (it is the only button on the Pi Pico), and then plug in the USB connector to the PC, and then release BOOTSEL. A drive letter will appear on the PC, and you can drag-and-drop the ready-built sound_fx_mixer.uf2 file onto it. After a minute or so, it will be programmed. Now the USB can be disconnected and a 9-12V battery can be attached (only connect it when the PC is disconnected). Shorting any trigger input GPIO pins to GND will make an animal sound! The PCB layout above has buttons connected to the trigger inputs.

The ready-built code uses the following sound assignments for the 8 triggers:

Cat, Cow, Dog, Goat, Hen, Rooster, Snake, Wolf.

The assignments are easy to modify in the code. You can also add any custom sounds.

If you wish to make such custom modifications to the code, then the next section explains what needs to be done. You need to be familiar with building C/C++ code for the Pi Pico – there are several blogs written by various people, explaining this on element14 and other websites.

Source Code

The software is written in C/C++ and requires ARM developer tools and the Pico C/C++ SDK to be installed; this is not discussed here; there are other blogs that explain how to set up the computer environment for this. This blog will assume a top-level path c:\development\pico, and then within that folder, there is a folder called pico-sdk which contains that Pico C/C++ SDK.

You’ll also need to install code known as pico-extras. To do that, type the following at c:\development\pico (or whichever top-level path you’re using):

git clone https://github.com/raspberrypi/pico-extras.git

Now you’ll have a pico-extras folder too.

Add the following environment variables to your system (how to do this is described in the blogs that explain how to use the Pico C/C++ SDK).

PICO_SDK_PATH=c:\development\pico\pico-sdk;PICO_EXTRAS_PATH=c:\development\pico\pico-extras

The triggered sound FX project source code is on GitHub. Download and extract that to C:\development\pico, so that a folder called sound_fx_mixer appears there. You could use the git clone command to do this:

git clone https://github.com/shabaz123/sound_fx_mixer

Now you can build the code in the usual way; follow any existing Pi Pico C/C++ SDK tutorial blogs. I used the CLion development environment for Pi Pico C/C++ projects (screenshot below), but there are tutorial blogs that show how to use Visual Code instead, and there are other tutorials that demonstrate how to build code directly from the command line.

image

Changing the Sounds

The code predominantly consists of a main.c file and a load of C files containing the animal sounds in C arrays.

If you wish to use different sounds, you must convert your desired sound files (in WAV format) to C array files. To do that, there is a Python script in the wav_convert folder. It will convert every .wav suffixed file placed in the wav_files sub-folder, into C files placed in the output sub-folder. You can then copy-paste the C files into the ~/development/pico/sound_fx_mixer folder. The C files will contain arrays that have the same name as the original WAV files, so it’s important to give good names to the WAV files before converting them. For instance, if you want a bird sound, call the WAV file something like bird1.wav and then the wav_convert.py Python program will generate a C file called bird1.c, containing a C array called bird1.

Note that only mono 24 kbit/sec WAV files must be used. Software such as Audacity may be able to convert files into that format.

In the code, the following changes need to be made.

First, add the file names to the CMakeLists.txt file:

add_executable(sound_fx_mixer
main.c
cat1.c
cat2.c
cow1.c

The remainder changes all need to be made in the main.c file.

Declare the C arrays in a similar style as shown below.

/********* extern declarations for all the sound arrays *********/
extern const int16_t cat1[18472];
extern const int16_t cat2[15190];
extern const int16_t cow1[36258];

Next, ensure that the desired new sound is part of the sound_array:

// array of pointers to the sound arrays
const int16_t *sound_array[21] = {
cat1, /* 0 */
cat2, /* 1 */
cow1, /* 2 */

Make sure that there are defines for the sounds:

// definitions for convenience
#define CAT1 0
#define CAT2 1
#define COW1 2

Fill in the sound_array_len array, with the entry for your new sound:

// array of lengths of the sound arrays
const int sound_array_len[21] = {
COUNT_OF(cat1), COUNT_OF(cat2), COUNT_OF(cow1),

There are 8 triggers supported currently (there are 10 buttons on the board, but only the first 8 are used for now).

The button_sound_map defines what sounds you want played whenever the trigger occurs. If the first button is pressed, the cat1 sound will be played with the example sound map below:

const int button_sound_map[8] = {CAT1, COW1, DOG1, GOAT1, HEN1, ROOSTER1, SNAKE1, WOLF1};

Now the code can be re-built.

Summary

It was nice to see that experimenting with audio using C programming with the Pi Pico is not difficult. It would be interesting to extend the project with (say) simultaneous background music capability!

As another project idea, the animal sounds could be replaced with musical instrument notes for up to 8-note polyphony, for a simple children’s toy.

If you have ideas for this project, it would be great to hear about them!

Thanks for reading.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 2 years ago +2
    colporteur fmilburn Guide to building Pi Pico projects is here: Working with Pi Pico C/C++ Projects Easily: A Docker Approach! I think watching the video there may help, since it shows all the steps…
  • shabaz
    shabaz over 2 years ago in reply to javagoza

    IHi Enrique,

    I was thinking the same, it's surprisingly fun for kids, I was not expecting that. I placed it next to a couple of kids yesterday, and as soon as they saw from the first button press or two that it made animal sounds, all they did after that was press many buttons simultaneously or quickly in succession, to hear a farm or jungle of animals : ) They liked the dog sound a lot, pressing it quickly many times while other animal sounds were playing. I found it interesting because I did not suggest to them to try more than one button at once!

    If I can find flat buttons where the keycaps cannot be accidentally pulled off and eaten by say 1-year-olds, then it would be neat to have a 100-animal, or say 144-animal jungle-in-your-home version, with pictures on the buttons : ) 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to genebren

    I've not tried Arduino environment with Pi Pico, but I think there's less need for that on the Pico since the C SDK is very good, just a long process to set up everything, and everyone's machine may have different stuff on it, some causing conflicts perhaps : (

    The Docker approach avoids that by having clean layers, so that there's  a far reduced chance of the environment having problems, if the container can run.

    I've just attempted that approach directly on Windows (without a Linux virtual machine) and that works, which is nice. It will save a bit more time for Windows users. I'll stick the details at  Working with Pi Pico C/C++ Projects Easily: A Docker Approach! 

    I tested with Windows 11, it should be fine with say Windows 10 too I hope. Earlier than that will be dependent on what the Docker engine supports (I'll google around in case I can find that answer). With this approach, very few lines of text need to be copy-pasted, and it will definitely work, because the original Docker container will be identical for everyone, so if the steps work for one person inside the container, then those steps have to work for others too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 2 years ago in reply to fmilburn

    "It is my ability to install the pico c/c++ development tools that I am unsure about."

    I understand what you are talking about.  I tried on multiple machines and different development packages (C and python) and I could not get a suitable development experience.  The libraries did not seem correct (I could not generate an I2C communication) and the development environment was incompatible with my machine (trying to store things in non-existing directories).  I even tried an example using the arduino IDE, but again library issues.

    I know that others have been much more successful, but it was not the experience that I expected.  Maybe when I have a bit more time, I will try again as I am really interested this device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 2 years ago

    Great, thanks for sharing. I'd love to play around with this when I have some more time this year. It is a great project to encourage kids to tinker.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago

    colporteur  fmilburn 

    Guide to building Pi Pico projects is here:  Working with Pi Pico C/C++ Projects Easily: A Docker Approach! 

    I think watching the video there may help, since it shows all the steps within 8 minutes, so it's not a lot of steps, and they can all be copy-pasted.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>