Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Model B Cases?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 180 replies
  • Subscribers 727 subscribers
  • Views 20203 views
  • Users 0 members are here
  • raspberry
  • help
  • pi
  • b
  • raspberry_pi
  • 3d_printing
  • model
  • case
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Raspberry Pi Model B Cases?

Wwessex
Wwessex over 14 years ago

Hi,

I was wondering if anyone knows of a case for the Model B?

  • Cancel
Parents
  • fustini
    fustini over 14 years ago

    That's a good question also I think a great business opportunity for those with laser cutters or 3d printers like hackerspaces.  I would definately pay some money for a nice case/enclosure.

     

    Looks like there's already a few designs on Thingiverse:

     

    http://www.thingiverse.com/search?q=raspberry&sa=Search

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    I have put a RepRap design on thingiverse : http://www.thingiverse.com/thing:16104

     

    Also put a version  on shapeways.   http://www.shapeways.com/shops/picase

    I have 4 versions there.

    With 1mm walls - open bottom and closed bottom

    With 1.4mm walls - open bottom and closed bottom

    I would advise the 1.4mm walls version, because it is much much stronger. Bad side it is a bit more expensive because it uses more material

     

    There is a big difference between a RepRap version and the one on shapeways.

    For RepRap printing everything needs to be supported, so there is a strange case split needed to get this working.

    The 2 case halfs stick together by friction....

     

    Downside of Shapeway is the price... but it is very very well made, very fine detail and the 2 halfs click together.

    This weekend I will put up a version with an open top and possible an open bottom with 1.4mm walls, but with room to put a transparent perspex sheet (5x8 cm) instead. So that will save a lot of material costs.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Home come the case is more expencive than the RPI itself ?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Because there are no cheap cases yet available.

    Shapeways 3D printing costs a lot, its meant to print single pieces, and not order 1000 of them....

    (and it is cheaper than the Pi....including vat and delivery...)

     

    If you have a 3D printer, you can use the thingiverse design and print it for under 1 Euro of plastic costs...

    But you need to have a 3d printer  image (and I don't have one) and it takes time to print one.

     

    Probably within a month or so there will be cheap cases available...

    The manufacturers probably also want to wait on a production model before they start making costs for molds....

    I believe even in the feature the price will include a lowcost see through plastic case.

     

    You just need to have patient...

    Or you want it now...or you want to have a unique case...

     

    The thingiverse design contains all sort of parameters which you can tailor to get an unique version...

    That is why I put it up there, so people would have a base case design which they can alter.... generate stl files from it

    and print it on a RepRap printer or sent it to shapeways (or someone else) to get it done.

     

    You can also buy some perspex sheets (not expensive) and cut them yourself and glue them together...

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • alecthegeek
    alecthegeek over 14 years ago in reply to e14 Contributor

    Or you can purchase a small cheap plastic food container, cut some holes for cables, and use some form of padding to hold it place when when the lid is on?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • alecthegeek
    alecthegeek over 14 years ago in reply to e14 Contributor

    Or you can purchase a small cheap plastic food container, cut some holes for cables, and use some form of padding to hold it place when when the lid is on?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to alecthegeek

    yes of course...

    Just look for creditcard boxes cases or whatever.  you can use, I don't know how its called in english, sticky stuff they use for putting up posters, to hold the board.

    Or you can use perspex sheets with distance holders with a 1.6 mm (thickness of the pcb)  groove in it, to hold the board in place...

     

    There was even someone who make a pdf which you could print, and with cutting and folding you would get a case

    There were also some suggestions to ship the Pi in cardboard which you could transform to a simple case

     

    That is the fun bit of having the first board...

    Too bad I wasn't able to get one, I hope that I got on one of the 'interested' list (filled it in), but until now I didn't get any confirmation...