Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Seneca breaks silence on Fedora Remix
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 84 replies
  • Subscribers 709 subscribers
  • Views 10083 views
  • Users 0 members are here
  • raspberry
  • help
  • helpme
  • raspberry_pi
  • raspberrypi
Related

Seneca breaks silence on Fedora Remix

e14 Contributor
e14 Contributor over 14 years ago

After a puzzling two months of silence from Seneca with regard to

plans for fixing the withdrawn Fedora Remix, there is a blog post

indicating that work is starting with the beginning of summer,

including fixing the problem with attempting to change the timezone.

 

http://roottothehead.blogspot.com/2012/05/summer-at-seneca.html

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Chris Tyler posted an update today.

    Estimated release date is 20th, but lots of work to do.

     

    http://lists.fedoraproject.org/pipermail/arm/2012-July/003631.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    That's a very interesting read.

    Lots of problems that appear directly related to trying to force options suited to todays desktops onto the comparatively resource light Pi.

    You have to wonder what PCI devices they expect to see on the Pi.

     

    Wanting to enable SELinux seems particularly strange. If there's any educational goal left, surely we want to get kids interested and hooked on doing stuff before we teach them to hate SELinux ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 14 years ago in reply to e14 Contributor

    From what I read here he actually says

     

    1) I want it to actually scan for the PCI devices ...yes the RPi doesn't have a PCI expansion  but it's quite possible for a
    SOC or any other part to have an internal PCI bus that the peripherals are attached to and also not all may be enabled since that GPU device does some configuring before hand so you can't just guess the config.

     

    2) X performance is poor......Yes it is!.... better than it was at day 0 though! ....I think theat X is very useful since most people don't want tto be thrown into a command line these days if they don't have UNIX experience

     

    3) Re SELinux he's actually saying the SELINUX configuration is TOO memory expensive not that he wants to put it in regardless just that the memory burn is a total PITA.

     

    BTW I saw some where that some bunch had got a generic openGL implementation going using the GPU how do we get this back to these guys rather than moaning !!!

     

    Thanks for the Update BTW Coder27

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to Problemchild

    I see that needing a different SD card for each different image is going to be a major pain in the backside.  Pi really needs a network image boot, so that we can store umpteen different images externally and the SD card can remain fixed --- let the VideoCore boot just a network-aware bootstrap, not a Linux kernel.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to Problemchild

    I see that needing a different SD card for each different image is going to be a major pain in the backside.  Pi really needs a network image boot, so that we can store umpteen different images externally and the SD card can remain fixed --- let the VideoCore boot just a network-aware bootstrap, not a Linux kernel.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jamodio
    jamodio over 14 years ago in reply to morgaine

    AMEN !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 14 years ago in reply to jamodio

    I'm wondering if a  network aware minikernel would be good for this then ?!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to jamodio

    If they really want the Pi to get into schools then network boot is pretty much mandatory.  The horrors of administering classroms full of devices each with local storage don't bear thinking about.  You have to have central administration or teachers will be jumping off bridges.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 14 years ago in reply to morgaine

    Yes and no. The idea of just been able to tinker means you need to be able to do your own thing with your own image.

    However if you are putting these into schools you need to be able to revert these systems at least for the period of the lesson to a common system image so that you can be certain of reaching a given outcome.

     

    Having said this failing is often the greatest learning experience....but the curiculum and the fact that they want to measure that such and such a fact was taught on such a day would probably exclude that.

     

    I hope that this RPi don't become a boring bit of crap that's just a vehicle to drive some ones idea of curriculum and to make it EASY for teachers to pour the same stuff down everybodys' neck ...At this point you would be better off with a propper real PC that can be got for bugger all 2nd hand

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    There's been some work done by swarren to get u-boot running. I know lots of people don't seem to like u-boot, but regardless. It does get you to a point where you can have a minimal amount of stuff on the sdcard and have u-boot do a network boot from there.

     

    Not sure you can get to the sort of nice boot menus you could do with pxelinux & vesamenu, but it's a step in the right direction at least.