Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum KindleBerry Pi.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 708 subscribers
  • Views 2753 views
  • Users 0 members are here
  • rpi.
  • website
  • that
  • rpi.org
  • raspberry
  • saw
  • on
  • connected
  • the
  • to
  • this
  • pi
  • just
  • morning
  • port
  • usb
  • raspberry_pi
  • and
  • thought
  • be
  • without
  • it
  • do
  • set-up
  • whole
  • would
  • easier
  • i
Related

KindleBerry Pi.

wallarug
wallarug over 13 years ago

I saw this on the RPi.org website this morning and I thought that it would be easier to do the whole set-up just without the Raspberry Pi connected to the USB port on the RPi.

 

I have a Kindle 3 Wi-Fi edition.  An Edumax USB Wi-Fi adapter. A Raspberry Pi.

 

Will this work and if so, ... how would I configure the /etc/network/interfaces file so that I can use wlan0 as an Ad-Hoc Network between the Raspberry Pi and the Kindle?  With the Raspberry Pi with a static IP Address and the kindle (doesn't really matter what IP address - I think).

 

Then, He says something about using the USB keyboard attached to the Raspberry Pi, that should work the same right?

 

I still have to Jail-Break my kindle and install all the hacked software but I though I would raise the Question of the Wireless KindleBerry Pi.

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 13 years ago

    Saw the picture and looks like something interesting to try but I'm not quite cool about screwing up my kindle, well not until a get a new one.

     

    I was very excited with the new Paperwhite but only 2GB bummer, with all the zillion books including technical that are no small and a large collection of datasheets, users manuals, reference manuals, schematics, and other various pdf, 2GB is not enough for me. I've the Kindle keyboard with 4GB with less than 100MB left.

     

    One of the projects I've on my list is to connect the IOIO board to the Rpi and see what can be done. (https://www.sparkfun.com/products/10748)

     

    I'm about to test it soon with the MK802.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to jamodio

    The Instructions are very vauge.

    The first part, connecting the Kindle to the Raspberry Pi is simple enough. Jail break the Kindle , install a terminal emulator like this one and then install UsbNetwork. Make sure the usbNetwork is enable, Connect the devices trough USB, do a quick ifconfig usb0 192.168.2.1 and Voila, I can login into the Raspberry Pi with no problem, using the great display of the Kindle but sadly also using it’s limiting keyboard.

    This would be ideal if you knew exactly what you are doing.  I don't.  I have, though, completed the above with great difficulty.  I will write out some detailed instructions later.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to wallarug

    Those instructions would be great. I have been thinking about buying a Kindle for a while but if I can dual purpose it as a "Pindle" then its def a must have.

     

    Thanks all in this thread its a great idea. Hope it all comes together.

     

    Ray image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to e14 Contributor

    It is hard to get the kindleberry working when the code he gives you is overously wrong.  If someone can get him to fix it, it would make life easier for me.

     

    I got it working but the settings for the "screen" s/ware is not right, I have to type in a few lines of code to get it working.  I will see if I can get a fix for this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scott.pett
    scott.pett over 13 years ago in reply to wallarug

    I've been through the Kindleberry Pi instructions twice and still haven't worked out how to do it.

     

    Jailbreaking a kindle is fairly easy - there are some good instructions here:-

     

    http://www.howtogeek.com/howto/37424/jailbreak-your-kindle-for-dead-simple-screensaver-customization/

     

    Make sure you select the right package for your Kindle - read the list at least twice.

     

    The screensaver hack is also easy and worth doing, to get your hand in for more complicated hacks.

     

    Cheers,

    Scott

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to scott.pett

    The writer of the post needs to fix his instructions so that IT WORKS!!!!!

     

    Currently, He has incorrect code on his site and this is not very good.  DETAILS need to be specified more on his post.  As well as a proper instructions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 13 years ago in reply to scott.pett

    The writer of the post needs to fix his instructions so that IT WORKS!!!!!

     

    Currently, He has incorrect code on his site and this is not very good.  DETAILS need to be specified more on his post.  As well as a proper instructions.