Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum KindleBerry Pi.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 708 subscribers
  • Views 2721 views
  • Users 0 members are here
  • rpi.
  • website
  • that
  • rpi.org
  • raspberry
  • saw
  • on
  • connected
  • the
  • to
  • this
  • pi
  • just
  • morning
  • port
  • usb
  • raspberry_pi
  • and
  • thought
  • be
  • without
  • it
  • do
  • set-up
  • whole
  • would
  • easier
  • i
Related

KindleBerry Pi.

wallarug
wallarug over 13 years ago

I saw this on the RPi.org website this morning and I thought that it would be easier to do the whole set-up just without the Raspberry Pi connected to the USB port on the RPi.

 

I have a Kindle 3 Wi-Fi edition.  An Edumax USB Wi-Fi adapter. A Raspberry Pi.

 

Will this work and if so, ... how would I configure the /etc/network/interfaces file so that I can use wlan0 as an Ad-Hoc Network between the Raspberry Pi and the Kindle?  With the Raspberry Pi with a static IP Address and the kindle (doesn't really matter what IP address - I think).

 

Then, He says something about using the USB keyboard attached to the Raspberry Pi, that should work the same right?

 

I still have to Jail-Break my kindle and install all the hacked software but I though I would raise the Question of the Wireless KindleBerry Pi.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi everyone.

     

    I have spent a couple weeks working on the issues presented in this thread. I'm going to do a writeup! It isn't complete yet, but bear with me. I'm adding photos and videos soon once the writing part is complete.

     

    The title is: Pi k3w – Kindle 3 display for Raspberry Pi

     

    Check it out on Wordpress: http://wp.me/p2k10-4

     

    Enjoy!

     

    image

    Click image for more info.

     

    image

    Click image for more info.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to e14 Contributor

    Great Work!

     

    Are you using wireless on the Kindle and Raspberry Pi? or the USB network?

     

    Did you find that the difficult bit is getting screen to clone on log on via ssh.  I found this very tempermental.

     

    Also, I have not got an Ad-Hoc up and running with the Raspberry Pi and the kindle.  This is becasue I could not get into the /etc/network/interfaces file via terminal on the Kindle - I didn't know how to get a "/" but I have solved that now.

     

    Nice to here someone is also working on this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to wallarug

    Hi Fergus Byrne,

     

    Nope, not using wireless sorry the two photos I posted here exclude the USB cable coming out of the Kindle. Yes I am using USBnetwork Check out the article in the post for lots more detail!

     

    As for difficulties with screen, no I didn't have problems with screen, actually I used a different terminal multiplexer called tmux. The problem was really in the script that Damaru posted though. The script for auto joining the screen session was seriously botched. I found a more elegant solution that works very well. I'm going to complete writing that section of the blog tomorrow if you would like to check back!

     

    Let me know about your progress with wireless. I am pretty sure mobileread forum: http://www.mobileread.com/ has a lot of information about using the wireless. I just haven't looked into it personally. It's next on my todo after getting all of this stuff written image

     

    Did you see my rant regarding the use of about.txt, is that how you figured out the forwardslash? ;D

     

    Thanks for the reply!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to wallarug

    Hi Fergus Byrne,

     

    Nope, not using wireless sorry the two photos I posted here exclude the USB cable coming out of the Kindle. Yes I am using USBnetwork Check out the article in the post for lots more detail!

     

    As for difficulties with screen, no I didn't have problems with screen, actually I used a different terminal multiplexer called tmux. The problem was really in the script that Damaru posted though. The script for auto joining the screen session was seriously botched. I found a more elegant solution that works very well. I'm going to complete writing that section of the blog tomorrow if you would like to check back!

     

    Let me know about your progress with wireless. I am pretty sure mobileread forum: http://www.mobileread.com/ has a lot of information about using the wireless. I just haven't looked into it personally. It's next on my todo after getting all of this stuff written image

     

    Did you see my rant regarding the use of about.txt, is that how you figured out the forwardslash? ;D

     

    Thanks for the reply!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wallarug
    wallarug over 13 years ago in reply to e14 Contributor

    The problem was really in the script that Damaru posted though. The script for auto joining the screen session was seriously botched

    This is what I meant.  The script that was posted did not work.

    Did you see my rant regarding the use of about.txt, is that how you figured out the forwardslash? ;D

    Nope.  I just google it and experimented till I got somewhere.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to wallarug

    I will be updating the article with the script today, and for future reference, the about.txt can give you all of the keyboard symbol combinations so you don't have to try them all!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to e14 Contributor

    Are you the person who did the original KindleBerry Pi that was on the front page?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to wallarug

    Nope, that guy is Damaru! I finished my article today! Check it out: http://wp.me/p2k10-4

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to e14 Contributor

    I will check this later.  Looks good after a quick read.