Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum How do I permanently disable the swap service?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 706 subscribers
  • Views 19963 views
  • Users 0 members are here
  • raspberry
  • raspberry_pi
  • raspberrypi
  • rpi
  • linux
Related

How do I permanently disable the swap service?

Kuya.Marc
Kuya.Marc over 13 years ago

My Device: Raspberry PiRaspberry Pi

 

Situation: Automatic Force-Restoration of Swap service

For some unknown reason, Raspbian OS permanently reloads the swap service at every reboot. Here are the steps I have to do after every reboot:

  1. sudo sync
  2. sudo swapoff -a
  3. sudo apt-get purge -y dphys-swapfile
  4. sudo rm /var/swap
  5. sudo sync

This stop swap, but it's back on a reboot. Writing this list into a script makes the script vanish upon a reboot with swap service activated.

Here are the other attempts I've tried and tried to kill the swap service:

  • sudo update-rc.d dphys-swapfile disable
  • sudo rm /etc/init.d/dphys-swapfile
  • sudo dphys-swapfile disable
  • sudo dphys-swapfile swapoff
  • sudo dphys-swapfile uninstall
  • sudo echo "CONF_SWAPSIZE=0" > /etc/dphys-swapfile
  • sudo rm /etc/dphys-swapfile
  • sudo chmod -x /etc/init.d/dphys-swapfile

All attempts to kill the swap service failed! Upon a reboot, a 100MB swapfile is restored and activated.

Anyone have a working solution?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    If you take away execute permissions from scripts in /etc/init.d they will not run in any runlevel.  So maybe you did not quite hit the right order of things.

     

    sudo chmod -x /etc/init.d/dphys-swapfile

    sudo swapoff -a

    sudo rm /var/swap

     

    Then and after reboot free shows 0 swap.

    efflandt@raspberrypi ~ $ ls /var

    backups  cache  lib  local  lock  log  mail  opt  run  spool  tmp

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Kuya.Marc
    Kuya.Marc over 13 years ago in reply to e14 Contributor

    Hi David,

     

    Actually, the problem is with the Element14 SDCardElement14 SDCard, itself. It mysteriously becomes read-only after a month of use.

     

    Marcos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Kuya.Marc
    Kuya.Marc over 13 years ago in reply to e14 Contributor

    Hi David,

     

    Actually, the problem is with the Element14 SDCardElement14 SDCard, itself. It mysteriously becomes read-only after a month of use.

     

    Marcos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Kuya.Marc

    I guess one other thing that should be done to avoid an error when symbolic links in runlevels try to run dphys-swapfile when it no longer has execute permission is to remove the symlinks with:

     

    sudo update-rc.d -f dphys-swapfile remove

     

    Can you still flash a new image to an SD card that became read-only?  If not, make sure that the little write protect switch on left side of SD is pushed away from you towards the contacts.  Some people have also had that issue of flash memory becoming read only in Ubuntu PC Linux, but I never have.  I did corrupt an SD card while overclock testing a Pi, but have never had any SD or other flash memory ever fail to the point that it could not be reflashed or formatted.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    > make sure that the little write protect switch on left side of SD is pushed away from you towards the contacts.

     

    I don't think this would help at all, since the RPi hardware doesn't connect up

    the write-protect switch, as noted here:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=29&t=10775&start=1

     

    One user suggests editing /etc/fstab to make the file system readonly:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=29&t=10775&start=9