Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry pi usb output from GPIO
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 707 subscribers
  • Views 9772 views
  • Users 0 members are here
  • raspberry
  • python
  • from
  • pi
  • gpio
  • hardwarehacking
  • hid
  • program
  • programming
  • usb
  • raspberry_pi
  • raspberry-pi
  • raspberrypi
Related

Raspberry pi usb output from GPIO

e14 Contributor
e14 Contributor over 12 years ago

I've had this idea and I've googled a lot to find out if it would be possible to attatch usb cable to raspberry pi's GPIO pins. I already got an old usb cable and cutted the other end off and i tought that I just attatch the vireing to GPIOs and plug other end, whitch have still the USB A port on it, to computer and I would be able to control all data.  I mainly am trying to program it to act as HID device.... Is there any python lybrary or can i just somehow output the raw data in bytes? How would i be able to do it?image

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 12 years ago

    Unless you can write kernel drivers for the RPI then you won't be able to do it.

     

    People have written (very poor performance - a hardware issue - not because their code isn't clever) USB code for some Atmel AVR processors which works by bit banging GPIO - have a look at that to get and idea of what you are attempting. And read the USB spec - it's free.

     

    V-USB - A Firmware-Only USB Driver for Atmel AVR Microcontrollers

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelkellett

    I need to write own kernel drivers???? Seriously? To control USB data with GPIOs? Why do I need usb drivers to control GPIOs?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelkellett

    I need to write own kernel drivers???? Seriously? To control USB data with GPIOs? Why do I need usb drivers to control GPIOs?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 12 years ago in reply to e14 Contributor

    Did you read the USB spec or look at the AVR examples?

    You are trying to emulate a USB device with GPIO - that means that you must support the USB timing without the aid of any dedicated hardware, you have to serialise/deserialise at a minimum rate of 1.5Mbit/s (12 or 400 for full speed or high speed). You can't afford an interrupt during a data transfer even at the lowest speed. The only way you might be able do this is to take complete control of the processor.

     

    If  you want additional USB connectivity on an RPi then consider using one of the FTDI chips which can be controlled via GPIO, UART or SPI ports.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelkellett

    Thanks a lot for this information and thanks for fast reply. I'll maybe create own drivers. And i checked the v-usb's github repository

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 12 years ago in reply to e14 Contributor

    The practical answer is: it is not physically possible: You need USB-hardware in the chip to be able to do what you want.

     

    Now, some fool managed to implement something for AVR in software that sort-of works. Normal hardware always implements the 12mbps mode of USB. The avr-software one only implements the 1.5mbps mode. If you want to do "HID" that's fine, but for other usb-standard-slave-devices, the standard specifies "at least 12mpbs". Some hosts don't mind and will allow such a function on a slow device, but others wiill enforce the standard.

     

    Getting the software-USB working on raspberry pi is a whole lot of trouble that is not worth it. There are many other more sensible ways to create a communications channel between your PC and the raspberry pi.

     

    The things you can easily get to work right niow are: ethernet and "serial". Get an USB-ttl-level-serial converter make sure the levels are 3.3V, and wire it up. Standard baud rates can go up to 115200bps, but both the USB-serial and the raspberry pi can go higher (but it's usually not worth the trouble)