Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry pi powersupply change from micro usb to dc power plug
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 708 subscribers
  • Views 1489 views
  • Users 0 members are here
  • raspberry
  • pi
Related

Raspberry pi powersupply change from micro usb to dc power plug

e14 Contributor
e14 Contributor over 11 years ago

Hi!

As topic suggests I want to change the powerconnection from the flimsy micro usb to a sturdy dc power plug.

Is this doable?

 

I was thinking something in the line of DC kontakt 2,5 mm chassi > DC-kontakter | Kjell.com

 

Thanks in advance

  • Sign in to reply
  • Cancel
  • Problemchild
    Problemchild over 11 years ago

    Not on the board since you have no provision for it there.

    You could however have make a micro USB to DC socket fly lead to do this.

    Easiest way to do this would be to get a micro USB lead cut off the unused end and solder the power connections on to the DC socket.

     

    Personally I wouldn't bother unless you have a specific reason the micro USB is pretty tough after all it's what phones use every day for years on end!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago

    Could a small board be made that plugs onto the GPIO header and provides power to the 5v pins on there?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Problemchild

    Thanks for the fast reply.
    The reason i want to change the connector is that i'm planning on building the pi into an old genesis/mega drive. And i'm afraid that moving the console will break the power supply.

    Also it looks more authentic =)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bbolo1
    bbolo1 over 11 years ago

    I have built a small buck power supply (using LM2596) that can take input voltages (through a DC connector like in here DC kontakt 2,5 mm chassi > DC-kontakter | Kjell.com) from 4V up to 40V.

    The PSU is built onto a small PCB which is mounted on a couple of plastic risers (~1.5cm in height) tight with screws on the 2 mounting holes of the RPI.

    Since this PSU can supply 5V and 3A, all the power supply issues that used to appear when using a phone charger as a PSU (5V/700mA) and USB hot-plug have disappeared.

    Now, I can plug into the USB even external 2.5" hard-drives with no danger of a brown-out reset of the RPI. For me, this solution works best.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to gadget.iom

    Hi Paul,

     

    Yes that is possible, it worked for me. However,I only tried on a RPI B model (and I don't know which one, they had all that trouble with polyfuses etc a while back and had another 'B' revision) and things may have changed again for the B+. I think it should be feasible, but I'm just not sure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to shabaz

    I might investigate the feasibility of designing one with a 7805 regulator etc.

    I do share Robins concerns over durability of the Micro-USB connector I would expect the 26/40-Pin header to withstand slightly more abuse..