Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is the Raspberry B+ GPIO passed through with the Cirrus Audio card?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 709 subscribers
  • Views 5306 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Is the Raspberry B+ GPIO passed through with the Cirrus Audio card?

gkzsolt
gkzsolt over 11 years ago

The previous Wolfson card has a 26 pin header with male pins to connect to the Raspberry GPIO header after pushed on top of it. Does the new audio card do the same for the 40 pin header? Sorry, but I cannot discern from the card images I have.

  • Sign in to reply
  • Cancel
Parents
  • fvan
    fvan over 11 years ago

    There is a table in the user manual with the remaining I/O on the expansion header.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • tonyhansen
    tonyhansen over 11 years ago in reply to fvan

    In this table (e), pins 16-20 are ALL described as "General Purpose Pin GPIO 3", which looks to me like a copy/paste error from the pin 15 description.

     

    It would be nicer if table (e) were to read:

     

    PinNameType

    Power

    Domain

    Description
    17GPIO6_EXDigital In/Out0 - 3.3VRPI General Purpose Pin GPIO6 (RPI pin 31)
    18GPIO12_EXDigital In/Out0 - 3.3VRPI General Purpose Pin GPIO12 (RPI pin 32)
    19GPIO16_EXDigital In/Out0 - 3.3VRPI General Purpose Pin GPIO16 (RPI pin 36)
    20GPIO26_EXDigital In/Out0 - 3.3VRPI General Purpose Pin GPIO26 (RPI pin 37)

     

     

    However, there are discrepancies between this table (e) and the description within the schematic that need to be figured out.

     

    Pins 10 and 11 are flipped between the schematic and table (e). (In the schematic, pin 10 is listed as PDMOUT_DAT [3] while table (e) says pin 10 is SDA. And vice versa for pin 11.) Which is correct?

     

    In the schematic, pin 14 is listed as connected to "GPIO5_EX [7]", which SHOULD correspond to PI GPIO 5 (PI pin 29). However table (e) lists pin 14 as being GND. Which is correct?

     

    In the Cirrus Logic Audio Card Comparison Table, it says that there are 8 PI connections (including the UART). The UART is connected to the Cirrus J8 Header. (RPI pins 8&10)

     

    Can anyone confirm definitively which are the other two GPIO pins that are tied directly from the PI into the Cirrus expansion header?

     

    • Expansion header pin 15 and 16 are marked GPIO4 and GPIO3, but those appear to be connected to GPIO4&3 on the WM5102_CSP137 chip instead of the RPi GPIO pins.
    • Pin 14 might be one of them if the schematic is correct but table e is not.

     

    Any definitive clues?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gkzsolt

    In Windows the pdf CLAC user manual also not text searchable (it searches only in small parts of text like tables and command examples).

    Yes, and looks like there is nothing relevant to your question in the manual, any way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tonyhansen
    tonyhansen over 11 years ago in reply to gkzsolt

    Zsolt Gere Kiss wrote:

     

    Hi Tony,

     

    No, I am not making the assumption that the SPI bus pins are exposed. I know they are not, and that is what makes me wonder: why have the designers decided to hide them? In general, there should be no reason for that, except in some (unusual) cases.

    In the schematics I see these 4 pins (MIS, MOSI, SCLK, SS) routed to the corresponding CIF2XX on the WM5102 chip (the RPI pins enter into IC U8, what seems to be a level shifter). From this I conclude that they are used for their purpose, in an SPI protocol and not been "reassigned to other uses", if you meant that. This also means that they can be used for other devices too (except SS). All SPI devices in a module share the same bus pins, ignoring them if their SS slave select pin is not active. So the question remains.

    (I could go and try this with some experiments, but I don't have a Cirrus card yet. I am trying to figure out if it is worth buying one.)

    May I ask if you could search through the "Cirrus Logic Audio Card User Manual.pdf"?

    I agree very much with you in that a Cirrus card takes a lot of RPi's resources. But what worries me more, is the quality of documentation (very poor) and the lack of support. Is somebody at Cirrus reading and taking notice of these discussions? Or is there a place we can show some of these to a competent personnel (thinking of your table, etc.) ?

    I cannot speak for the Wolfson designers - I don't know why they made some of their trade offs. I think they've heard loud and clear, though, that GPIO access is important to RPi designers.

     

    However, their bottom line design rule appears to have been to provide access to a high-quality audio board. Everything else seemed to be secondary for them.

     

    If that's your highest priority, as it was mine, then the answer is clear. If something else is more important, then your mileage will vary.

     

    Searchability of PDF files is entirely dependent on the tools used when they are built. These do not appear to be searchable. But they are perfectly valid PDF files.

     

    A number of people have asked similar questions to what you're asking. There's no consensus on any answers yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to tonyhansen

    I have put together a complete table to capture the 26/40 way pins for the B and A+/B+ and the use of these pins on both the Wolfson and Cirrus cards. Hopefully this helps bring the information together and highlights the functions and availability of pins on the card. If there are any comments or feedback on the information please provide here, I think this will be useful based on the questions in the forum so I will pass the information on to E14 with the aim of adding to the user manual.

     

    26/40 Way Pin allocation and function

    P1 PinNameModel BModel A+ /B+
    GPIO (BCM)WAC FunctionGPIO (BCM)CLAC Function
    13V3 Power
    25V0 Power
    3SDA1GPIO2WM8804 I2C - SDAGPIO2WM8804 I2C - SDA
    EXP/11
    45V0 Power
    5SCL1GPIO3WM8804 I2C - SCLKGPIO3WM8804 I2C - SCLK
    EXP/9
    6Ground
    7GPIO_GCLKGPIO4WM5102 MCLK2 (unused)
    WM8804 MCLK (unused)
    GPIO4WM5102 MCLK2 (unused)
    WM8804 MCLK (unused)
    8TXD0 (UART)GPIO14J8/1GPIO14
    J8/1
    9Ground
    10RXD0 (UART)GPIO15J8/2GPIO15J8/2
    11GPIO_GEN0GPIO17WM5102 RSTGPIO17WM5102 RST
    12GPIO_GEN1 (PCM_CLK)GPIO18WM8804 - I2C Address ConfigGPIO18WM5102 AIF PCM - BCLK
    13GPIO_GEN2GPIO27WM5102 IRQGPIO27WM5102 IRQ
    14Ground
    15GPIO_GEN3GPIO22WM5102 LDO EnableGPIO22WM5102 LDO Enable
    16GPIO_GEN4GPIO23WM8804 - Control I/F ConfigGPIO23WM8804 - Control I/F Config
    173V3 Power
    18GPIO_GEN5GPIO24WM5102 GPIO5 (unused)GPIO24WM5102 GPIO5 (unused)
    19SPI_MOSIGPIO10WM5102 SPI - MOSIGPIO10WM5102 SPI - MOSI
    20Ground
    21SPI_MISOGPIO9WM5102 SPI - MISOGPIO9WM5102 SPI - MISO
    22GPIO_GEN6GPIO25WM5102 GPIO3 (unused)
    EXP/16
    GPIO25WM5102 GPIO3 (unused)
    EXP/16
    23SPI_SCLKGPIO11WM5102 SPI - SCLK1GPIO11WM5102 SPI - SCLK1
    24SPI_CE0_NGPIO8WM8804 RSTGPIO8WM8804 RST
    25Ground
    26SPI_CE1_NGPIO7WM5102 SPI - CEGPIO7WM5102 SPI - CE
    27ID_SD GPIO0EEPROM
    28ID_SC GPIO1EEPROM
    29GPIO5 GPIO5EXP/14
    30Ground
    31GPIO6 GPIO6EXP/17
    32GPIO12 GPIO12EXP/18
    33GPIO13 GPIO13WM8804 - I2C Address Config
    34Ground
    35GPIO19 (PCM_FS) GPIO19WM5102 AIF PCM - FS
    36GPIO16 GPIO16EXP/19
    37GPIO26 GPIO26EXP/20
    38GPIO20 (PCM_DIN) GPIO20WM5102 AIF PCM - DIN
    393V3 Power
    40GPIO21 (PCM_DOUT) GPIO21WM5102 AIF PCM - DOUT
    Note: Unused functions need to be treated carefully. Although they are not enabled in the current driver
    they provide scope for increased functionality going forward.

     

    P5 Connector (Model B Only)
    PinNameModel B
    15V0 Power
    23V3 Power
    3PCM_CLKGPIO28
    4PCM_FSGPIO29
    5PCM_DINGPIO30
    6PCM_DOUTGPIO31
    7Ground
    8Ground

     

    Based on Tony's table of the 8 available GPIOs, I have updated this to include additional information. To clarify the 8 referenced available GPIO are numbers 6 to 13 in the table. I2C and SPI are functions utilised on the card so these can not be changed for other functions.

    Cirrus Logic
    Audio Board
    Pin
    RPi GPIO
    Description
    RPI Alternate
    Description
    RPi pin
    1EX 9GPIO 3SCL I2C5
    2EX 11GPIO 2SDA1 I2C3
    3J9-19GPIO 10SPI_MOSI19
    4J9-21GPIO 9SPI_MISO21
    5J9-23GPIO 11SPI_SCLK23
    6EX 14GPIO 5 29
    7EX 16GPIO 25 22
    8EX 17GPIO 6 31
    9EX 18GPIO 12 32
    10EX 19GPIO 16 36
    11EX 20GPIO 26 37
    12J8-1GPIO 14UART TX8
    13J8-2GPIO 15UART RX10
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Thank you, Scott, it looks great and very helpful!

     

    "Although they are not enabled in the current driver they provide scope for increased functionality going forward."

    Does it mean I can use those "unused" GPIOs as is, or I need to hack kernel driver somehow to make them free for using?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gkzsolt
    gkzsolt over 11 years ago in reply to e14 Contributor

    >  Does it mean I can use those "unused" GPIOs as is, or I need to hack kernel driver somehow to make them free for using?

     

    I guess it means that you could use them now as is, if you'd want this very much, but you are not advised to do so, because they can be used some time in the future (drivers), for "increased functionality going forward" image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gkzsolt
    gkzsolt over 11 years ago in reply to e14 Contributor

    Scott, many thanks for this and for passing the information on to E14. Could you pls. correct "SCL I2C" in the table to "SCL1 I2C"? (there are 2 I2C interfaces on the RPi, and that is from intf. 1)

     

    Also, if you could ask E14 to generate the doc pdf-s as for them to be searchable, it would be great. I don't think this to be too complicated, but the current manual is very, very hard to use. You cannot search any text, but neither can you copy and paste most of them, should it be a link, for example (text in tables *is* searchable, but normal text is not). I had to manually enter the (long) link from Annexe 7 d. of the "Schematic diagram" (have to enter this as well;), and on top of that, as I remember it was wrong, linking to the schematic of the Wolfson audio card! So please, can somebody at Cirrus check the links validity as well? Thanks,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gkzsolt

    If so, I'm happy to hear that! It solved half of my alleged problems. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gkzsolt
    gkzsolt over 11 years ago in reply to e14 Contributor

    Scott,

     

    Your table suggests that the SPI control pins are still exposed through a header called J9. While this is good news, I am sorry to not find this header on the Cirrus schematics. Maybe I've missed it, but if not, would you be so kind to ask them for an update?

     

    Thanks,

      Zsolt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tonyhansen
    tonyhansen over 11 years ago in reply to e14 Contributor

    Thank you for posting this table, Scott.

     

    It took me a while to realize how to interpret your references to the SPI functions on the J9 header. (J9 is the name for the 40-pin connector from the Cirrus board to the RPi J8 40-pin header.)


    The actual pins are NOT easily connected to, as they require you to use either: a shim connector between the two boards, or resoldering the pins.

     

    Nonetheless, the data IS important in that it confirms that the SPI pins ARE indeed being used for SPI and haven't been used for some other GPIO purpose.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gkzsolt

    I have some comments about using "semi free" or "unused" GPIOs of Cirrus Logic AC. I mean GPIOs 04, 24, 25, and 27.

    In my project I use RPi with CLAC and SleepyPi to make battery powered field recorder for animal sounds. To make possible these three boards be connected I had have to make an adaptor from Exp. header of CLAC to Sleepy. To managing power of Rpi Sleepy needs GPIOs 24 and 25. 25 is present in CLAC Exp. header, so at the beginning I wanted to use it as is. But it didn't work, and when I checked voltage on this pin, my multimeter showed 0.7V, but not 3.3V. I measured this pin voltage in all combinations of boards (I have Rpi B+, couple of RPi A+, two CLACs and two Sleepy Pi) - results were the same. On Rpi without audio card and normal Raspbian loaded, those GPIOs of course had 3.3V when I switched them to High. Finally I have used "true free" pins from Exp. header, and everything is working properly.

     

     

    Thus, these pins (at least 25th), it seems, can not be used as normal GPIOs, despite the fact that they are unused in this version of the CLAC driver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gkzsolt

    I have some comments about using "semi free" or "unused" GPIOs of Cirrus Logic AC. I mean GPIOs 04, 24, 25, and 27.

    In my project I use RPi with CLAC and SleepyPi to make battery powered field recorder for animal sounds. To make possible these three boards be connected I had have to make an adaptor from Exp. header of CLAC to Sleepy. To managing power of Rpi Sleepy needs GPIOs 24 and 25. 25 is present in CLAC Exp. header, so at the beginning I wanted to use it as is. But it didn't work, and when I checked voltage on this pin, my multimeter showed 0.7V, but not 3.3V. I measured this pin voltage in all combinations of boards (I have Rpi B+, couple of RPi A+, two CLACs and two Sleepy Pi) - results were the same. On Rpi without audio card and normal Raspbian loaded, those GPIOs of course had 3.3V when I switched them to High. Finally I have used "true free" pins from Exp. header, and everything is working properly.

     

     

    Thus, these pins (at least 25th), it seems, can not be used as normal GPIOs, despite the fact that they are unused in this version of the CLAC driver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks for the feedback. We believe we have discovered and resolved the cause of the problem in the 3.18 driver which has been just been released. The GPIO pin of the WM5102 was incorrectly configured as an output, in the 3.18 driver this is now configured as an input. This issue was stopping the use of GPIO25 from the Pi as reported by Ivan W.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Correct me if I'm wrong, but from reading this thread it seems like one needs to use (some of) the 20 Expansion Header pins for GPIO access.

    If this is the case is there a recommended 2 x 10 pin ribbon cable ?

     

    Thanks