Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Interface old laptop camera with RasPi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 676 subscribers
  • Views 999 views
  • Users 0 members are here
  • raspberry
  • pi
  • raspberry_pi
  • raspberry-pi
  • camera
  • webcam
Related

Interface old laptop camera with RasPi

Former Member
Former Member over 11 years ago

Hey guys,

 

I have recently salvaged two old laptops and got my hands on two webcam modules, but I cannot find out the pinouts for these modules.

1. How could I determine which connections are which without destroying the modules ??

2. Does anyone have information on the pinout of these devices ??

 

I am suspecting that the modules are directly connected as a usb device so the pinouts would be vcc, gnd, d+, d- and nothing for the 5th pin. On the second module the connections should be the same, but there is a smd led looking thing sticking through the copper tape and maybe the 5th connection could be the power line for the led. Just a thought.


Pictures of the modules:

image

image

The numbers on these modules are:

 

#1: CNF6037

#2: GD M812

 

Any help is appreciated, since I am not so knowledgable in electronics it would be really cool if I could learn about finding out about the pins.

 

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    0 Problemchild over 11 years ago

    Yes the majority are in fact USB cams, to be honest a lot of the other peripherals on the laptops such as Keyboards and touch pads are also USB.

    They obviously must have the chipsets for the desktop peripherals and there is simply no point in having silly custom interfaces.

     

    As far as pin outs are concerned I think you need to apply some intelligent guess' for the ground and power then from there look for the D+,D-

     

    This stuff is good for robot use as well!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 11 years ago

    Yes the majority are in fact USB cams, to be honest a lot of the other peripherals on the laptops such as Keyboards and touch pads are also USB.

    They obviously must have the chipsets for the desktop peripherals and there is simply no point in having silly custom interfaces.

     

    As far as pin outs are concerned I think you need to apply some intelligent guess' for the ground and power then from there look for the D+,D-

     

    This stuff is good for robot use as well!