Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Questions about the Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 704 subscribers
  • Views 336 views
  • Users 0 members are here
  • raspberry
  • pi
  • connector
  • hdmi
  • quesion
  • about
  • raspberry_pi_getting_started
Related

Questions about the Raspberry Pi

freddruppel
freddruppel over 12 years ago

Hello everyone !!!

 

I have a question about the raspberry pi : Is it possible to desolder the HDMI connector from the Raspberry Pi and extend it with wires ?

My Pi model is "Raspberry Pi model B rev 2.0".

 

Thank you for your answers !!!

 

Regards, Frédéric Druppel

 

 

 

 

P.S.: Feel free to correct my English if needed !!! image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello sir,

    From looking at the HDMI port on the board it looks like it would be difficult because the ground shielding is soldered into the board with lead solder and the pins are very small. It may be possible though if you had a high temperature soldering iron that could melt the lead free solder and a very small soldering tip so you could re-solder the pins properly. Also it will work better if you do not use lead free solder to solder  your wires and after the wires are soldered to the port and the board cover the connections with hot glue to prevent shorts.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello sir,

    From looking at the HDMI port on the board it looks like it would be difficult because the ground shielding is soldered into the board with lead solder and the pins are very small. It may be possible though if you had a high temperature soldering iron that could melt the lead free solder and a very small soldering tip so you could re-solder the pins properly. Also it will work better if you do not use lead free solder to solder  your wires and after the wires are soldered to the port and the board cover the connections with hot glue to prevent shorts.image