Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Strange screen artifact
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Subscribers 712 subscribers
  • Views 3746 views
  • Users 0 members are here
  • raspberrypi
Related

Strange screen artifact

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I have 3 Pies

#1  1x Model B with 2 USB ports

#2  1x Model B+ with 4 USB ports

#4  1x Pi2  (there is only one model, right?)

 

I have used all 3 to run Openelec.

#1 works perfectly

#2 and #3 also run openelec but they both show an artifact on the top right-hand corner. It seems to be a miniature version of the colour screen that is shown right after the Pi wakes up but before it runs an OS.

 

Has anyone else seen this????

 

Cheers,

Nick

image

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    It's a low-power warning. It shows up when the 5V supply goes below 4.65 if I remember correctly.

    http://www.raspberrypi.org/forums/viewtopic.php?f=29&t=82373

     

    --

    Ragnar

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thank you very much Ragnar!!!!!

    That's exactly what was happening.

     

    I've had issues many years ago with crappy USB leads, so I started buying one at a time from different ebay vendors until I found one that had cables that could carry 2,000 mA and then I bought a dozen or more from him, tested them each and gave most of them to my friends who were complaining about slow charging times.

    (I also bought a bunch for myself)

     

    So, when I saw your message, I collected a few of my 5V, 2,000mA power packs and tested them (as well as 2 different cables) with the Pi2.

    Voila!!!

     

    One substandard cable in the bin later and the Pi is happy.

     

    Thanks again,

    Nick

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royleith
    0 royleith over 11 years ago in reply to e14 Contributor

    @ Nick

     

    I don't think it is as simple as low capacity power supplies or poor USB leads. In fact, I think the leads either work or don't work. I don't think they have much chance of going high enough resistance at the sorts of current taken by the Pi to stop it working correctly.

     

    Anyway, here's my practical experience. I was getting freezes and a loss of USB with my Pi2 and found that transferring the mouse/keyboard and wifi dongles to a hub powered from the same dual USB PSU as the Pi, solved the problem. I had noticed the rainbow square at times, but not related it to power.

     

    Recently, I decided to try the dongles plugged straight into the Pi and it was fine. The reason was that the (cheapo)  hub supplied power over its USB ports as long as the power was connected and that fed back to the Pi and supplemented the 5V rail. It also lights the red LED even if the Pi is not powered up.

     

    I unplugged the hub from the Pi and rebooted. It worked well, but every time it communicated over the wifi dongle (a very cheap, very short device that probably has to work at full power) the warning rainbow square faded in and out.

     

    The key points are,

     

         1) The hub and the Pi are getting power from the same PSU and so it is not a problem with the power supply lowering the 5V rail under load.

         2) It is unlikely to be a high resistance power lead. I just don't accept that two leads in parallel solve the problem.

     

    The most likely problem is that the internal power arrangements for the Pi are not able to supply the peaks of load from the cheap wifi dongle. It's well known that Wifi is a significant drain of mobile device power, but it will take a bit of pfaffing about with USB PCB sockets and soldered wiring to find out how much this particular dongle is drawing. I may try with an up-market, slightly longer dongle to see if it draws less power, but that needs the IP blacklist on my router to be modified so I am in no rush.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to royleith

    Hi Roy,

    Thanks for the information!

     

    Alas, in my case, I have actually found USB leads in the past that vary a lot, as far as how much current they can carry. (This was done as part of a phone-charging issue....)

    It took me a while to find ones that could carry (very close to ) 2A.

     

    In the case of my Pi, replacing the lead and 5V supply helped fix the rainbow problem. I noticed that just changing the cable made the rainbow appear for a while, fade away, come back and so on....indicating brief outages, as opposed to consistent low-voltage. Once I also changed the PS fixed, it all went away.

     

    I am using a wired-LAN connection, instead of WiFi, so that is not causing me any issues.

     

    If this Pi was used in a critical application, I'd have looked for a nice, regulated 5V supply but, since it is only used as a media center and it works reliably, I'll keep using the little powerpack I have,

    I've got a lot on at the moment, developing software for paying clients, so my hardware itch of getting the multimeter out and measuring resistance in various USB cables, as well as output voltages from the various powerpacks, has been put on hold!

     

    Thanks again,

    Nick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to royleith

    OHMS LAW my dear friends OHMS LAW.

     

     

     

    On the newer versions of the Raspbian, there is a core feature that measures the onboard voltage and if it is detected below a set point then the little rainbow square shows up on the top right of the screen, you PI may not crash but it might

     

     

     

    USB Cables come in all sorts of grades and by that I mean how thick the wires are in the cable, under light loads the drop across the cable can be low due to a lower current, as you start spinning up applications or adding load in the form of USB devices plugged directly into the PI, the current increases and therefor the voltage drop increases, I have shown this specifically through experimentation and presented the readings in my post. THE CABLE MATTERS.

     

     

     

    I agree that based on your observations, the power adapter is not lightly to be the issue if everything works when the hub is powered via a separate cable from the power adapter than that of the PI and if you read my blog post on the matter you will see that in all the testing I performed it was never the PSU wall wart.

     

     

     

    Cheap USB hubs that back feed to the PI should not be used especially if the PI is also powered from its own power input, the two can interfere with each other and cause problems, use a better quality HUB.

     

     

     

    Your experience with the WIFI adapter proves my point, as you start to use things  like the WIFI, power consumption goes up (WIFI adapters and most other devices to not consume the same power all the time, it goes up and down depending on how much your asking them to do)

     

     

     

    Powering the PI through a Keyboard USB outlet of from the standard PC USB port may work for low loads but these USB interfaces are nearly always limited to 500mA, not even close to that needed by a busy PI

     

     

     

    Technically two leads in parallel could solve your problem, although impractical the technical result of two resistors in parallel is lower resistance and therefor lower voltage drop for the same current flowing through. In your case it is not really two leads in parallel, one lead is powering the HUB and the connected devices, the other lead it powering the PI, if you have a non-compliant HUB that back feeds to the PI then you will get a partial parallel effect but this is not why it is working better. It is because lower current is flowing in each cable and therefor lower losses before the power gets to the device (PI or HUB)

     

     

     

    You need a Power adapter rated at 1.5A or more for the PI, especially if your adding loads of USB devices, the overall load on the PSU does not change if you separate the load over to cables, you just reduce the risk of dropping too much volts to the PI

     

     

     

    PI 2 will require more power when up and running due to quad core etc. etc. If you still have keyboard, WIFI, and other devices attached, consider a HUB for them and use a 2A Adapter with GOOD quality cables

     

     

     

    I said it at the top and Ill say it again “THE CABLE MATTERS”

     

     

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royleith
    0 royleith over 11 years ago in reply to Robert Peter Oakes

    Yeah, yeah, yeah: whatever!

     

    So, I decided to do some measurements.

    I measured the round loop resistance of the 1 metre USB cable currently in use, using a component tester. The power pins were short-circuited at one end and the resistance measured between the pins at the other.
    Round loop resistance of the lead = 0.6 Ohms
    Then I measured a full sized Type A to Type B USB cable of 1.8m. Resistance = 0.6 Ohms.
    I measured my current PSU (see what I did, there?) and it measured 5.120 Volts, The previous Belkin high power PSU measured 5.136V.
    I connected a USB cable to one of the Raspi USB ports and measured the voltage at the other end with a digital meter.
    • No USB Devices and with the Raspi idling             Vout = 4.904V
    • With Mouse/Keyboard USB Dongle                        Vout = 4.879V
    • With above and idle WiFi Dongle                            Vout = 4.85V
    • With active web-page download                             Vout = 4.764
    Using Ohm's Law of Volts = Amps x Resistance
    • Voltage Drop of idle Raspi2        = 0.27V   @ 0.6 Ohms                  Current = 450 mA
    • Voltage Drop of m/Keyboard     = 0.025V  @ 0.6 Ohms                  Current = 41.7 mA
    • Voltage Drop of keyb +idle WiFi = 0.029V  @ 0.6 Ohms                  Current = 48.3 mA
    • Voltage Drop of WiFi surfing       = 0.083V  @ 0.6 Ohms                  Current = 138.3 mA
    Lowest Voltage during booting - 4.705 Average 4.772V
    So, with the keyboard and WiFi dongle plugged in and surfing going on, the maximum current draw is around 630 mA. Although the USB voltage under these conditions is nominally around 4.772V it is quite likely that it dips below the warning level. The 'Rainbow Square' appears at around this 4.772V point.
    The micro USB lead has a skinny cable, but the full sized lead has a large diameter cable. Nevertheless, they both have the same resistance which means that even a 'heavy duty' micro USB cable of 1.8m will be no better. Even with the modest additional load of the WiFi and keyboard/mouse USB dongles, the Pi2 is maxed out. Using the two remaining ports is only possible with self powered USB devices.
    Before this test, I had already Ebayed for a USB lead with a stout 'Charger' cable. Fortunately, I went for the cheapest which was only 1m long.  With any luck it should come in at something like 0.4 Ohms. However, the message to take away from all this is that 'SIZE MATTERS'. Get the very shortest USB power lead you can use between the power supply and the Raspi. The leads to the four USB ports are not so important as they carry less current. If you have high powered USB peripheral devices they should be self powered or driven from a powered hub, but we knew that anyway.
    The half meter 'charging' cable I found on Ebay would be good and I found one example at a quarter of a meter that should be better still. However, that is cutting it a bit fine in my circumstances. If you can bring a mains patch board or extension cable near to your Raspi, the 1/4 meter cable would be perfect.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 11 years ago in reply to royleith

    My phone definitively likes the 10cm micro USB cable better than the 25cm one. (When depleted, it will charge a little, try to boot, and shut down repeatedly unless the charger is my 20000mAh battery pack and the cable is the 10cm one....Everything else repeats the loop.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royleith
    0 royleith over 11 years ago in reply to royleith

    I have new information to add on the cable front.

     

    I purchased 1m 'Charging and Data' cables before my previous test. The new cables were wimpier than the old ones despite the illustration suggesting otherwise, but actually worked somewhat better. After the test, I purchased 0.5m cables and 0.25m cables all sold as 'Charging and Data' cables.

     

    I have now tested their loop resistance. The values are at the limit of my tester and so are somewhat of a guide.

     

    Old 1m cable    0.6Ω

    New 1m cable   0.6Ω

    0.5m cable        0.2-0.3Ω over a number of measurements

    0.25m cable      0.2Ω

     

    The wire gauge of the old cable was not shown, but all three of the new cables were marked 28AWG. I suspect the cable came from the same cable factory even if the assembly factories were different.

     

    The quality of my short-circuit was not great (a screw-driver gently inserted into the micro USB plug). I know that this could easily have added up to 0.05Ω if not more and so the accuracy of the results drops quickly with the length of the cable. All the measurements were taken several times and only the 0.5m cable showed any variation.

     

    The conclusion is that a 1m USB power cable is likely to be on the verge of causing the rainbow square voltage warning when wireless and wifi USB dongles are used. Use a powered hub if using a cable of 1m or above, although you might just get away with a good 1m cable with some devices.

     

    I am using a 0.5m cable without any signs of problems and without a powered hub. You might well be able to use all four USB ports as long as power hungry devices are not involved. A 0.25m cable does not give a significant advantage over a 0.5m cable, but might still be useful in some circumstances as when running off a mobile device charging battery. As the battery pack discharges and the output voltage drops, the shorter cable might give you a useful extension in operational time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to e14 Contributor

    If you look carefully at USB cables you will find that they are marked with the gauge of wire they use. Although they vary slightly it is usually in the form of something like: 28AWGx1P+26AWGx2C.

    This means they are using 28 AWG wire for the data connections ( 1 pair) and 26 AWG wire for the power pins. One thing I have noticed, and it seems to be fairly consistent is that longer cables (2 m)

    tend to use smaller gauge wire (30AWGx1P+28AWGx2C is typical) than shorter (0.5 m) ones. This means that shorter cables have two obvious advantages when they are used for providing power, they

    use larger wire which can handle more current, and they have less resistance because they are shorter.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to gdstew

    I have found in my investigation and as published in my post that most cables don’t even bother to mention what the wire gauge is, these ones tend to be the under rated ones

     

     

     

    I found the best way to get a good cable is to use a USB “A” type connector and replace the end with the micro connector of choice, these older cables have proven so far to consistently have better gauge wiring in them

     

     

     

    A point of interest is the typical resistance and current rating of the popular gauges

     

     

     

    This is from the American Wire Gauge Standards + some math of my own

     

     

     

     

    1Amp Load

     

                               

     

     

     

               

     

     

     

     

     

     

     

    Current

     

    1ft USB Cable

     

    1M USB Cable

     

    6ft USB Cable

     

     

    AWG

     

    Ohm/M

     

    Ohm/Ft

     

    Chassis

     

    Transmission

     

    V Drop

     

    LOAD Volts

     

    V Drop

     

    LOAD Volts

     

    V Drop

     

    LOAD Volts

     

     

    22

     

    0.05296

     

    0.01614

     

    7

     

    0.92

     

    0.03228

     

    4.96772

     

    0.10592

     

    4.89408

     

    0.19368

     

    4.80632

     

     

    24

     

    0.08422

     

    0.02567

     

    3.5

     

    0.577

     

    0.05134

     

    4.94866

     

    0.16844

     

    4.83156

     

    0.30804

     

    4.69196

     

     

    26

     

    0.1339

     

    0.04081

     

    2.2

     

    0.361

     

    0.08162

     

    4.91838

     

    0.2678

     

    4.7322

     

    0.48972

     

    4.51028

     

     

    28

     

    0.2129

     

    0.0649

     

    1.4

     

    0.226

     

    0.1298

     

    4.8702

     

    0.4258

     

    4.5742

     

    0.7788

     

    4.2212

     

     

    32

     

    0.5383

     

    0.1641

     

    0.53

     

    0.091

     

    0.3282

     

    4.6718

     

    1.0766

     

    3.9234

     

    1.9692

     

    3.0308

     

    For a 2A Load there are no 6 foot cables that are suitable

     

     

     

     

     

     

     

     

    Current

     

    1ft USB Cable

     

    1M USB Cable

     

    6ft USB Cable

     

     

    AWG

     

    Ohm/M

     

    Ohm/Ft

     

    Chassis

     

    Transmission

     

    V Drop

     

    LOAD Volts

     

    V Drop

     

    LOAD Volts

     

    V Drop

     

    LOAD Volts

     

     

    22

     

    0.05296

     

    0.01614

     

    7

     

    0.92

     

    0.06456

     

    4.93544

     

    0.21184

     

    4.78816

     

    0.38736

     

    4.61264

     

     

    24

     

    0.08422

     

    0.02567

     

    3.5

     

    0.577

     

    0.10268

     

    4.89732

     

    0.33688

     

    4.66312

     

    0.61608

     

    4.38392

     

     

    26

     

    0.1339

     

    0.04081

     

    2.2

     

    0.361

     

    0.16324

     

    4.83676

     

    0.5356

     

    4.4644

     

    0.97944

     

    4.02056

     

     

    28

     

    0.2129

     

    0.0649

     

    1.4

     

    0.226

     

    0.2596

     

    4.7404

     

    0.8516

     

    4.1484

     

    1.5576

     

    3.4424

     

     

    32

     

    0.5383

     

    0.1641

     

    0.53

     

    0.091

     

    0.6564

     

    4.3436

     

    2.1532

     

    2.8468

     

    3.9384

     

    1.0616

     

     

     

    And this assumes the cable is truly as advertised and of good quality, some I have inspected have shown severe corrosion on the wires inside, sometimes not tined or thinner that advertised

     

     

     

    One other point to note too is that if your run the wire close or above its rating it WILL become warm and its resistance WILL increase further

     

     

     

    ONE REALLY INTERESTING POINT IS THAT NON OF THESE ARE RATED ABOVE AN AMP FOR TRANSMISSION LINE WHICH IS WHAT A USB CABLE IS.

     

     

     

    Hope this helps clarify the situation for everyone

     

     

     

    Btw, the math is correct, if our thinking the volts drop is too much, you probably forgot that there are two wires involved, one out and one back so the drop is doubled for the USB values.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to Robert Peter Oakes

    Twenty eight USB cables I have are marked. There were two clear insulation/shielded cables which were supplied with USB peripherals I bought that are not

    marked. I believe in the US at least that the wire gauge and voltage ratings (this is on all of the marked cables also) must be on the cables for regulatory approval.

     

    All of the cables I purchased were bought on the Internet from reputable companies in the US although most (all?) were made in China.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Robert Peter Oakes

    Only thing I could say here Peter is any one who had the parts and to some extent the skills to solder that horrid micro USB connector  probably wont be  asking the question.

    You are right though that a bit of decent copper sorts out many problems on the RPI especially the older ones!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 11 years ago in reply to Robert Peter Oakes

    Only thing I could say here Peter is any one who had the parts and to some extent the skills to solder that horrid micro USB connector  probably wont be  asking the question.

    You are right though that a bit of decent copper sorts out many problems on the RPI especially the older ones!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Problemchild

    While that is true, what I have done on occasion it cut the last inch from the crappy cable (Including the connector) and soldering it to the end of the good cable replacing the big connector. (I did not have any wire able connectors to use)

     

     

     

    1” of crappy wire on 6’ of excellent wire is way better than 6’ of crappy wire.

     

     

     

    I scanned many of the cables on the E14 sire and many of the ones there do not advertise their AWG so there is no way of knowing before you buy. This does not mean their crappy, just you have no way of knowing

     

     

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Robert Peter Oakes

    I was figuring that was what you were intending since wireable  micro USBs are just about as rare as unicorns for general high street use. Even so you need to do a reasonable job not to end up with 3 crap bits of wire image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Problemchild

    True but I am able to do that (Most of the time image )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to Problemchild

    John Alexander wrote:

     

    Only thing I could say here Peter is any one who had the parts and to some extent the skills to solder that horrid micro USB connector  probably wont be  asking the question.

    Adafruit has a nice DIY Micro USB plug: http://www.adafruit.com/product/1390

    I haven't tried it yet, but it looks a lot easier to solder than normal Micro USB plugs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to johnbeetem

    johnbeetem

    John

    Nice find, I'll have to add some to my next order.

     

    Mark