Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Strange screen artifact
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Subscribers 712 subscribers
  • Views 3746 views
  • Users 0 members are here
  • raspberrypi
Related

Strange screen artifact

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I have 3 Pies

#1  1x Model B with 2 USB ports

#2  1x Model B+ with 4 USB ports

#4  1x Pi2  (there is only one model, right?)

 

I have used all 3 to run Openelec.

#1 works perfectly

#2 and #3 also run openelec but they both show an artifact on the top right-hand corner. It seems to be a miniature version of the colour screen that is shown right after the Pi wakes up but before it runs an OS.

 

Has anyone else seen this????

 

Cheers,

Nick

image

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    It's a low-power warning. It shows up when the 5V supply goes below 4.65 if I remember correctly.

    http://www.raspberrypi.org/forums/viewtopic.php?f=29&t=82373

     

    --

    Ragnar

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thank you very much Ragnar!!!!!

    That's exactly what was happening.

     

    I've had issues many years ago with crappy USB leads, so I started buying one at a time from different ebay vendors until I found one that had cables that could carry 2,000 mA and then I bought a dozen or more from him, tested them each and gave most of them to my friends who were complaining about slow charging times.

    (I also bought a bunch for myself)

     

    So, when I saw your message, I collected a few of my 5V, 2,000mA power packs and tested them (as well as 2 different cables) with the Pi2.

    Voila!!!

     

    One substandard cable in the bin later and the Pi is happy.

     

    Thanks again,

    Nick

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 11 years ago in reply to royleith

    My phone definitively likes the 10cm micro USB cable better than the 25cm one. (When depleted, it will charge a little, try to boot, and shut down repeatedly unless the charger is my 20000mAh battery pack and the cable is the 10cm one....Everything else repeats the loop.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royleith
    0 royleith over 11 years ago in reply to royleith

    I have new information to add on the cable front.

     

    I purchased 1m 'Charging and Data' cables before my previous test. The new cables were wimpier than the old ones despite the illustration suggesting otherwise, but actually worked somewhat better. After the test, I purchased 0.5m cables and 0.25m cables all sold as 'Charging and Data' cables.

     

    I have now tested their loop resistance. The values are at the limit of my tester and so are somewhat of a guide.

     

    Old 1m cable    0.6Ω

    New 1m cable   0.6Ω

    0.5m cable        0.2-0.3Ω over a number of measurements

    0.25m cable      0.2Ω

     

    The wire gauge of the old cable was not shown, but all three of the new cables were marked 28AWG. I suspect the cable came from the same cable factory even if the assembly factories were different.

     

    The quality of my short-circuit was not great (a screw-driver gently inserted into the micro USB plug). I know that this could easily have added up to 0.05Ω if not more and so the accuracy of the results drops quickly with the length of the cable. All the measurements were taken several times and only the 0.5m cable showed any variation.

     

    The conclusion is that a 1m USB power cable is likely to be on the verge of causing the rainbow square voltage warning when wireless and wifi USB dongles are used. Use a powered hub if using a cable of 1m or above, although you might just get away with a good 1m cable with some devices.

     

    I am using a 0.5m cable without any signs of problems and without a powered hub. You might well be able to use all four USB ports as long as power hungry devices are not involved. A 0.25m cable does not give a significant advantage over a 0.5m cable, but might still be useful in some circumstances as when running off a mobile device charging battery. As the battery pack discharges and the output voltage drops, the shorter cable might give you a useful extension in operational time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to e14 Contributor

    If you look carefully at USB cables you will find that they are marked with the gauge of wire they use. Although they vary slightly it is usually in the form of something like: 28AWGx1P+26AWGx2C.

    This means they are using 28 AWG wire for the data connections ( 1 pair) and 26 AWG wire for the power pins. One thing I have noticed, and it seems to be fairly consistent is that longer cables (2 m)

    tend to use smaller gauge wire (30AWGx1P+28AWGx2C is typical) than shorter (0.5 m) ones. This means that shorter cables have two obvious advantages when they are used for providing power, they

    use larger wire which can handle more current, and they have less resistance because they are shorter.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to gdstew

    I have found in my investigation and as published in my post that most cables don’t even bother to mention what the wire gauge is, these ones tend to be the under rated ones

     

     

     

    I found the best way to get a good cable is to use a USB “A” type connector and replace the end with the micro connector of choice, these older cables have proven so far to consistently have better gauge wiring in them

     

     

     

    A point of interest is the typical resistance and current rating of the popular gauges

     

     

     

    This is from the American Wire Gauge Standards + some math of my own

     

     

     

     

    1Amp Load

     

                               

     

     

     

               

     

     

     

     

     

     

     

    Current

     

    1ft USB Cable

     

    1M USB Cable

     

    6ft USB Cable

     

     

    AWG

     

    Ohm/M

     

    Ohm/Ft

     

    Chassis

     

    Transmission

     

    V Drop

     

    LOAD Volts

     

    V Drop

     

    LOAD Volts

     

    V Drop

     

    LOAD Volts

     

     

    22

     

    0.05296

     

    0.01614

     

    7

     

    0.92

     

    0.03228

     

    4.96772

     

    0.10592

     

    4.89408

     

    0.19368

     

    4.80632

     

     

    24

     

    0.08422

     

    0.02567

     

    3.5

     

    0.577

     

    0.05134

     

    4.94866

     

    0.16844

     

    4.83156

     

    0.30804

     

    4.69196

     

     

    26

     

    0.1339

     

    0.04081

     

    2.2

     

    0.361

     

    0.08162

     

    4.91838

     

    0.2678

     

    4.7322

     

    0.48972

     

    4.51028

     

     

    28

     

    0.2129

     

    0.0649

     

    1.4

     

    0.226

     

    0.1298

     

    4.8702

     

    0.4258

     

    4.5742

     

    0.7788

     

    4.2212

     

     

    32

     

    0.5383

     

    0.1641

     

    0.53

     

    0.091

     

    0.3282

     

    4.6718

     

    1.0766

     

    3.9234

     

    1.9692

     

    3.0308

     

    For a 2A Load there are no 6 foot cables that are suitable

     

     

     

     

     

     

     

     

    Current

     

    1ft USB Cable

     

    1M USB Cable

     

    6ft USB Cable

     

     

    AWG

     

    Ohm/M

     

    Ohm/Ft

     

    Chassis

     

    Transmission

     

    V Drop

     

    LOAD Volts

     

    V Drop

     

    LOAD Volts

     

    V Drop

     

    LOAD Volts

     

     

    22

     

    0.05296

     

    0.01614

     

    7

     

    0.92

     

    0.06456

     

    4.93544

     

    0.21184

     

    4.78816

     

    0.38736

     

    4.61264

     

     

    24

     

    0.08422

     

    0.02567

     

    3.5

     

    0.577

     

    0.10268

     

    4.89732

     

    0.33688

     

    4.66312

     

    0.61608

     

    4.38392

     

     

    26

     

    0.1339

     

    0.04081

     

    2.2

     

    0.361

     

    0.16324

     

    4.83676

     

    0.5356

     

    4.4644

     

    0.97944

     

    4.02056

     

     

    28

     

    0.2129

     

    0.0649

     

    1.4

     

    0.226

     

    0.2596

     

    4.7404

     

    0.8516

     

    4.1484

     

    1.5576

     

    3.4424

     

     

    32

     

    0.5383

     

    0.1641

     

    0.53

     

    0.091

     

    0.6564

     

    4.3436

     

    2.1532

     

    2.8468

     

    3.9384

     

    1.0616

     

     

     

    And this assumes the cable is truly as advertised and of good quality, some I have inspected have shown severe corrosion on the wires inside, sometimes not tined or thinner that advertised

     

     

     

    One other point to note too is that if your run the wire close or above its rating it WILL become warm and its resistance WILL increase further

     

     

     

    ONE REALLY INTERESTING POINT IS THAT NON OF THESE ARE RATED ABOVE AN AMP FOR TRANSMISSION LINE WHICH IS WHAT A USB CABLE IS.

     

     

     

    Hope this helps clarify the situation for everyone

     

     

     

    Btw, the math is correct, if our thinking the volts drop is too much, you probably forgot that there are two wires involved, one out and one back so the drop is doubled for the USB values.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to Robert Peter Oakes

    Twenty eight USB cables I have are marked. There were two clear insulation/shielded cables which were supplied with USB peripherals I bought that are not

    marked. I believe in the US at least that the wire gauge and voltage ratings (this is on all of the marked cables also) must be on the cables for regulatory approval.

     

    All of the cables I purchased were bought on the Internet from reputable companies in the US although most (all?) were made in China.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Robert Peter Oakes

    Only thing I could say here Peter is any one who had the parts and to some extent the skills to solder that horrid micro USB connector  probably wont be  asking the question.

    You are right though that a bit of decent copper sorts out many problems on the RPI especially the older ones!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Problemchild

    While that is true, what I have done on occasion it cut the last inch from the crappy cable (Including the connector) and soldering it to the end of the good cable replacing the big connector. (I did not have any wire able connectors to use)

     

     

     

    1” of crappy wire on 6’ of excellent wire is way better than 6’ of crappy wire.

     

     

     

    I scanned many of the cables on the E14 sire and many of the ones there do not advertise their AWG so there is no way of knowing before you buy. This does not mean their crappy, just you have no way of knowing

     

     

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Robert Peter Oakes

    I was figuring that was what you were intending since wireable  micro USBs are just about as rare as unicorns for general high street use. Even so you need to do a reasonable job not to end up with 3 crap bits of wire image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Problemchild

    True but I am able to do that (Most of the time image )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to Problemchild

    John Alexander wrote:

     

    Only thing I could say here Peter is any one who had the parts and to some extent the skills to solder that horrid micro USB connector  probably wont be  asking the question.

    Adafruit has a nice DIY Micro USB plug: http://www.adafruit.com/product/1390

    I haven't tried it yet, but it looks a lot easier to solder than normal Micro USB plugs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to Problemchild

    John Alexander wrote:

     

    Only thing I could say here Peter is any one who had the parts and to some extent the skills to solder that horrid micro USB connector  probably wont be  asking the question.

    Adafruit has a nice DIY Micro USB plug: http://www.adafruit.com/product/1390

    I haven't tried it yet, but it looks a lot easier to solder than normal Micro USB plugs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 11 years ago in reply to johnbeetem

    johnbeetem

    John

    Nice find, I'll have to add some to my next order.

     

    Mark