Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum New reworked driver for Wolfson/Cirrus Logic audio card
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 390 replies
  • Subscribers 767 subscribers
  • Views 50586 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

New reworked driver for Wolfson/Cirrus Logic audio card

hiassoft
hiassoft over 9 years ago

I've been working on a driver rework, mainly to get rid of the requirement to carry around a bunch of patches to upstream driver code, and also to fix some outstanding issues and introduce some new features.

 

Most issues have been ironed out so here's the first public release.

 

Edit: the driver has been included in official RPi kernels. Just run sudo rpi-update to install it.

You still have to install the mixer scripts and add the /etc/modprobe.d file. See my website for details

RPi Linux driver for Wolfson / Cirrus Logic Audio Card

 

Source: https://github.com/HiassofT/rpi-linux/tree/cirrus-ng-4.9.0

Precompiled kernel: http://www.horus.com/~hias/tmp/cirrus/cirrus-ng-linux-4.9.0.tgz

New mixer scripts: http://www.horus.com/~hias/tmp/cirrus/cirrus-ng-scripts.tgz

 

Important notes:

  • The new driver bases on the rather fresh kernel 4.9.0 which means there's some risk of (yet unknown) issues. Use it at your own risk and please run "rpi-update" to get the latest firmware before installing the new driver.
  • The soundcard name has been changed from "snd_rpi_wsp" to "RPi-Cirrus", also several ALSA controls have been removed and new ones were added. This means the old usecase scripts and any custom-made scripts will no longer work. Use the new mixer scripts instead of the old usecase/listen scripts.
  • The new driver supports setting (and receiving) of the S/PDIF channel status bits (aka AES bits). If you add an ALSA card configuration file this means applications like Kodi can do proper AC3/DTS passthrough. A sample card configuration file (plus the mixer scripts) can be found here: https://github.com/HiassofT/rpi-cirrus-config
  • I haven't fully updated the documentation on my website RPi Linux driver for Wolfson / Cirrus Logic Audio Card  yet, will do that during the next weeks/months. But except for the things noted above most stuff should still work as in previous driver versions.

 

Please report back if you tested the driver (either successfully or unsuccessfully), any feedback will help me!

 

so long,

 

Hias

  • Sign in to reply
  • Cancel
Parents
  • timg73
    timg73 over 9 years ago

    Hias,

    A huge thank-you for all the work you've put into supporting the Cirrus Audio card.  Until now I've been using your kernel packages, and have just got round to trying the latest official 4.9 kernel which is also working very nicely.  It's a real shame that the Cirrus card has (or appears to have) gone out of production just when the software support became so good.  The older Wolfson cards are still available, so perhaps I'll get a couple and try modifying them to fit a 40-pin header.  Anyway, thanks again for everything you've done.  I really do appreciate it.

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hystrix
    hystrix over 9 years ago in reply to timg73

    The Cirrus Card does seem to be out of stock everywhere - what a shame.  I just started working on an alternative ultrasound sensistive microphone, since the electret type I was using has been out of production for years and is now virtually impossible to get hold of.

     

    What other options are there for recording audio at 192kHz with the Raspberry Pi?

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hystrix
    hystrix over 9 years ago in reply to hiassoft

    Ha! I was just looking at those pogo pin connections myself.  From the photo, it looks like the connections are:

     

    P5 Pin 3 to GPIO Pin 12

    P5 Pin 4 to GPIO Pin 35

    P5 Pin 5 to GPIO Pin 38

    P5 Pin 6 to GPIO Pin 40

     

    And remove R39.

     

    Are those the only chnages to make?  On the piggy-back board, what is that connection on GPIO Pin 33 on the 40 pin header and GPIO Pin 12 on the 26 pin header?

     

    Many thanks :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 9 years ago in reply to hystrix
    It's a shame that the Wolfson card doesn't have Line In micbias, but I could live with that.

    Looking at the schematic it seems you can add it quite easily: remove C8 (it's next to the WM5102), then connect that to 2 2k2 resistors and solder the other end to line in (junction between R55/L6/C33 and R56/L7/C32). Then it'd be like the Cirrus card.

     

    Taking Micbias from the headset in would also be a possibility, just remember that'd you'd need to enable Headset input as well (you could just do a "cirrus-listen headset headset" then micbias on headset in will always be on).

     

    Is removing R39 on the Wolfson board absolutely essential?

    Yes. During reset pin 5 of the WM8804 is used as in input to select the I2C address - so you need to have it connected to the pullup. Afterwards it's an output so if you leave it connected to P1 header pin 12 it'd clash with the I2S clock. I haven't found an easier way to cut the connection from GPIO pin 12 to the WM8804 so removing the in-line 0R resistor R39 seems to be the easiest method ATM.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • psyj
    psyj over 9 years ago in reply to hystrix

    Hystrix

     

    See Hias comment, it looks as though I have mirrored the J5 pins, so wait for the revised diagram! Sorry!  But the link you are referring to provides the correct connection back to the 8804.  That is done for completeness, because as Hias says, the pin on the 8804 can be left open circuit without a problem.

     

    The minimum set of connections are just as you say.

     

    As per Hias suggestion, I had thought of making the piggy back card "full size" so that it can offer mechanical support.  At the moment I am thinking of what else to use the card space for.  I need to drive a relay(!) based digital attenuator for the output of the Wolfson, so I will probably put a couple of I2C ports on the card.

     

    Hias,

     

    Once again, thank you for your help

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • psyj
    psyj over 9 years ago in reply to psyj

    And herewith the revised pcb

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hystrix
    hystrix over 9 years ago in reply to psyj

    Hi John - thanks for the update.

     

    Now all I have to do is find the elusive R39.  I only had a quick look last night.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 9 years ago in reply to hystrix

    Now all I have to do is find the elusive R39. I only had a quick look last night.

     

    It's on the bottom side of the PCB, near the mounting hole.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hystrix
    hystrix over 9 years ago in reply to hiassoft

    Hias and John,

     

    I got my "Frankenson" sound card working with a Pi2 image.

     

    I didn't de-solder the pogo pins.  I found a cover that fits over them nicely - made from a UK 3-pin mains plug protector that all new electrical devices come with.  I cut the end off the Earth pin end of the protector.  It fits neatly onto the pogo pins.  Once the Wolfson card is attached to the Pi, the cover is held nicely in place, and stops them shorting on anything on the Pi.

     

    image

     

    Here's the pogo cover made from a plug protector:

     

    imageimageimage

     

    Thanks for your help with this neat hack.

     

    Hystrix

     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • psyj
    psyj over 9 years ago in reply to hystrix

    Bravo, I like it.  One of the positive british traits that, improvisation.

     

    I knew UK plugs would prove better one day .... It has only taken 60 years  ..... Ironically I cut the last one off my appliances only this week.

     

    More seriously, note that there is a wee bit of strain introduced by the pin protector, perhaps raise the Wolfson card a millimetre to compensate.

     

    I have just made the mark 1 piggy back board, so if I can get the single sided version to work, expect photos of that too.  It's good to see an active community

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hystrix
    hystrix over 9 years ago in reply to psyj

    Ha!  I knew someone would mention the strain caused by the pogo pin protector. image   This was an early photo - I actually trimmed off some more of the plastic on the left-hand side.  You can see the black header is catching on it in the photo - it's much better now.

     

    My only concern is whether the springs in the pogo pins will eventually start to push the audio card off the header.  Time will tell.  I may even file off some of the plastic from the bottom of the pin protector, so the springs aren't compressed as much.

     

    I look foward to the photos of the piggy-back board.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 9 years ago in reply to hystrix

    I got my "Frankenson" sound card working with a Pi2 .

     

    I didn't de-solder the pogo pins. I found a cover that fits over them nicely - made from a UK 3-pin mains plug protector that all new electrical devices come with. I cut the end off the Earth pin end of the protector. It fits neatly onto the pogo pins. Once the Wolfson card is attached to the Pi, the cover is held nicely in place, and stops them shorting on anything on the Pi.

    That's looking really nice, well done! And I think the cap over the pogo pins is a rather clever idea!

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hiassoft
    hiassoft over 9 years ago in reply to hystrix

    I got my "Frankenson" sound card working with a Pi2 .

     

    I didn't de-solder the pogo pins. I found a cover that fits over them nicely - made from a UK 3-pin mains plug protector that all new electrical devices come with. I cut the end off the Earth pin end of the protector. It fits neatly onto the pogo pins. Once the Wolfson card is attached to the Pi, the cover is held nicely in place, and stops them shorting on anything on the Pi.

    That's looking really nice, well done! And I think the cap over the pogo pins is a rather clever idea!

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • psyj
    psyj over 9 years ago in reply to hiassoft

    Matthias,

     

    Really sorry to bother you, but having got my piggy back +pi 3 working, I played with the kernel. Fatal mistake.  I had been running Runeaudio + your(?) 4.4.14 kernel, but I have messed up.  I could spend days finding the problem (and 5 minutes fixing it), but perhaps it is time to leave the past behind. What kernel would you recommend to run headless MPD, with linux shell available over SSH and the ability to run brutefir? It sounds like I dont need Jessie (which you kindly support) nor the librelec kernel (which you kindly support).

     

    Many thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 9 years ago in reply to psyj

    Hi John!

    What kernel would you recommend to run headless MPD, with linux shell available over SSH and the ability to run brutefir? It sounds like I dont need Jessie (which you kindly support) nor the librelec kernel (which you kindly support).

    I'd recommend using Raspbian Lite (Jessie), this is what I'm using for my (mostly headless) test setups as well. The Lite version comes with a minimal set of packages preinstalled, no desktop environment and unnecessary cruft for headless setups, and you can easily install the packages you want. mpd and brutefir are all available from the Raspbian repo, "sudo apt-get install mpd brutefir" and you can get going image Ah, well, and "sudo rpi-update" for the 4.9 kernel with cirrus drivers plus downloading the mixer scripts, of course image

     

    so long,

     

    Hias

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • psyj
    psyj over 9 years ago in reply to hiassoft

    Matthias,

     

    As always, thanks for the rapid reply.  It all went smoothly, though not as quickly as I would like.  Below I have listed the steps I took in painstaking detail ....  Obviously this is stuff you already know!  But if somebody else wants to do the same thing, it saves you from having to reply.  Your instructions at RPi Linux driver for Wolfson / Cirrus Logic Audio Card are concise and 100% correct.  Here I just spell it out.

     

     

    1) Download jessie lite and unzip it from the base repository

     

    2) In a terminal on a linux machine with a blank memory card inserted (at device $)

            sudo dd bs=4M if=2017-03-02-raspbian-jessie-lite.img of=/dev/sd$

     

    3) SSH is enabled in jessie by creating a file with name "ssh" in the boot partition

     

    4) Install card and boot pi (with wired ethernet)

     

    5) SSH to device  ssh $.$.$.$ -l pi (password=raspberry), thence

     

        sudo apt-get install rpi-update

     

        sudo rpi-update (y at prompt.  We do this to get the 4.9 kernel to get the driver for the Wolfson)

     

        sudo raspi-config (to enable i2c and spi, follow the menus)

     

        sudo reboot

     

    6) SSH to device (again)

     

        uname -a (just to check at kernel 4.9)

     

        sudo apt-get install mpd brutefir (to install my tools for later)

    (this failed, so)

        sudo apt-get update

     

        sudo apt-get install mpd brutefir (to install my tools for later)

    (locale warnings from perl, but unpacks a lot more, esp stuff for brutefir like fft)

     

        sudo apt-get install mpc (useful add on to mpd)

     

        sudo apt-get install i2c-tools (to check device presence.  8804 on card shows at 3b using  sudo i2cdetect -y 1)

     

        sudo apt-get install vim to get vim editor (easier to edit through SSH than playing the permissions game through ftp)

     

    (you could wrap all those gets up into a single line, skip the reboot etc, this is just my log!)

     

       sudo vim /boot/config.txt (uncomment #dtparam=i2s=on and add the line "dtoverlay=rpi-cirrus-wm5102")

        sudo vim /etc/modprobe.d/cirrus.conf (to create new file, with content "softdep arizona-spi pre: arizona-ldo1")

     

        sudo reboot

     

     

    SSH to device

     

    At this point aplay -l shows the (piggy backed) Wolfson card and alsamixer allows you to play with it

     

     

    (Apologies to all, I must learn the correct protocol for doing this on the board)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • psyj
    psyj over 9 years ago in reply to psyj

    Postscript,

     

    The rest of getting the new system working went very smoothly, a bog standard MPD configuration and moving the system to run from HD (I don't like writing to SD ad infinitum) .  The only hiccup came when I imported my alsactl state file (alsactl allows you to store and restore complete configurations for the sound card, very useful when playing with something as complex as this sound card).  Matthias has indicated in an earlier post that the driver had changed and so my import failed    ...... my own silly fault .......

     

    alsactl: set_control:1325: failed to obtain info for control #36 (No such file or directory)        (ditto 37,38,39)

    alsactl: set_control:1325: failed to obtain info for control #162 (No such file or directory)

    alsactl: set_control:1325: failed to obtain info for control #298 (No such file or directory)       (ditto 299,300,301)

    alsactl: set_control:1325: failed to obtain info for control #461 (No such file or directory)       (ditto 462,463,464)

     

    The first group are the EQn filter equalisation parameters, which I use as a partial room correction filters....... in fact a large number of other controls have changed numbering too, so I do not suggest this path for migrating parameters

     

    So now a few tweaks and I am done!

     

    (Matthias,  I remember you mentioning the EQ parameters changing from 42 to 40 bytes, so no need to reply, unless you want to.  It is only when you look at the state file that you realise how enormous the driver is.  Yet again, many thanks)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • psyj
    psyj over 9 years ago in reply to hiassoft

    Matthias,

     

    It is a 100 to one shot I know, but by any chance did you compile WISCEbridge support into your driver?  (From what I can find WISCEbridge allows raw register read/write through ports 22348/22349 using a "simple" protocol)  I am guessing not, but it has proved impossible for me to find a copy of WISCEbridge for Linux (which is in the WISCE SDK).

     

    From an ideological point of view, I am guessing that it would not be correct to integrate what would effectively be a back-door for this control route into the driver for the 5102. I ask because I would like to know what you would see as the correct way of setting up the EQ parameters .... raw writes to your driver, a cosmetic layer or direct access to the registers via i2c/spi (I've rewired one of my Wolfson to make the 5102 visible on i2c).  Of course direct access could well give rise to clashes with your driver.

     

    So I am guessing I have many happy evenings with wireshark ahead of me!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 9 years ago in reply to psyj

    Hi John!

    It is a 100 to one shot I know, but by any chance did you compile WISCEbridge support into your driver? (From what I can find WISCEbridge allows raw register read/write through ports 22348/22349 using a "simple" protocol) I am guessing not, but it has proved impossible for me to find a copy of WISCEbridge for Linux (which is in the WISCE SDK).

     

    I didn't have much luck with WISCE so far. Downloaded the latest version (3.6.1.3) and installed the WM5102 setup from cirrus.com but I just got an error message when trying to create a simulation project. WISCE log says "Internal Error - WARNING: Firmware on WM5102's DSP1 core is NOT valid" - not sure what's going wrong there.

     

    Do you have the original installation files and could you upload them somewhere?

     

    As for direct register access: I wrote a simple program to do that, via I2C, needed that for debugging as well image http://www.horus.com/~hias/tmp/cirrus-reg.c

     

    The kernel driver accesses the WM5102 chip via SPI but the chip is also connected via I2C. The I2C interface is only available when the chip is active (i.e. not in standby), so you either need to have aplay/arecord running in the background or run a listen script - otherwise the WM5102 will enter standby mode and only react on SPI.

     

    As for the EQ registers: WM5102 has 21 16-bit registers for each equalizer, EQ1 registers are 0xE10-0xE24. The first 2 registers control the 5 band volumes and are exposed via alsa mixer controls ("EQ1 B1 Volume" .. "EQ1 B5 Volume"). The EQ enable bit in the first EQ register is controlled via DAPM, that means whenever you route signals through the EQ it'll automatically be enabled.

     

    The mixer control "EQ1 Coefficients" sets registers 0xE11-0xE24 - which means they overlap with the B4 and B5 controls in 0xE11.

     

    For details about the register and mixer definitions look at include/linux/mfd/arizona/registers.h and sound/soc/codecs/wm5102.c in the kernel tree - just search for _EQ1_

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • psyj
    psyj over 9 years ago in reply to hiassoft

    Hias,

     

    Many thanks.  Here is a link https://www.dropbox.com/s/q5syxn3asr2yirq/WISCESetup.zip?dl=0 to the WISCE I use, without any problems. Cannot help with the error, I have never seen it. I have noted that WISCE does a lot of parameter checking.  Is it posssible that you have some DSP microcode loaded (or are trying to load) that WISCE does not like? (Which is to say that WISCE is working perfectly, it is just that it doesnt like DSP code).  As I understand it, none of us are using/loading the DSP. 

     

    I have been digging around this evening looking for an alternative to WISCEBridge for connecting to the 5102 from WISCE (which would be ideal since there is WISCEbridge for linux)  ..... WISCE will allow a direct i2c/spi connection to the 5102 via an Aardvark USB interface  ...... which has the same pinout as the USBi/ freeUSBi   ...... so it is JUST possible that the freeUSBi interface will allow a USB -> i2c/spi connection from WISCE to the 5102  .... but of course there are bus master problems if the pi is connected as well

     

    I have been using i2c-tools to write to the 5102 directly  .... and it took a while to find out that nothing worked except when playing some music!  It is buried away in the 5102 documentation  .... the device will respond to SPI and/or I2C when being clocked, but only the original bus used at boot time if the device is "stopped". So your explanation that you use spi at boot fits well :- except that I am confused! My reading of the Wolfson circuit schematic suggests that there is only an i2c connection to the 8804, so I added a couple of wires to link in the 5102  ... but that does not fit with what you say, unless of course you added two link wires as well.

     

    I'll look at cirrus-reg.c .... I am sure that it will be easier that using i2cwrite/read! (Postscript:- yes that will make life simpler, thanks)

     

    And the Wolfson documentation is invaluable for working out how to program the 400 odd registers for the four EQ!!  At the moment I am not optimistic about getting good low frequency equalisation

     

    Best Wishes

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 9 years ago in reply to psyj

    Hi John!

    Many thanks. Here is a link https://www.dropbox.com/s/q5syxn3asr2yirq/WISCESetup.zip?dl=0 to the WISCE I use, without any problems. Cannot help with the error, I have never seen it. I have noted that WISCE does a lot of parameter checking. Is it posssible that you have some DSP microcode loaded (or are trying to load) that WISCE does not like? (Which is to say that WISCE is working perfectly, it is just that it doesnt like DSP code). As I understand it, none of us are using/loading the DSP.

    Thanks for the link, but I didn't have much luck with this version either. Here's what I did:

    • start up my WindowsXP virtualbox VM
    • uninstall previous WISCE version and WM5102 setup
    • install your WISCE, using default settings (I even let it install the FTDI drivers)
    • in WISCE click on "Add System" and choose "Create a new simulated system"
    • Add device dialog pops up, only selectable chip is WM5102 Rev C, I accept the default settings (SMBUS, address 0x34)
    • After a few seconds a dialog pops up with the message "Failure adding device 'WM5102'. Please contact WISCESupport@cirrus.com with the details of the device you were trying to use"

     

    Then I checked the logfile, found this at the end of it:

    06-04-2017 10:23:52.369 * Detecting devices for Simulated system.
    06-04-2017 10:23:52.369 *    - No devices detected.
    06-04-2017 10:25:22.178 *    - fully loaded c:\programme\wolfson evaluation software\devices\wm5102_regmap_revc 2v9.wxd
    06-04-2017 10:25:23.340 * Internal Error - WARNING: Firmware on WM5102's DSP1 core is NOT valid.
    06-04-2017 10:25:23.570 * Internal Error - Failure adding device entity for region 'WM5102': System.IO.FileLoadException: Eine von "Wolfson.WISCE.Filters.dll" importierte Prozedur konnte nicht geladen werden.
    Dateiname: "Wolfson.WISCE.Filters.dll"
       bei System.Windows.Forms.Control.MarshaledInvoke(Control caller, Delegate method, Object[] args, Boolean synchronous)
       bei System.Windows.Forms.Control.Invoke(Delegate method, Object[] args)
       bei System.Windows.Forms.WindowsFormsSynchronizationContext.Send(SendOrPostCallback d, Object state)
       bei Wolfson.WISCE.Entities.DeviceEntity.Initialize(IDataRegion region)
       bei Wolfson.WISCE.Entities.DeviceEntity..ctor(SystemEntity system, IDataRegion dataRegion, String deviceName)
       bei Wolfson.WISCE.Entities.DeviceEntity.Create(SystemEntity system, IDataRegion dataRegion)
       bei Wolfson.WISCE.Entities.SystemEntity.GDNNINCJKLLEILDPMMHMEAAEBPCLDIJFCBAH(IDataRegion  )
    
    
    06-04-2017 10:25:23.570 * Error - Failure adding device 'WM5102'. Please contact 'WISCESupport@cirrus.com' with details of the device you were trying to use.
    06-04-2017 10:27:14.810 * --------------------Closing WISCE™--------------------

     

    Not quite sure what's going wrong there, the DSP firmware warning could be a red herring and the real issue some dll/system incompatibility. I guess I'll leave it there.

     

    I have been using i2c-tools to write to the 5102 directly .... and it took a while to find out that nothing worked except when playing some music! It is buried away in the 5102 documentation .... the device will respond to SPI and/or I2C when being clocked, but only the original bus used at boot time if the device is "stopped". So your explanation that you use spi at boot fits well :- except that I am confused! My reading of the Wolfson circuit schematic suggests that there is only an i2c connection to the 8804, so I added a couple of wires to link in the 5102 ... but that does not fit with what you say, unless of course you added two link wires as well.

    Just checked the schematics, on the Cirrus card I2C of the WM5102 is connected to RPi as well, but on the original Wolfson card the I2C interface of the WM5102 seems only to be routed to the ext connector. See page 3 of the schematic PDFs, CIF1SCLK and CIF1SDA signals.

     

    I did most tests with the Cirrus card so that explains why I didn't have to modify anything image

     

    BTW: Why are you trying to access the WM5102 directly? The majority of the WM5102 registers are exposed via alsa controls and if you access the chip directly the register contents of the WM5102 will be out of sync with the (cached) register settings used by ASoC/Linux - check /sys/kernel/debug/regmap/spi0.1/registers for example. This can quickly lead to a mess, so be very careful with that. Better stick to the alsa controls and only use direct access for registers that are not exposed via alsa.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • psyj
    psyj over 9 years ago in reply to hiassoft

    Hias,

     

    Well on the WISCE software, perhaps it is the 5102 exe file that is the problem ..... so just in case  ....  https://www.dropbox.com/s/lwokz6h2bn81pvt/WM5102Setup_Rev2_9.zip?dl=0  > It seems quite possible, since the problem only occurs when you load the device.  I have also uploaded the 8804 specific file  https://www.dropbox.com/s/sen92d6zv2mazss/WM8804Setup_Rev1_1.zip?dl=0   , that way you can try starting WISCE without loading the 5102 information.

     

    On the I2C, I did wonder whether that was the explanation

     

    As to direct writes, you are of course right  ..... it is just that repeatedly typing 80 quasi random hex charecters is pretty error prone when I want to change one byte (well strictly 2 bytes).  I guess I could write a script, but I might end up spending more time on the temporary fix than on the experiment.  The purpose of my earlier email was to find out what way you thought best  ..... and I will happily follow your advice.  Any final system, I will use the alsa set/get  .... but like you I need a quick debug route to find out whether I can get low frequency (less than 500hz) filtering working to my needs before investing lots of time on scripts (in which I am not particularly well experienced.  My plan is to use php to serve up pages of possible settings and receive user adjustments.  Have some basic stuff working, but have not tried the complex maths that is going to be needed to convert.  By the way, is there an easy way to determine current sample rate through an alsa call to the driver, because this will be set by MPD autonomously and it is a key number in filter calculations)

     

    Cheers

     

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • psyj
    psyj over 9 years ago in reply to psyj

    Hias,

     

    Bad form replying to my own post, but I have started playing with the EQ filter parameters, guided by WISCE.  herewith some results

    image

     

    The curves here are not particularly important. what is important is that WISCE only allows certain, heavily quantised frequencies, all of them above 100Hz.  The purple curve might give a clue why,  I think that (for obvious reasons) it is seeking to have zero gain at 0Hz.  Well that is all sensible, but when I try to "ski off piste" by putting raw values into amixer set commands (nothing extreme, just shifting the frequencies slightly) the linux driver throws me out with an "invalid parameter" warning. So not only WISCE , but ALSA as well are doing parameter checking.  So in answer to your earlier question, it would seem the only way to use other parameters is by direct register access via i2c   ....... accepting of course the risks involved!

     

    (Postscript:  any idea where the parameter checking is done?    ...... .with a bit of generous help from A.N.Other it is done in arizona.c  . which fails all A and B parameters whose absolute value exceeds 4095 and also does a ratio check between A and B)

     

     

    John