Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Weird I2C Issue with Pi CM3 [SOLVED]
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 39 replies
  • Subscribers 707 subscribers
  • Views 13141 views
  • Users 0 members are here
  • raspberry
  • i2c
  • issue
  • wiring
  • connection
  • jessie
  • protocol
  • raspbian
  • compute module
  • linux
Related

Weird I2C Issue with Pi CM3 [SOLVED]

balearicdynamics
balearicdynamics over 9 years ago

This is a strange issue I have no idea how to solve; it seems I am unable to debug correctly the problem to find at least what class of issue it is.

 

I have tried several I2C devices set as slave including Infineon XMC1100 Boot KitXMC1100 Boot Kit and Arduino UNOArduino UNO. Then I moved to the simple two cap sense buttons PmodCDC1PmodCDC1 by Digilent; as the device is powered and connected to the I2C bus it starts in continue sending data. I should expect to see at least its address will be detected by the CM3 I/O board but nothing happens.

image

I2C has been set and enable correctly in /boot/config.txt and the raspbian version running on the eMMC of the CM3CM3 is the latest Jessie (July, 5 , 2017). Signals are connected to the GPIO2 and GPIO3 (SDA1, SCL1) accordingly with the eLinux table specifications (see in attach) to the GPIO Pins 2 and 3. Digilent device is powered with the 3V3 and voltage is correct and stable.

I have not used external pull-up resistors on SDA/SCL signals as the CM3 already includes 1.8K pull-up resistors on these two lines, following the CM3 peripheral recommendations.

imageimage

Initially I though that it was possible that wrong resistor values was blocking the signals to go up but as shown in the video below, hardware seems working fine. Note that when I send a i2cdetect -y 1 command from the terminal data are sent by the CM3 side. But nothing is shown.

Any suggestion is welcome.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Update

Supposing that despite what the documentation says the internal pull-up resistor is not enabled I have added a 1.5K resistor pulled up to the 3V3 (the nearest I have at home respect the declared in the documentation (1K8). What I get with the protocol analyser is a series of packets as shown in the images below but always nothing is detected by the master (Pi side).

image

image

image

image

 

Last update

After trying and discussing with all the helpful members that spent time with me I have received in the meantime a second Pi Compute Module IO board and as all the suggested tests and possible mistakes was converging to the right setup for the I2C protocol, as expected, the problem was for  some unknown reason the board itself. As I replaced the board with a new one things started working perfectly.

 

Thanks to shabaz Robert Peter Oakes rew Jan Cumps and... johnbeetem for the useless suggestion of the thread image LoL

 

Update

After the last testing and following some suggestions of the starting supposition is that - together with the I/O board - also the Compute Module 3 booting from the eMMC maybe with some hardware failure as all the tests with the Compute Module 3 Lite booting from the eMMC is working fine with the same Raspbian distribution, desktop version (instead of headless like on the eMMC side).

 

First test: a new microSD with the Raspbian Jessie Lite has been set and after booting the Compute Module 3 Lite I have done the same setup of the Compute Module eMMC. At this point bot boards runs the same version. And after sudo update / upgrade the command i2cdetect -y 1 works perfectly! So we can think 90% sure that the issue is in the Compute Module 3 with eMMC memory. Remain a last test to see if this issue is systematic or not: flashing another Compute Module 3 eMMC and see if it work.

 

Update - Conclusion

After doing the test mentioned in the update above a new Compute Module 3 eMMC board has been setup with a fresh installation and with the same connections of the previous settings, same Jessie Lite July 2017 and I2C protocol worked immediately without problems. So, the main issue was the CM3 eMMC board and the I/O board kit.

image

 

XMC1100 Boot Kit + TLE94112LE I2C communication

The setup of the two boards (XMC1100 + TLE94112LE) connected to the CM3 via the I2C bus was creating a trouble on the bus signals so that the i2cdetect -y 1 command was no longer able to recognise any connected peripheral.

The board has been configured as slave on the address 0x04. A check with the same software and the same hardware setup using and Arduino UNO instead was working fine. Investigating on this issue I have found the problem was already known involving Wire library version for the XMC1100 board updated by mhollfelder on the Infineon XMC1100 GitHub repository, the Pull Request #13.

On Aug, 31, 2017 Manuel (thanks) completed the update of the pull request, merged in the main and released a new XMC1100 Arduino board core  library version 1.0.4 (the module downloadable / upgradable in the Board Manager of the Arduino IDE) and all worked fine with the Infineon board alone connected to the I2C bus.

 

As I have integrated the XMC1100 Boot Kit board with the TLE94112LE DC Motor controller I have included the the TLE94112 Arduino library in the sketch detecting another non-blocking issue in the I2C Wire library (XMC1100 version) and opened the issue #14

The behaviour details are explained in the issue note; the problem can be easily avoided initialising the Wire library as the last call in the Setup() method of the sketch ;twe can consider this the workaround to the problem until it is not definitely solved.

Attachments:
imageRPi BCM2835 GPIOs - eLinux.pdf
imageRPI-CMIO-V3_0-SCHEMATIC.pdf
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 9 years ago

    have you loaded the drivers on for the lcd?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to e14 Contributor

    Yes Luvie, as you can see in the picture it is up and running (showing i2c detected address)

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to balearicdynamics

    Its good to see you got it working, whatever was using that port is gonna remain a mystery Relaxed

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to e14 Contributor

    Thank you dear Lucie, but it is good and bad too image The problem is that the only working device is the Compute Module 3 Lite (booting from the microSD). Now there are two possible reasons:

     

    1. The Compute Module 3 booting from eMMC has a problem and I will verify flashing another identical to see if the issue repeats. I think this is probable at 20%
    2. The Raspbian jessie live image has something wrong in the kernel modules that has been solved (or is not present) in the desktop module. It is not possible to install the full jessie on the eMMC due the image is too large but it is possible to do the opposite and it is what I will do first to see. If the issue happens too on the Compute Module 3 lite, we are almost sure that the issue is in the jssie lite image.

    I'll keep you update. Preparing a fresh installation microSD now.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to balearicdynamics

    A possibility here is the pi compute module 3 uses the I2C1 bus to communicate with the emmc? Just a thought, maybe studying the schematic will explain more

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to e14 Contributor

    Accordingly with the documentation we should say absolutely no. As the i2c protocol is available on the CM3 and it is explicitly mentioned for both. I am finishing a second CM3 installation to test if the same issue occurs. Question of minutes image

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to e14 Contributor

    Complete the update of the post and the question is solved. The I2C protocol works perfectly also with the Compute Module eMMC, on a different board. The issue is in the board itself. image

     

    Happy. Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 9 years ago in reply to e14 Contributor

    Without looking at the documentation, that is extremely unlikely. EMMC is "storage".  The faster the better! I2C was designed in the days when 100kbps was thought to be plenty. So I2C is slow. It has been enhanced to be able to do 1Mbps, and one or two chips allow you to go even faster than that, but that's about it. EMMC is essentially SPI and SPI will do 16Mbps without any trouble. Add three or seven more datalanes and you are doing 8 or 16 Mbyte per second. That's still slow by modern standards.... EMMC will beat that and it's already 100 times faster than I2C topspeed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to rew

    Yes, many devices that require a faster bus still use an additional i2c/smbus connection for device setup etc...

     

    For instance if you look at the datasheet for the the emmc module on the pi compute you'notice it has CLK and CMD pins, further down in the datasheet it explains these pins can be used as a way of transferring additional commands.

     

    Also to note, these pins are connected to the bcm2835, if theyre not connected to one of the user i2c busses then they'll be connected to a reserved bus that hasnt been broken out to the user(which is either an i2c bus or an smbus).

     

    You'll find even ram modules on a pc use an additional 2 wire bus to tranfer additional data (even if its just to retrieve the make and model number, speed constraints, data storage method, bit width, ram depth etc...) Thats how computers are able to configure themselves and detect new devices added etc. The high speed data transfer busses are only used for the data transfers in most cases but most hardware also needs to transfer some configuration backwards and forwards too.

     

    http://www.datasheetspdf.com/mobile/947361/KLM4G1FE3B-B001.html

     

    enjoy the reading!

     

    --------

    edit

     

    Excerp from the datasheet

     

    image

     

     

    The CLK and CMD pins are used to even specify a data write operation, once this is done the data travels across the wider DATA bus where the CLK pin is still used by the host to signal the arrival of that data, also is the case with standard sdcards etc...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to rew

    Yes, many devices that require a faster bus still use an additional i2c/smbus connection for device setup etc...

     

    For instance if you look at the datasheet for the the emmc module on the pi compute you'notice it has CLK and CMD pins, further down in the datasheet it explains these pins can be used as a way of transferring additional commands.

     

    Also to note, these pins are connected to the bcm2835, if theyre not connected to one of the user i2c busses then they'll be connected to a reserved bus that hasnt been broken out to the user(which is either an i2c bus or an smbus).

     

    You'll find even ram modules on a pc use an additional 2 wire bus to tranfer additional data (even if its just to retrieve the make and model number, speed constraints, data storage method, bit width, ram depth etc...) Thats how computers are able to configure themselves and detect new devices added etc. The high speed data transfer busses are only used for the data transfers in most cases but most hardware also needs to transfer some configuration backwards and forwards too.

     

    http://www.datasheetspdf.com/mobile/947361/KLM4G1FE3B-B001.html

     

    enjoy the reading!

     

    --------

    edit

     

    Excerp from the datasheet

     

    image

     

     

    The CLK and CMD pins are used to even specify a data write operation, once this is done the data travels across the wider DATA bus where the CLK pin is still used by the host to signal the arrival of that data, also is the case with standard sdcards etc...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to e14 Contributor

    Always precise and punctual! Great Lucie image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to balearicdynamics

    Most emmc's are designed to operate as a direct sdcard would. Certainly as Roger points out you can use an SPI bus to communicate and send data but this is considered a slower speed alternative.

     

    Looking at the datasheet and connections I would imagine the emmc (which is designed to operate exactly like an sdcard) uses a method where read/write commands are sent then data is transfered seperatly over a wider bus. This method was generally kept a secret only allowing most people to use the SPI interface but I'd like to think that Samsung's emmc has its own version of the high speed data transfer built in.