Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Setting up Bluetooth on the Raspberry Pi 3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: cstanton
  • Date Created: 16 Mar 2016 1:01 AM Date Created
  • Last Updated Last Updated: 10 May 2021 7:23 PM
  • Views 17513 views
  • Likes 18 likes
  • Comments 61 comments
Related
Recommended

Setting up Bluetooth on the Raspberry Pi 3

Wireless at Last!

 

Now that it has been a few weeks since the release of the Raspberry Pi 3Raspberry Pi 3, support for the WiFi and Bluetooth chip has settled and you can use it with Raspbian. Support with Windows 10 IoT Core will be available in the early days via the Insider Program before it is pushed through to the full release.

 

As usual, with Raspbian ensure that you have your distribution up to date, with this guide we will be using Raspbian Jessie, at present it is still the ARMv7 32bit kernel. Connect your Raspberry Pi to the internet either via WiFi or Ethernet and run the following commands:

 

sudo apt-get update

sudo apt-get upgrade -y

sudo apt-get dist-upgrade -y

sudo rpi-update

 

Installing the Software

 

From a console terminal, either from within your desktop environment, which at the time of writing the window manager is still LXDE. This will ensure your system is up to date.

 

Now you have a few options, you can install the following package:

 

sudo apt-get install pi-bluetooth

 

Which should install what you need to use the bluetooth portion of the chip, this installs the following packages which you can, if you want, install instead of pi-bluetooth:

 

sudo apt-get install bluez bluez-firmware

 

As the chip requires a firmware blob to work along with the driver. Bluez also installs a suite of tools. These will work from the console terminal. Should you wish to manage your bluetooth devices from your X environment, aka your windows manager, aka your desktop then you can install the following package:

 

sudo apt-get install blueman

 

After installing the software and drivers, reboot your Raspberry Pi. Unless you know otherwise, to load the driver for the adapter.

 

Terminal / Console

 

Bluez comes with a tool called 'bluetoothctl' which you can run from the console terminal, typing 'man bluetoothctl' does not give you a great deal of detail, so you have to type 'help' from within the software:

pi@raspberrypi:~ $ bluetoothctl

[bluetooth]# help

Available commands:

  list                       List available controllers

  show [ctrl]                Controller information

  select <ctrl>              Select default controller

  devices                    List available devices

  paired-devices             List paired devices

  power <on/off>             Set controller power

  pairable <on/off>          Set controller pairable mode

  discoverable <on/off>      Set controller discoverable mode

  agent <on/off/capability>  Enable/disable agent with given capability

  default-agent              Set agent as the default one

  scan <on/off>              Scan for devices

  info <dev>                 Device information

  pair <dev>                 Pair with device

  trust <dev>                Trust device

  untrust <dev>              Untrust device

  block <dev>                Block device

  unblock <dev>              Unblock device

  remove <dev>               Remove device

  connect <dev>              Connect device

  disconnect <dev>           Disconnect device

  version                    Display version

  quit                       Quit program

 

Now we are in bluetoothctl we can run the commands, first lets make sure that bluetooth is on, running and discovering devices:

 

image

With the commands 'power on', 'agent on' and 'scan on'. Though we likely only need 'power on' and 'scan on'.

image

image

Devices! and while the software is running we will see devices appear, change, delete, etc. We can then connect to a device using its MAC address. Basically, we are talking to the devices directly at the hardware layer, usually on your typical WiFi or Ethernet network this is done transparently to you and we only work with IP addresses. However with Bluetooth at this point, no.

 

image

We can also then pair and trust the device and do all the fun features of Bluetooth, provided these are successful.

 

GUI

Some consider the blueman package and software to be unstable, though the sources saying so are a bit dated by now and it may be somewhat more stable.

 

image

 

When you have the blueman package installed, you should have a nice Bluetooth icon in your system tray. If you left-click with a mouse connected to your Raspberry Pi you should get a menu with all of the, hopefully, self explanatory options for you to play with, which for some reason I could not capture with scrot/imagemagick, so you get a nice photograph:

 

image

 

Yum, pixelated (it was an old Dell monitor). If we want to scan for devices, similarly to using the 'scan' command for bluetoothctl then we select 'Devices' on the menu:

 

image

And from here we can see what is available in the vicinity, you may be surprised at suddenly finding your neighbours smart television or phone, you will find out how thin your walls really are. It can be more fun in the office at work.

 

However, let us select "setup a new device":

 

{gallery} Add New Device

image

Add New Devices: Introduction

image

Add New Device: Choose the Device to Connect to

image

Add New Device: Choose a pairing code

 

However, what I discovered is that the passkey method is practically deprecated or ignored, it may be applicable for older Bluetooth software or devices, but these days you will get a prompt appear (and for myself, then hide) on Raspbian, next to the icon for blueman, there will be a message, and in this message it will display a message like:

 

This device wants to pair with this machine, with this code xxxxxxxx, do you want to permit or deny?

 

This likely happens with new devices such as smart phones and televisions, as a security measure that you are physically holding or looking at the device in question. Of course you then 'permit' on either the device or Raspbian and the two will be paired. Allowing you to then setup drivers for your Bluetooth device functionality, to use it as a modem, in the case of a phone, share its internet access or simply send files to and from it. Potentially, you can even use it as an audio device!

 

Attaching to devices such as headsets tends to be easier, and usually does not use a pairing code. A standard is usually four zeroes (0000) with most consumer devices.

 

Have you setup your Raspberry Pi 3 with Bluetooth?

Perhaps speakers, or even the Panasonic Grid Eye sensor boardPanasonic Grid Eye sensor board? (yes, it has bluetooth). I am not sure what I will do with mine, but after I backed the Bluetooth Audio Link I may use it with some speakers, or perhaps add the functionality to remote control a Plex Server.

  • bluetooth
  • ble
  • raspberry pi 3 bluetooth
  • ble 4.0
  • bluetooth low energy 4.0
  • ble 4.1
  • raspberry_pi
  • bluetooth_4.1
  • raspberry pi
  • bluetooth 4
  • bluetooth 4.1
  • raspberry_pi_space
  • raspberry_pi_3_bluetooth
  • bluetooth 4.0
  • bluetooth low energy
  • raspberry pi 3
  • ble_4.1
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 10 years ago +3
    Nice! I just tried it - worked a treat with my keyboard following your instructions. The update/upgrade part is super important, I tried it first without that (I was curious lol). After the upgrade, I…
  • shabaz
    shabaz over 10 years ago +2
    Also, cool smartphone name ; )
  • bwelsby
    bwelsby over 10 years ago in reply to cstanton +2
    Christopher Stanton wrote: So just for clarification, you're pairing more than one device at once to the Raspberry Pi? Yep and playing music from one device through the RPi to the other BTW another cause…
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    Check Wolfteck: Raspberry Pi - Bluetooth iPhone Tethering for help.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57

    Ok I installed the tools per the instructions.

    Using the graphical interface I could not get the devices to pair so I used the control line insteadt.

    I set the Vizop ZRA700 into pairing mode

    then on the pi

     

    pi@raspberrypi:~ $ bluetoothctl

    [NEW] Controller B8:27:EB:FD:93:94 raspberrypi [default]

    [NEW] Device 00:19:9D:7C:4F:A7 VIZIO XRA700 Remote Control

    [bluetooth]# devices

    Device 00:19:9D:7C:4F:A7 VIZIO XRA700 Remote Control

    [bluetooth]# trust 00:19:9D:7C:4F:A7

    [CHG] Device 00:19:9D:7C:4F:A7 Trusted: yes

    Changing 00:19:9D:7C:4F:A7 trust succeeded

    [bluetooth]# pair 00:19:9D:7C:4F:A7

    Attempting to pair with 00:19:9D:7C:4F:A7

    Failed to pair: org.bluez.Error.ConnectionAttemptFailed

    [bluetooth]# connect 00:19:9D:7C:4F:A7

    Attempting to connect to 00:19:9D:7C:4F:A7

    Failed to connect: org.bluez.Error.Failed

    [bluetooth]# connect 00:19:9D:7C:4F:A7

    Attempting to connect to 00:19:9D:7C:4F:A7

    [CHG] Device 00:19:9D:7C:4F:A7 Connected: yes

    [CHG] Device 00:19:9D:7C:4F:A7 Modalias: bluetooth:v0058p2000d011B

    [CHG] Device 00:19:9D:7C:4F:A7 UUIDs:

    00001124-0000-1000-8000-00805f9b34fb

    00001200-0000-1000-8000-00805f9b34fb

    [CHG] Device 00:19:9D:7C:4F:A7 Paired: yes

    Connection successful

    [CHG] Device 00:19:9D:7C:4F:A7 Connected: no

    [bluetooth]# exit

     

    Reran bluetoothctl

    [DEL] Controller B8:27:EB:FD:93:94 raspberrypi [default]

    [bluetooth]# connect 00:19:9D:7C:4F:A7

    Attempting to connect to 00:19:9D:7C:4F:A7

    [CHG] Device 00:19:9D:7C:4F:A7 Connected: yes

    Connection successful

    [bluetooth]#

     

    The icon in the screen turns green and then after a few minutes turns off.

    Checking status

    bluetooth]# paired-devices

    Device 00:19:9D:7C:4F:A7 VIZIO XRA700 Remote Control

     

    I try to reconnect without having the Vizio in pair mode

     

    [bluetooth]# connect 00:19:9D:7C:4F:A7

    Attempting to connect to 00:19:9D:7C:4F:A7

    Failed to connect: org.bluez.Error.Failed

    Turn pair mode on and it reconnects.

    In the GUI it shows the Vizio with the following icons

    TRusted and bonded

    to the right it shows an Icon for I think touchpad a green stripped bar and a blue wireless symbol with a blue square above it.

     

    I appears if I dont do anything on the remote it disconnects.

    I do see lots of activity in the status bar on the GUI pa panel for bluetooth

    If I don't do anything again with the remote if disconnects.

    When the remote is connected I cannot seem to make it do anything no pointer movement or keyboard entry.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    Usually when I follow instructions and does not work, I go back and repeat to find I missed a key element that fixes it.

    At least I can document what I did to give to someone else as more knowledgeable which is needed to help here.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Great instructions. I just got a PI 3 and am learning as I go . I was able to pair a Vizio XRA700 remote to the PI 3 following thes instructions but nothing works on it. No touchpad /Keyboard etc. Is there a driver or scrip I need to fix to recognize this as a multi function remote?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to clem57

    By the way, this is not BLE, but just normal Bluetooth for audio.

    (The Pi 3 hardware supports BLE, but normal Bluetooth is what is supported by headsets).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to cstanton

    I tested playing music to the bluetooth speaker from the RPi whilst copying files to and from my  NAS server via WiFi  at the same time and that was fine.

     

    Yes the investigations continue image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to cstanton

    Well partially true. On the BLE side, the software can control 98% of activity. Turn off advertising can save most of the activity. I will leave WiFi  for others to comment.

    Clem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 10 years ago in reply to bwelsby

    My thoughts are that it could too much for the antenna to handle, I think it requires testing!

     

    From my understanding, WiFi has traffic going over the antenna even if you're not actively using it, there are beacons being sent/received all the time. The same can be said for Bluetooth, along with it being on 2.4Ghz which is typically an over saturated frequency.

     

    So the question is, is this just the software? Or is this reaching a bandwidth limit? The investigations continue!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to cstanton

    Christopher Stanton wrote:

     

    Have you also connected the Pi to a WiFi access point, at the same time?

    Yes but there was little to no WiFi traffic at the time.

     

    Just run another test::

    1. RPi configured with audio out connected to HDMI  (Not bluetooth speaker)

    2. Normal TV connected to RPi HDMI

    3. Only Kindle Fire connected to RPi via bluetooth ( On kindle the RPi comes up as bluetooth headset)

     

    Play music from Kindle via bluetooth to RPi  audio out to TV  sounds  distorted and breaking up.

    Tried again but from a mobile phone rather than Kindle  - same result.

    Playing music on the  RPi itself no problem

     

    Looks like it may be an issue with the part of the bluetooth software that handles audio input.

    I will investigate further tomorrow.

     

    Brian

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to cstanton

    So use BLE and 802n same time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>