Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Which accessories are compatible with the New Raspberry Pi 4 Model B?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 19 Jun 2019 1:28 PM Date Created
  • Last Updated Last Updated: 25 Jun 2019 4:10 PM
  • Views 12323 views
  • Likes 7 likes
  • Comments 15 comments
Related
Recommended

Which accessories are compatible with the New Raspberry Pi 4 Model B?

image

NEW! Raspberry Pi 4

Technical Specifications | GPIO Pin Out | Unboxing Video | Benchmark Tests | Comparison Chart | FAQ | Quiz | Pi Accessories | Pi Projects | RoadTest

 

 

 

To give you some context to this post, first, meet the new Raspberry Pi 4 Computer.

It has the same physical almost "Credit Card Size" footprint but some major changes to the I/O which could interfere with your accessory choices.

 

Unsupported video URL format.

 

Raspberry Pi 4 Model B 1GB RAMRaspberry Pi 4 Model B 2GB RAMRaspberry Pi 4 Model B 4GB RAM
  • 1.5-GHz Quad Core Cortex-A72
  • Dual Micro-HDMI (Up to 4Kp60)
  • 5V/3A USB type C
  • 2x USB 3.0 and 2x USB 2.0
  • 1GB RAM

 

RASPBERRY PI 4 MODEL B, 1GBRASPBERRY PI 4 MODEL B, 1GB

  • 1.5-GHz Quad Core Cortex-A72
  • Dual Micro-HDMI (Up to 4Kp60)
  • 5V/3A USB type C
  • 2x USB 3.0 and 2x USB 2.0
  • 2GB RAM

 

RASPBERRY PI 4 MODEL B, 2GBRASPBERRY PI 4 MODEL B, 2GB

  • 1.5-GHz Quad Core Cortex-A72
  • Dual Micro-HDMI (Up to 4Kp60)
  • 5V/3A USB type C
  • 2x USB 3.0 and 2x USB 2.0
  • 4GB RAM

 

RASPBERRY PI 4 MODEL B, 4GBRASPBERRY PI 4 MODEL B, 4GB

 

Raspberry Pi is going through physical changes

 

The Older Raspberry Pi 3 Model B+The NEW Raspberry Pi 4 Model B
imageimage
So what has changed?

New USB 3 Ports and the (Now Gigabit) Ethernet Port has changed sides!

imageimage
Micro USB and Full Size HDMIDual Micro-HDMI and USB-C Type

 

Will my old case fit the New Raspberry Pi 4?

Fairly unlikely that your old case will fit and if it does It likely wont have I/O holes in the right places for the new Micro HDMI, USB 3, USB C and Ethernet

 

Will I need a new charger for the Raspberry Pi 4?

Yes. This one swap is the greatest positive, you are now less constrained and less likely to get "Brown Outs" caused by power hungry peripherals.

 

Will my GPIO Hat work on the new Raspberry Pi?

Very Likely! The Raspberry Pi 40Pin GPIO is built to be backwards compatible! You can double-check this here: Raspberry Pi 4 Model B Default GPIO Pinout with PoE Header

 

Will I need a new version of the PoE hat?

No, the PoE HAT designed for the Raspberry Pi 3 Model B+ is fully compatible with the Raspberry Pi 4 Model B.

 

element14 Recommended Accessories

Due to the change in board layout and the new USB Type C power connector, we recommend the following accessories.

 

{tabbedtable} Tab LabelTab Content
USB Power Supplies

USB C Power Supplies

image

USB C Power SupplyManufacturer
5.1V, 3A USB-C PSU - UK WHITERaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - EU WHITERaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - US WHITERaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - AU WHITERaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - UK BLACKRaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - EU BLACKRaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - US BLACKRaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - AU BLACKRaspberry PiBuy NowBuy Now
Micro HDMI to HDMI Cable

Micro HDMI to HDMI Cable

image

Micro HDMI to HDMI CableManufacturer
1M MICRO-HDMI TO HDMI CABLE - WHITERaspberry PiBuy NowBuy Now
2M MICRO HDMI TO HDMI CABLE - WHITERaspberry PiBuy NowBuy Now
1M MICRO-HDMI TO HDMI CABLE - BLACKRaspberry PiBuy NowBuy Now
2M MICRO HDMI TO HDMI CABLE - BLACKRaspberry PiBuy NowBuy Now
Compatible Cases

Compatible Cases

image

Raspberry Pi 4 CasesManufacturer
Official Pi 4 CasesRaspberry PiBuy NowBuy Now
Official Pi 4 CasesRaspberry PiBuy NowBuy Now
RASPBERRY PI 4 CASE - BLACKMulticomp ProBuy NowBuy Now
RASPBERRY PI 4 CASE - WHITEMulticomp ProBuy NowBuy Now
RASPBERRY PI 4 CASE - CLEARMulticomp ProBuy NowBuy Now
RASPBERRY PI 4 CASE - REDMulticomp ProBuy NowBuy Now
RPI 4 CASE W/PWR BUTTON - BLACKMulticomp ProBuy NowBuy Now
RPI 4 CASE W/PWR BUTTON - WHITEMulticomp ProBuy NowBuy Now
RPI 4 CASE W/PWR BUTTON - CLEARMulticomp ProBuy NowBuy Now
RPI 4 CASE W/PWR BUTTON - REDMulticomp ProBuy NowBuy Now



 

Want to know more?

Meet The New Raspberry Pi 4 Model B - element14 Presents

Raspberry Pi 4 Model B - Technical Specifications

Raspberry Pi 4 Model B Frequently Asked Questions (FAQ)

Benchmarking the Raspberry Pi 4 Model B

Which accessories are compatible with the New Raspberry Pi 4 Model B?

Raspberry Pi 4 Model B Default GPIO Pinout with PoE Header

Do You Know Your Pi from Pie? Raspberry Pi Quiz!

Eben Upton talks about the new Raspberry Pi 4 Model B

 

Want to buy the new Raspberry Pi 4 Model B?

 

Product NameManufacturer
RASPBERRY PI 4 MODEL B, 1GBRaspberry PiBuy NowBuy Now
RASPBERRY PI 4 MODEL B, 2GBRaspberry PiBuy NowBuy Now
RASPBERRY PI 4 MODEL B, 4GBRaspberry PiBuy NowBuy Now
  • raspberry pi 4 accessories
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • jomoenginer
    jomoenginer over 7 years ago +4
    Oh. my! Looks like the 2Gb and above use a USB-C power adapter so a new power source will be required for these. The ethernet port location swap and dual HDMI will result in new cases being released for…
  • shabaz
    shabaz over 7 years ago +4
    Hi! Maybe it's worth adding a fan and heatsinks to this list. Here's some suggestions: Ceramic heatsink for the CPU, 15x15x2mm: MPC151525T MPC151525T Ceramic heatsink for the RAM, 10x10x2mm: MPC101020T…
  • colporteur
    colporteur over 7 years ago +3
    No fair, after reading your post I now feel I am forced to apply for the RoadTest the Raspberry Pi 4 Model B (2GB) so I can experience all the new changes for myself. Great post, thanks.
  • mconners
    mconners over 7 years ago in reply to travellingkiwi

    Well, technically they all do image

     

    Just the others have that, plus some. image

     

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • travellingkiwi
    travellingkiwi over 7 years ago

    So all 3, the -1GB, -2GB and -4Gb have 1GB of RAM? image

     

    Yeah, I know it's a typo... Someone forgot to check it...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 7 years ago in reply to Jan Cumps

    Thanks Jan Cumps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago

    There is a -C missing under the last of the four Pi photos:

     

    Dual Micro-HDMI and USB Type-C

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago

    Oh. my!

     

    Looks like the 2Gb and above use a USB-C power adapter so a new power source will be required for these.  The ethernet port location swap and dual HDMI will result in new cases being released for it, so fire up those 3d printers.  You gotta dig the 1.5GHz quad-core 64-bit ARM Cortex-A72 CPU and the VideoCore VI graphics where they are switching to the Mesa "V3D" video driver supporting OpenGL ES 3.x and 4K .  They are also switching to Debian 10 Buster which should be interesting.  The 4Gb version will jump to $55 US where the 1Gb version will stay at $35 US.

     

    I can't wait to get me mits on the the new RasPi 4 B.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<