Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Introducing The New Raspberry Pi 4 Model B 8GB
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 28 May 2020 5:50 AM Date Created
  • Last Updated Last Updated: 28 May 2020 8:11 AM
  • Views 14259 views
  • Likes 12 likes
  • Comments 12 comments
Related
Recommended

Introducing The New Raspberry Pi 4 Model B 8GB

image

NEW! Raspberry Pi 4

Technical Specifications | GPIO Pin Out | Unboxing Video | Benchmark Tests | Comparison Chart | FAQ | Quiz | Pi Accessories | Pi Projects | RoadTest

 

 

 

Introducing the new addition to the Raspberry Pi 4 line, The Raspberry Pi 4 Model B 8GB.

 

This revision of the ever popular Raspberry Pi will be a welcome addition to most serious or even casual users.

It has the same physical footprint as the other Raspberry Pi 4 range, with some slight changes to the PCB, and TWICE the ram as the previous most powerful, 4GB, unit.

Users of the Raspberry Pi 4 have been crying out for more power and the Raspberry Pi Foundation has heard their call. This 8GB Raspberry Pi will give you the RAM headroom to open more chrome tabs and give your applications way more wiggle room.  This welcome upgrade will really help people use the Raspberry Pi 4 as a day to day computer.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

RASPBERRY PI 4 MODEL B, 8GBRASPBERRY PI 4 MODEL B, 8GB

 

Buy The Raspberry Pi 4 8GB

Buy the Raspberry Pi 4 Model B 8GB here.

 

NEW! Raspberry Pi 4 Model B 8GB RAM
  • 1.5-GHz Quad Core Cortex-A72
  • Dual Micro-HDMI
    (Up to 4Kp60)
  • 5V/3A USB type C
  • 2x USB 3.0 and
  • USB 2.0
  • 8GB RAM
RASPBERRY PI 4 MODEL B, 8GBRASPBERRY PI 4 MODEL B, 8GB

 

 

Raspberry Pi 4 Model B
1GB RAM
Raspberry Pi 4 Model B
2GB RAM
Raspberry Pi 4 Model B
4GB RAM
  • 1.5-GHz
    Quad Core Cortex-A72
  • Dual Micro-HDMI
    (Up to 4Kp60)
  • 5V/3A USB type C
  • 2x USB 3.0
  • 2x USB 2.0
  • 1GB RAM

 

RASPBERRY PI 4 MODEL B, 1GBRASPBERRY PI 4 MODEL B, 1GB

  • 1.5-GHz
    Quad Core Cortex-A72
  • Dual Micro-HDMI
    (Up to 4Kp60)
  • 5V/3A USB type C
  • 2x USB 3.0
  • 2x USB 2.0
  • 2GB RAM

 

RASPBERRY PI 4 MODEL B, 2GBRASPBERRY PI 4 MODEL B, 2GB

  • 1.5-GHz
    Quad Core Cortex-A72
  • Dual Micro-HDMI
    (Up to 4Kp60)
  • 5V/3A USB type C
  • 2x USB 3.0
  • 2x USB 2.0
  • 4GB RAM

 

RASPBERRY PI 4 MODEL B, 4GBRASPBERRY PI 4 MODEL B, 4GB

imageimage

The Board that should not have existed.

image

Some of you may remember that when the initial versions of the Raspberry Pi 4 launched, the Compliance leaflet mentioned a 8GB Variant, to which all hopes were quickly squashed as a typo.
To quote Eben Upton:

While we launched with 1GB, 2GB and 4GB variants, even at that point we had our eye on the possibility of an 8GB Raspberry Pi 4. We were so enthusiastic about the idea that the non-existent product made its way into both the Beginner’s Guide and the compliance leaflet.

The BCM2711 chip that we use on Raspberry Pi 4 can address up to 16GB of LPDDR4 SDRAM, so the real barrier to our offering a larger-memory variant was the lack of an 8GB LPDDR4 package. These didn’t exist (at least in a form that we could address) in 2019, but happily our partners at Micron stepped up earlier this year with a suitable part. And so, today, we’re delighted to announce the immediate availability of the 8GB Raspberry Pi 4, priced at just $75.

 

How to Identify your Raspberry Pi 4 8GB

 

To Identify the amount of ram on your Raspberry Pi 4 you simply need to have a look at the numbers written on the RAM Chip and match them to this handy guide:

 

1GB - 4HBMGCJ

2GB - D9WHZ

4GB - D9WHV

8GB - D9ZCL

 

image

Raspberry Pi 4 8GB - D9ZCL

 

 

Raspberry Pi 4 8GB PCB Changes

 

As we spotted in our unboxing video the Raspberry Pi 4 8GB has some PCB changes that help out the new beefier memory package.

James at the Raspberry Pi Foundation has shuffled the power supply components around the board, removing a switch-mode power supply from the right-hand side of the board next to the USB 2.0 sockets and adding a new switcher next to the USB-C power connnector.

 

imageimage

In addition to the changes in power supply components the Raspberry Pi 4 8GB has had some changes to the silkscreen on the back.

 

 

image

 

Will my old case fit the New Raspberry Pi 4?

Fairly unlikely that your pre-raspberry pi 4 case will fit and if it does It likely wont have I/O holes in the right places for the new Micro HDMI, USB 3, USB C and Ethernet, but any case made for any version of the Raspberry Pi 4 will fit.

 

Will I need a new charger for the Raspberry Pi 4?

Yes. This one swap is the greatest positive, you are now less constrained and less likely to get "Brown Outs" caused by power hungry peripherals.

 

Will my GPIO Hat work on the new Raspberry Pi?

Very Likely! The Raspberry Pi 40Pin GPIO is built to be backwards compatible! You can double-check this here: Raspberry Pi 4 Model B Default GPIO Pinout with PoE Header

 

Will I need a new version of the PoE hat?

No, the PoE HAT designed for the Raspberry Pi 3 Model B+ is fully compatible with the Raspberry Pi 4 Model B.

 

element14 Recommended Accessories

Due to the change in board layout and the new USB Type C power connector, we recommend the following accessories.

 

{tabbedtable} Tab LabelTab Content
USB Power Supplies

USB C Power Supplies

image

USB C Power SupplyManufacturer
5.1V, 3A USB-C PSU - UK WHITERaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - EU WHITERaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - US WHITERaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - AU WHITERaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - UK BLACKRaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - EU BLACKRaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - US BLACKRaspberry PiBuy NowBuy Now
5.1V, 3A USB-C PSU - AU BLACKRaspberry PiBuy NowBuy Now
Micro HDMI to HDMI Cable

Micro HDMI to HDMI Cable

image

Micro HDMI to HDMI CableManufacturer
1M MICRO-HDMI TO HDMI CABLE - WHITERaspberry PiBuy NowBuy Now
2M MICRO HDMI TO HDMI CABLE - WHITERaspberry PiBuy NowBuy Now
1M MICRO-HDMI TO HDMI CABLE - BLACKRaspberry PiBuy NowBuy Now
2M MICRO HDMI TO HDMI CABLE - BLACKRaspberry PiBuy NowBuy Now
Compatible Cases

Compatible Cases

image

Raspberry Pi 4 CasesManufacturer
Official Pi 4 CasesRaspberry PiBuy NowBuy Now
Official Pi 4 CasesRaspberry PiBuy NowBuy Now
RASPBERRY PI 4 CASE - BLACKMulticomp ProBuy NowBuy Now
RASPBERRY PI 4 CASE - WHITEMulticomp ProBuy NowBuy Now
RASPBERRY PI 4 CASE - CLEARMulticomp ProBuy NowBuy Now
RASPBERRY PI 4 CASE - REDMulticomp ProBuy NowBuy Now
RPI 4 CASE W/PWR BUTTON - BLACKMulticomp ProBuy NowBuy Now
RPI 4 CASE W/PWR BUTTON - WHITEMulticomp ProBuy NowBuy Now
RPI 4 CASE W/PWR BUTTON - CLEARMulticomp ProBuy NowBuy Now
RPI 4 CASE W/PWR BUTTON - REDMulticomp ProBuy NowBuy Now



 

Want to know more?

Meet The New Raspberry Pi 4 Model B - element14 Presents

Raspberry Pi 4 Model B - Technical Specifications

Raspberry Pi 4 Model B Frequently Asked Questions (FAQ)

Benchmarking the Raspberry Pi 4 Model B

Which accessories are compatible with the New Raspberry Pi 4 Model B?

Raspberry Pi 4 Model B Default GPIO Pinout with PoE Header

Do You Know Your Pi from Pie? Raspberry Pi Quiz!

Eben Upton talks about the new Raspberry Pi 4 Model B

 

Want to buy the new Raspberry Pi 4 Model B?

 

Product NameManufacturer
RASPBERRY PI 4 MODEL B, 1GBRaspberry PiBuy NowBuy Now
RASPBERRY PI 4 MODEL B, 2GBRaspberry PiBuy NowBuy Now
RASPBERRY PI 4 MODEL B, 4GBRaspberry PiBuy NowBuy Now
RASPBERRY Pi 4 MODEL B, 8GBRaspberry PiBuy NowBuy Now
  • raspberry pi 4 8gb
  • raspberry pi 4 accessories
  • rpi 4 8gb
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 6 years ago +4
    8GB was inevitable, wasn't it!
  • shabaz
    shabaz over 6 years ago +4
    That's very neat! I've never looked into the A72 specs, and now the Pi 4 finally has 8GB DDR4, just out of curiosity I wonder if with an SSD it outperforms the average consumer laptop (not that it replaces…
  • ashutosh_pandey
    ashutosh_pandey over 6 years ago in reply to shabaz +4
    It entirely depends on the use case. Making a comparison is not at all straightforward because the Raspberry Pi is an ARM SBC while all laptops and desktops are x86 based. This makes benchmarking so much…
  • ashutosh_pandey
    ashutosh_pandey over 6 years ago

    This is proper low end desktop replacement territory. When I roadtested the 2gb version of 4B: RoadTest the Raspberry Pi 4 Model B (2GB) - Review  the only thing I complained about was the lack of RAM, and now thats gone.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 6 years ago

    8GB was inevitable, wasn't it!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<