RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Adding Remotely Controlled Headlights to Tricopter
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: tomaja
  • Date Created: 15 Jan 2016 2:18 PM Date Created
  • Views 1064 views
  • Likes 2 likes
  • Comments 1 comment
Related
Recommended
  • illuminated_multirotor
  • tps92512
  • ppm
  • pwm
  • wuerth_elektronik
  • ledroadtestplus
  • würth

Adding Remotely Controlled Headlights to Tricopter

tomaja
tomaja
15 Jan 2016

Related posts:

Kit unboxing - LED RoadTest

Introduction to Bluetooth Low Energy Light Development Kit - CC2540TDK-LIGHT

Android Support for TI's BLE LED Control

MSP430FR4133 Launchpad - Magnetic North Visualisation

Illuminated Tricopter Upgrade - Adding an Addressable LED Ring

MSP430FR4133 BoosterPack for Illuminated Tricopter

Bookshelf Lights Using TI's CC2450 BLE LED Modules

MSP430FR4133 Launchpad with Custom BoosterPack in Action

MSP430FR4133 Launchpad with Custom BoosterPack in Action - appendix

MSP430FR4133 Launchpad with Custom BoosterPack update

Adding Remotely Controlled Headlights to Tricopter

 

Introduction

My final touch to this project are the remote controlled LED headlights. As most of the other reviewers did, I also decided to use Würth Elektronik’s high power LEDs for my illuminated tricopter. These LEDs are powered using TPS92512 buck converter from Texas Instruments. TPS92512 provides two different ways of dimming and I chose to use PWM as it’s more suitable for my project.

 

Remote control

Turing 9X is the remote controller that I use for all my aircrafts. It’s cheap but still provides most of the features that I need - except for being able to receive the telemetry data back from the aircraft. Since I don’t have the real telemetry this project is oriented to adding useful (or just good looking :)) LED indicators to my newest tricopter. Additionally, I wanted to be able to fly at night, at least to near proximity. That's why I planned to add high power headlights. I decided to dedicate one transmitter channel for headlight control. This station has 8 channels of which 4 are used to control the flight (pitch, roll, yaw and throtle), one is used to arm the controller and one is used to switch between flight modes (self-level, free flight etc.).

Receiver demodulates the transmitted signal and then converts the PPM signal into a set of PWM signals that are used to control the servos, ESCs, linear actuators and similar.

RC_Receiver_Timing_Diagram1.jpg

Receiver output signals are pulses with varying duration depending on potentiometer/switch positions on the transmitter but duty cycle has a very low range of 5%-10%.

Here, I'm showing the single decoded PWM signal that I use to control the brightness of Würth Elektronik high power LEDs:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

So, as TPS92512 expects 0% to 100% duty cycle I had to output the desired PWM depending on receiver pulse duration. For that I added a small function that utilises pulseIn function to my Energia sketch so that I can measure the input pulse duration. Also I had to shift the 5V input signal to 3.3V input for MSP430.

 

Here you can see both input and output signals (IN: yellow; OUT: blue). This output signal is further connected to TPS92512's PDIM pin to control the LED brightness.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

And here how the headlights operate (still not mounted):

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Next update with test flight footage will be ready when all parts are mounted and when I get rain-free window of time.

 

Cheers!

  • Sign in to reply

Top Comments

  • tonyboubady
    tonyboubady over 10 years ago +1
    Really COOL...
  • tonyboubady
    tonyboubady over 10 years ago

    Really COOL...