RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs MSP430FR4133 Launchpad with Custom BoosterPack in Action - appendix
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: tomaja
  • Date Created: 6 Jan 2016 1:15 PM Date Created
  • Views 981 views
  • Likes 3 likes
  • Comments 2 comments
Related
Recommended
  • msp430fr4133
  • illuminated_multirotor
  • boosterpack
  • ledroadtestplus
  • energia
  • launchpad

MSP430FR4133 Launchpad with Custom BoosterPack in Action - appendix

tomaja
tomaja
6 Jan 2016

Related posts:

Kit unboxing - LED RoadTest

Introduction to Bluetooth Low Energy Light Development Kit - CC2540TDK-LIGHT

Android Support for TI's BLE LED Control

MSP430FR4133 Launchpad - Magnetic North Visualisation

Illuminated Tricopter Upgrade - Adding an Addressable LED Ring

MSP430FR4133 BoosterPack for Illuminated Tricopter

Bookshelf Lights Using TI's CC2450 BLE LED Modules

MSP430FR4133 Launchpad with Custom BoosterPack in Action

MSP430FR4133 Launchpad with Custom BoosterPack in Action - appendix

MSP430FR4133 Launchpad with Custom BoosterPack update

Adding Remotely Controlled Headlights to Tricopter

 

Issues when running LaunchPad from BoosterPack power

I've been powering the MSP430FR4133 LaunchPad from USB for a while and life was beautiful image Then, I switched to using the BoosterPack to power all the components and here's where the trouble starts. LP started working sporadically, I could never guarantee that code will start executing. Then I started debugging the booster back since I assumed it's something I did wrong. I even decided to use a more powerful 3.3 voltage regulator (TI's LM1117-3.3) and had to etch another PCB to fit the different footprint image

 

However, this didn't help. So I continued debugging and at some point I decided to remove all the jumpers from the LP (not only the recommended ones - GND, 5V and 3.3V) - And that was it! It seems that when you have the programming jumpers connected LP will start at random. This is what happens with Energia, at least. CCS might behave better since it's using a different driver for debugger.

 

Anyway, this was good enough for me but at some point I got tired from removing 7 jumpers and putting them back on every time I flash and test an updated Energia sketch.

Today I decided to use a bit of hot glue and a piece of board to make single block of jumpers that are easy to remove and put back onto the LP.

 

image

 

image

 

Cheers!

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 10 years ago +1
    That's a neat trick! I'll have to remember that : ) It is irritating when some boards have so many jumpers (Raspberry Pi GertX boards are guilty of that) that it becomes hard to remember what does what…
  • mcb1
    mcb1 over 10 years ago +1
    Excellent trick. Well done. Mark
  • mcb1
    mcb1 over 10 years ago

    Excellent trick.

     

    Well done.

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago

    That's a neat trick!

    I'll have to remember that : )

     

    It is irritating when some boards have so many jumpers (Raspberry Pi GertX boards are guilty of that) that it becomes hard to remember what does what!