RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Aim-TTi SMU4201 Road Test | Power Supply and Load Experiments
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: Attila Tőkés
  • Date Created: 9 Jul 2023 5:00 AM Date Created
  • Views 2247 views
  • Likes 13 likes
  • Comments 6 comments
Related
Recommended
  • RoadTest
  • smu
  • aim-tti
  • SMU4201

Aim-TTi SMU4201 Road Test | Power Supply and Load Experiments

Attila Tőkés
Attila Tőkés
9 Jul 2023
Souring, Sinking and Measurement Experiments with the Aim-TTi SMU4201
  • 1. Specifications
  • 2. Experiments
    • 2.1. Power Supply Experiments
    • 2.2 Electronic Load Experiments
    • 2.3. Measuring a Zero-Ohm Link

Hi All! Let's continue the Road Test of the Aim-TTi SMU4201 Source Measure Unit (SMU)! Slight smile

Previous blog posts:
 Aim-TTi SMU4201 Road Test | Unboxing, First Look and User Interface 

1. Specifications

First, lets take a look on some values from the specification of the Aim-TTi SMU4201 source measure unit:

Feature

Ranges

Resolution
/ Slew Rate

Accuracy

Voltage

Measurement

(all modes
except MC)


20mV
200mV
2V
20V
200V

10nV
100nV
1µV
10µV
100µV

±0.06%rdg ± 50µV
±0.015%rdg ± 50µV
±0.015%rdg ± 50µV
±0.02%rdg ± 5mV
±0.02%rdg ± 5mV

Current
Measurement

(all modes
except MV)


200nA
2µA
20µA
200µA
2mA
20mA
200mA
1A
3A

100fA
1pA
10pA
100pA
1nA
10nA
100nA
1µA
1µA

±0.04%rdg ± 300pA
±0.03%rdg ± 300pA
±0.02%rdg ± 2nA
±0.02%rdg ± 2nA
±0.02%rdg ± 200nA
±0.02%rdg ± 2µA
±0.02%rdg ± 20µA
±0.07%rdg ± 100µA
±0.2%rdg ± 300µA


Voltage Source

(SV and
MHR modes)

±21V
±210V

210V/s
to 1.2V/µs

Same as voltage
measurement accuracy

Current Source or Load

(SC, LC, LR, LP
and MR modes)

±3.15A

3.15A
250MΩ
26.25W


3A/s to
36mA/µs

25W/s to
LP mode
0.25W/µs

Same as current
measurement accuracy

The specifications of the SMU4201 are really impressive. The measurement accuracy is about two orders of magnitude (100x) better compared to a handheld DMM. On the voltage / current sourcing and sinking side it meets the specification of a precision laboratory power supplies and electronic loads.

As far I can see the specification are on par with other SMU from the market. The more detailed comparison with competitors will also come in my final review.

Now let's try out some of the functionality offered by the instrument!

2. Experiments

The Aim-TTi QPX750SP is a 750W switching mode power supply I Road Test-ed in 2021. Back then, I compared several power supply units, including lab power supplies, power bricks and batteries. In this blog post I wanted to replicate some of the experiments with the Aim-TTi SMU4201 source measure unit, along with a set of experiments focusing the current sinking and measuring capabilities of the instrument.

image

The instruments used in this experiment are the Aim-TTI SMU4201, the Aim-TTi QPX750SP and the Keysight MSOX3034T oscilloscope.

2.1. Power Supply Experiments

In this first section we will test the behaviour of the two instruments when loaded with resistive, capacitive and inductive loads.

Resistive Loads

Most of the devices used in hobby electronics can be considered resistive loads, so I thought to put accent on this type of load.

The resistive loads used are floor heating sheet and various heating elements extracted from broken household appliances. Their resistance value with the current and power value at the tested voltages are shown in the table bellow:

Voltage

(V)

Resistance (Ω)
Current (A) | Power (W)

4.20 Ω

image


19.00 Ω

(36 Ω + 41 Ω)

image

36.00 Ω

image

93.00 Ω

image

3.3 0.79 2.59 ― ― ― ― ― ―
5 1.19 5.95 ― ― ― ― ― ―
10 2.38 23.81 0.53 5.26 ― ― ― ―
21 ― ― 1.11 23.21 0.58 12.25 ― ―
42 ― ― ― ― ― ― 0.45 18.87

Note: the test voltages values were chosen to mostly cover the 25W power envelope of the SMU4201.

Using the oscilloscope the noise / ripple values along with the rise and fall times during turn on and turn off actions were captured: 

Resistive Loads

Aim-TTi
SMU4201

Aim-TTi
QPX750SP

Waveforms

Noise
rms | p-p
(mV)

Turn
On / Off
Times
(ms)

Noise
rms | p-p
(mV)
Turn
On / Off
Times
(ms)

3.3 V

4.2 Ω

1.37
―
26.65

~3.0
―
~4.0

2.52
―
16.92

~150
―
~150

SMU4201
image image image

QPX750SP
image image image

5 V

4.2 Ω

1.33
―
24.41

~4.0
―
~4.0

1.33
―
13.35

~200
―
~350

SMU4201
image image image

QPX750SP
image image image

10 V

4.2 Ω

1.34
―
21.9

~3.5
―
~4.5

1.26
―
~13.34

~150
―
~50

SMU4201
image image image

QPX750SP
image image image

19 Ω

1.55
―
30.49

~2.5
―
~2.5

1.10
―
10.00
~150
―
~150

SMU4201
image image image

QPX750SP
image image image

21 V

19 Ω

1.85
―
28.93

~2.0
―
~ 2.5

1.10
―
10.00
~200
―
~150

SMU4201
image image image

QPX750SP
image image image

36 Ω

1.84
―
28.95

~1.5
―
~2.0

1.32
―
13.36
~175
―
~200

SMU4201
image image image

QPX750SP
image image image

42 V

93 Ω

2.37
―
38.53

~2.0
―
~1.5

1.33
―
13.61
~150
―
~175

SMU4201
image image image

QPX750SP
image image image

Note: the measures values were captured at the output terminal of the power supplies. However the test setup was far from perfect, so some noise is expected in the measured values.

As we can see both the SMU4201 and QPX750SP handles restive load excellently. The RMS noise / ripple is around ~1.0-2.5mV (including measurement noise) with peak-to-peak values under 40mV, with higher for the SMU4201. With the default settings the SMU4201 has much more aggressive turn on and off times (<5ms) compared to the QPX750SP (~200ms).

Negative voltages

The SMU4201 contrary to the QPX750SP can also supply negative voltages. I tested this at 21V with a 36Ω load:

Resistive Loads

Aim-TTi
SMU4201

Aim-TTi
QPX750SP

Waveforms

Noise
rms | p-p
(mV)

Turn
On / Off
Times
(ms)

Noise
rms | p-p
(mV)
Turn
On / Off
Times
(ms)

21 V

36 Ω

3.33
―
37.38

~2.5
―
~2.5

―

―

SMU4201
image image image

The measured values are similar to the ones obtained with positive voltages.

Capacitive Loads

Next, I wanted to try out some capacitive loads. What I used is five of 470 µF electrolytic capacitors connected in parallel:

image

The capacitors were tested at 5V with a current limit of 1.5A.

Note: the default OFF State Mode of the SMU4201 is 0V/100µA, and with this settings it takes "forever" to discharge this capacitors at turn off. For this reason I decided to set the OFF State Mode to ZERO, with the current limit configured above.

Capacitive Load

Aim-TTi
SMU4201

Aim-TTi
QPX750SP

Waveforms

Noise
rms | p-p
(mV)

Turn
On / Off
Times
(ms)

Noise
rms | p-p
(mV)
Turn
On / Off
Times
(ms)

5 V

5
x
470 µF

1.17
―
14.18

~120
―
~150

1.09
―
10.74

~200
―
~250

SMU4201
image image image

QPX750SP
image image image

Both the SMU4201 and the QPX750SP showed very low noise, with slightly lower turn on and off times for the SMU. In the case of the SMU there are some overshoots visible at turn on and off, probably caused by the aggressive slew rate settings.

Inductive Loads

As the last step I wanted to try out some inductive loads. First I wanted to use a 12V brushed DC motor, but because of the high inrush current and switching node, I gave up on that idea. Instead, I used one half of a common mode choke, which is basically an inductor of 6.8 mH:

image  image

The tests were done @ 1V with a current limit of 1.5A. In the inductor this caused an initial current spike, after which the current settled at around 0.7-0.9A.

Capacitive Load

Aim-TTi
SMU4201

Aim-TTi
QPX750SP

Waveforms

Noise
rms | p-p
(mV)

Turn
On / Off
Times
(ms)

Noise
rms | p-p
(mV)
Turn
On / Off
Times
(ms)

1 V

6.8 mH

1.39
―
22.62

~100?
―
~300

37.24
―
126.80

~50
―
~10

SMU4201

image image image image

QPX750SP

image image image

I must say the two power supply supplies did not liked my inductive load. Grin

First on the SMU4201 the over power protection (OPP) was tripped, so I needed to activate the High Reactance mode, and set the Slew Rate to the minimum value of 210V/s. Then sometimes the instrument and the inductor entered some resonance mode causing ~50V ripple.

Overshoots were present both with the SMU4201 and QPX750SP. When the setup stabilized the SMU managed to maintain a significantly lower noise level.

2.2 Electronic Load Experiments

A source measure unit (SMU) can both source and sink current. To test this capability of the SMU4201, the instrument was configured as an electronic load, while the QPX750SP acted as the power source.

image

The SMU4201 has 3 main Sink modes: load current (LC), load resistance (LR) and load power (LP). I tested the turn on and off behaviour of each mode, as well as switching between two load values.

Instead of measuring voltage, in these experiment I used a the Hantek CC-65 current clamp probe to take a look on the current waveforms produces by intrument.

Load Current
Mode

Aim-TTi
SMU4201

Waveforms

5 V

-100 mA
/
-200 mA

Turn On / Off
Times (ms):

0.150 / 0.250


100 <-> 200 mA
Times (ms):

0.150 / 0.200

SMU4201
image image
image image

Load Resistance
Mode

Aim-TTi
SMU4201

Waveforms

5 V

20 Ω
/
50 Ω

Turn On / Off
Times (ms):

0.200 / 0.300


20 <-> 50 Ω
Times (ms):

0.150 / 0.150

SMU4201
image image

image image

Load Power
Mode

Aim-TTi
SMU4201

Waveforms

5 V

2 W
/
4W

Turn On / Off
Times (ms):

0.150 / 0.300


2 <-> 4 W
Times (ms):

0.200 / 0.250

SMU4201
image image

image image

The produced waveform are clear, and does not contain any glitches. The turn on and off times, and well the load switching times of the SMU4201 are around 0.15 - 0.30 ms.

Sinking with negative voltages

The SMU4201 is a four quadrant instrument, so along sinking negative (-) currents from positive (+) voltage sources (quadrant Q4), it should also be able to sink positive currents (+) from negative (-) voltage sources (quadrant Q2).

For some weird reason the Load operation modes (CC, CR, CP) can only be used with positive (+) voltages and therefore negative (-) currents. To sink current from negative (-) voltages, we must use one of the source voltage or current mode.

I managed to get it working in Source Voltage (SV) mode with setting a negative source voltage near zero (-0.5V) with the desired current limit applied in both polarities (+/-). Because I was a bit afraid I will accidentally apply negative voltages to the output of the QPX750SP, I decided to do the negative voltage sink test with a 1.5V AAA battery.

Constant Current
Sink
(negative supply)

Aim-TTi
SMU4201

Waveforms

-1.5 V

+100 mA
/
+50 mA

Turn On / Off
Times (ms):

~1.0 / ~7.0


100 <-> 50 mA
Times (ms):

~1.5 / ~0.0

SMU4201
image image
image image

2.3. Measuring a Zero-Ohm Link

Along souring and sinking current, the SMU4201 can also be used as a 6½ digit resolution multimeter. It can measure voltages, currents and resistances and has support for 4-wire measurements.

To demonstrate the measurement capability of the instrument, I choose to do a 4-wire resistance measurements of a "zero-ohm link":

image

A "zero-ohm link" is a resistor with a nominal 0 Ω value, and it is used for various purposes. In reality, according to Wikipedia the resistor will have a resistance of around 10-50 mΩ, so it is a great way to demonstrate the 4-wire measurement technique.

The purpose of 4-wire measurement techniques is to eliminate the measurement errors resulting from the contact and lead resistances of the test leads. With 4-wire measurement we are using 2 wires dedicated to passing the test current, and an another two to measure voltage.

For this test I used a random SMD 0805 package "zero-ohm link" soldered to prototype board, along some right angle pin headers on each side. This setup allows connecting 4 test clips, 2 on side of the resistor.

The SMU4201 was set up for resistance measurements first in 2-wire, then in 4-wire mode. The test current used was 100 mA.

Using the 2-wire mode the measure resistance was 794 mΩ, it was really unstable and I even needed temporarily apply 1A test current to somewhat stabilize the measurement.

image 

Switching to the 4-wire measurement technique immediately showed the real 17.20 mΩ value value of the resistor:

image

and the measurement remained stable.

In the next weeks, I will get into the programming / remote control side of the instrument. This will include among others automated experiments with low power wireless devices, battery characterization and simulation.

Hope you enjoyed this update! Slight smile

  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 3 years ago +1
    Great progress so far! I have been looking forward to the reviews of this SMU. I really appreciate the effort you're going through to take and post relevant scope screenshots. For some weird reason…
  • jc2048
    jc2048 over 3 years ago +1
    Yes, I enjoyed the update. Thanks for taking the roadtest seriously and doing all of this in addition to the review itself. Your Hantek has 'up to 20kHz' bandwidth, but that might only be for small currents…
  • DAB
    DAB over 3 years ago

    Very good test report.

    I might have to get one of these.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Attila Tőkés
    Attila Tőkés over 3 years ago in reply to Attila Tőkés

    Just measured the rise time of the Hantek CC-65 and it looks to be around 12-15µS:

    image
    (10 sample averaging; the yellow trace is the voltage source)

    The fastest edge measured with the SMU4201 is around 50µS, so the probe does not seems to be a limiting factor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Attila Tőkés
    Attila Tőkés over 3 years ago in reply to jc2048

    Hmm, I completely forgot that the Hantek CC-65 has only 20 kHz of bandwidth. Slight smile According to some online calculator 20 kHz corresponds to 17.5 µS rise time, which is kind of close to what we are measuring. A bit later, I will try to measure the bandwidth of probe.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 3 years ago

    Yes, I enjoyed the update. Thanks for taking the roadtest seriously and doing all of this in addition to the review itself.

    Your Hantek has 'up to 20kHz' bandwidth, but that might only be for small currents. Do you think you might be measuring the current probe risetime, rather than that of the SMU?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Attila Tőkés
    Attila Tőkés over 3 years ago in reply to baldengineer

    There are 3 load modes: Load Current (LC), Load Resistance (LR) and Load Power (LP), and these seems to be limited to positive (+) voltages only.

    There is a block diagram in the SMU4201's datasheet showing a dedicated Load module:
    image

    It may be the case that the 3 Load modes uses this dedicated load module, and the module is limited to positive (+) voltages.

    However, the Voltage Source is also capable of sinking current, both from the positive (+) or negative (-) voltages. It is the UI configuration which is bit cumbersome in this mode, as both a current limit and a "threshold" voltage is needed to be set. Also, in Source Voltage (SV) mode we can only configure sinking current in constant current mode. There are no constant resistance or constant power settings, which in the Load modes are implemented via a SMU's digital feedback loop. This may just be firmware limitation, as the feedback loop should be also available in the Source Voltage (SV) mode.

    I'm not sure about the Current Source. I will try to take a look into this later.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>