RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs Keysight Technologies U1282A Digital Multimeter - Applications - Water Level Sensing
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: dougw
  • Date Created: 12 May 2016 4:34 AM Date Created
  • Views 1533 views
  • Likes 6 likes
  • Comments 5 comments
Related
Recommended
  • u1282a
  • water_level
  • capacitive sensor
  • keysight_technologies
  • road_test

Keysight Technologies U1282A Digital Multimeter - Applications - Water Level Sensing

dougw
dougw
12 May 2016

One of the applications I wanted to include in this road test is capacitance water level sensors because you can get an accurate depth measurement for almost no cost as long as you have a meter that can measure capacitance The Keysight  U1282AU1282A meter does measure capacitance and is useful for testing and calibrating such sensors The physics behind why this technique works is a little trickier than it looks but I want to provide a bit of a feel for the technique without delving into math Basically the capacitance between 2 conductive plates is proportional to their area and the dielectric constant or relative permittivity of the intervening material It is also inversely proportional to the distance between plates

If we have a 2 conductive capacitor plates immersed in water, where one plate is bare metal and the other is insulated with a film of PVC plastic, a capacitor is formed with 2 dielectric materials between the plates - PVC and water. The permittivity of PVC is 3.4 and the permittivity of water is 80.4. The way I think of the combined permittivity is it is like the combined capacitance of a large capacitor in series with a small capacitor, so something like 3.3 in this example, which is very close to the smaller permittivity. This low permittivity doesn't help make capacitance in water high, but what the high permittivity of water does is effectively move the capacitive charge of the bare plate close to to the PVC insulation, reducing the effective plate separation distance to just the thickness of the insulation. This effect does make the capacitance dramatically higher.

If the 2 plates are in air the situation is reversed because the PVC has a higher permittivity than air, but it only effectively moves the plates closer by the thickness of the insulation.

If the plates have significant physical separation and are partly in air and partly immersed, the capacitance will be completely dominated by the immersed portion. When making a sensor that uses this property, the plates can be metallic strips, round wires, or rods of any uniform cross-section. To get higher capacitance from the sensor, make the wire diameter larger and the insulation thinner, or use insulation with a higher dielectric constant. Here are the dielectic constants of a few wire insulation materials plus air and water:

MaterialDielectric Constant
Air1
Teflon2.1
PVC3.4
PVDF12
Water80.4

Here is a little video demonstrating the Keysight directly measuring water depth via capacitance:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

If you want to develop a really accurate capacitance sensor system, you may need to minimize the influence of people, objects and stray electric fields on the sensor capacitor. There are a number of ways to tackle this:

  1. if you are able to put the probe into the water, the ground electrode (capacitor plate) can be a stainless steel tube. The other plate is an insulated wire or rod right down the middle of the tube. The tube acts like a Faraday shield.
  2. If you need the sensor probe to be outside the tank, you can partly shield it in a similar way - use a ground strip on either side of the sense electrode and put a conductive cover over the sense strip connecting to both ground strips.

In both cases there should be enough air around the sense conductor to keep the air capacitor from being too significant.

Another technique is to employ out-of-phase signals. This is explained in an app note from TI.

In summary capacitance is a great way to easily inexpensively and accurately measure water levels of any depth and the Keysight  U1282AU1282A is a great asset in working with such sensors Especially because it will not be harmed if you happen to drop it in the water.

 

Links to other installments of this road test:

unboxing

component and DC voltage measurements exploration

waveform measurements exploration

teardown research

applications exploration - component sorting

applications exploration - water level measurement

applications exploration - sensor datalogging

formal road test link

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 10 years ago +1
    Wonderful video. I learn a lot by the testing you did. Thanks.
  • Jan Cumps
    Jan Cumps over 10 years ago +1
    I particularly like your 'out of the tank' measurements. I have experience doing out-of-container measurements with ultrasone (the ultrasone signal bounces against the border where the liquid meets air…
  • DAB
    DAB over 10 years ago +1
    Great road test Douglas. I have been thinking about doing measurements of different materials and this device might be very useful. DAB
  • hudoj
    hudoj over 10 years ago

    That’s an approach I had not seen before. Thanks I will do a
    few tests and work out the scaling.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 10 years ago in reply to Jan Cumps

    Capacitance has a few drawbacks, as you mentioned, but it can measure to 1 mm if you want need precision. I might add a section on driven shields which can eliminate stray capacitance.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Great road test Douglas.

     

    I have been thinking about doing measurements of different materials and this device might be very useful.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago

    I particularly like your 'out of the tank' measurements. I have experience doing out-of-container measurements with ultrasone (the ultrasone signal bounces against the border where the liquid meets air and echos back to the source).

    It's nice to see your alternative.

     

    I think your approach has the advantage of not requiring fast precise timers or a microcontroller - a decent sensitive capacitor measurement circuit would do. The downside is that you need build plates outside the container that go the full height.

    With ultrasone, you need devices that can record the (very) fast response time of your ultrasone signal. On the other hand, you just need one sensor tagged to the outside bottom of the container.

     

    I wonder how the precision between the two mechanisms compare...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago

    Wonderful video. I learn a lot by the testing you did. Thanks.