RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs TI SWIFT™︎ Power Module EVM RoadTest: Module Review and Test Setup
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: Jan Cumps
  • Date Created: 2 Mar 2018 2:32 PM Date Created
  • Views 3979 views
  • Likes 7 likes
  • Comments 20 comments
Related
Recommended
  • RoadTest
  • switching_controller
  • smps
  • dc dc converters
  • power electronics
  • ti_rt

TI SWIFT™︎ Power Module EVM RoadTest: Module Review and Test Setup

Jan Cumps
Jan Cumps
2 Mar 2018

I'm reviewing a single component DC converter for the TI SWIFTTm Power Module EVM RoadTest.

This article is a review of the switching device and the test setup.

 

Feel free to comment with the tests you'd like to see done with the module.

image

 

 

The Switching Device TPSM84A21

 

The TPSM84A21TPSM84A21 is a hybrid DC to DC Buck converter. All electronics to make it switch are in the package. It doesn't require external inductors or capacitors to work.

In the simplest setup, no other component is needed. The unit will then switch 8 - 14 V DC to 0.508 V. Maximum current of the output is 10 A.

image

 

When you want to set the output to another value between 0.508 V to 1.35 V,  the only external component is a voltage selector resistor (RSET).

This component is not involved in power conversion and can be a low power small one.

image

For ripple reduction, the module has input and output capacitors on board.

If your application is OK with the ripple figures of the device (documented in the datasheet), you don't need external capacitors.

If you need better filtering, you can add input and output capacitors. Guidelines are in that datasheet.

image

 

The device has additional functionality such as Power Good, under-voltage lockout and a possibility to externally synchronise the 4 MHz switching frequency.

Check this functional block diagram for the possibilities.

image

 

The Evaluation Module

 

As expected with hybrid componenst, there's not much more on the evaluation board than the  TPSM84A21TPSM84A21.

The only passives are a set of resistors to select different outputs, and to test the device enable, current limit, sync and power good.

 

image

The board gives you good access to all the interesting measure points. It also has footprints for additional capacitors if you want to test such a setup.

For the input and output rails, there are test points very close to the device. They are intended to be probed with an oscilloscope probe with ground spring.

This doesn't work that well with the probes of the Tektronix and Rigol scopes I have.

Their pins are thinker and the distance between center pin and ground spring wider than what the measure point on the PCB takes.

All other test points are solder-on loops that allow easy access with meter test leads or oscilloscope probes.

 

image

There's an empty footprint for a coax connector to sync the switcher's clock externally.

 

Test Setup

 

The EVM is connected to an electronic load that draw a current of up to 7.5 A. It can log the current and voltage measured.

The load is connected to the EVM with short thick wires. With these low voltages and high currents, resistance of the wire matters.

I'm using a linear power supply that can deliver more than enough power to feed the EVM at maximum load.

image

For measuring, I have a few DMMs and a 4 channel oscilloscope.

 

The PSU, load and oscilloscope are programmable. I can measure and log info in scenarios where the input voltage and output loads change over time.

Things I can automatically log:

  • Current at EVM input and output
  • Voltage at the EVM output
  • Any 4 points that I probe with the scope.

 

Let me know in the comments below if you're interested in particular load operating conditions o the EVM.

I will try the ones that I can perform with the above setup without damaging one of the components.

 

Edit: requests received:

  • image. efficiency compare to spec and Frank's review
  • image.  noise specification
  • automate efficiency measurement for input and load ranges
  • transient check

 

 

Related blog
TI SWIFTTm Power Module EVM RoadTest: Module Review and Test Setup
TI SWIFTTm Power Module EVM RoadTest: Noise Measurements
TI SWIFTTm Power Module EVM RoadTest: Efficiency
  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 8 years ago +4
    Hi Jan, It is nice to see your electronic load in action. I will be interested to see how well my efficiency measurements match yours. I am also interested in seeing how the TI transient response curves…
  • Jan Cumps
    Jan Cumps over 8 years ago +4
    Temperature after running 4 hours at 0.6 V 7.5 A, with a 14 V input: 42.5° C
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to fmilburn +4
    He Frank, I'll do the efficiency measurements and compare. I'd be surprised if they'd differ significantly. For the transients, I don't know (yet) if I'm well equipped. jc2048 hes profiled the transient…
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps

    Trouble with that is they've taken the drain straight down to the plane with that double row of vias just above the MOSFET package. You'd need to separate the MOSFET from the vias by cutting across the plane. You could do that with a craft knife and then solder a wire just above TP9 for the connection. Quite easy to do but messes up the board a bit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to genebren

    genebren  wrote:

     

    Nice road test report.  I look forward to seeing more of your data as you move forward.  Have you characterized the noise levels on the output?  It would be interesting to see what the output looks like.  Nice to see your load in action.

    Gene

    I've put measurements for the noise in this blog: TI SWIFTTm Power Module EVM RoadTest: Noise Measurements

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    jc2048  wrote:

     

    If it helps, I experimented with one of Jan's cast-offs at the end of 2016. That board had a test circuit on it (so you can see how TI thought to do it) and my blog also included me doing something similar with a separate MOSFET as a comparison.

     

    TPS54A20EVM evaluation - part 3

    I still have the board that I repaired, with the transient test circuit.

    image

     

    I'll check if it's feasible to wire it in to the load side of the SWIFT board ...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to fmilburn

    If it helps, I experimented with one of Jan's cast-offs at the end of 2016. That board had a test circuit on it (so you can see how TI thought to do it) and my blog also included me doing something similar with a separate MOSFET as a comparison.

     

    https://www.element14.com/community/people/jc2048/blog/2016/12/27/tps54a20evm-evaluation-part-3

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps

    Since you can control both the PSU and the load, you should be able to get very nice curves for the efficiency for a range of different input voltages. It's one area where the automation really pays off. I'd be interested to see you do it, even if your results were the same as everyone else, just to see how you set it up and how involved it was.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>