RoadTest: Taiyo Yuden Bluetooth® LE EVK
Author: navadeepganeshu
Creation date:
Evaluation Type: Development Boards & Tools
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: Espressif - ESP32 SoC, Microchip Technology - RN4870 Bluetooth 5.0 Module, ST Microelectronics - BLUE-NRG BLE SoC, Texas Instruments - SimpleLink CC2640 BLE MCU.
What were the biggest problems encountered?: Supportability. Taiyo Yuden Bluetooth® LE EVK is recommended to use with Nordic nRF52 SDK which isn't completely compatible. It needs some modifications to be done in memory mapping and allocation. This would have been nice if there was a separate chip specific SDK for Taiyo Yuden chipsets to make the development process easy and handy.
Detailed Review:
Looking into the RoadTest posting, this product looked excellent and thought would have some very good applications. Indeed it was excellent after fully reviewing this Kit.
Here, I am going to leave a glimpse on my experience with this starting from breaking the box seal to running a complex UART application with Taiyo Yuden BLE KIT.
Review Flow [ ] First look >> Gallery >> Getting started >> Hardware Tools >> Software Tools >> Testing >> Projects >> Summary/Feedback >> Links/References.
Taiyo Yuden BLE KIT EYSNSNZWW has the following features :
Being tiny, this module is open to vast applications in fitness/health trackers, wearables, telemedicine, home automation, Proximity, HID areas. By integrating with Nordic Tools, one can make any application up and running in a few hours. Also, ample amount of use cases and examples are readily available through nRF52 SDK.
Taiyo Yuden BLE KIT reached me with good look and packaging. This is very much appreciated because some products lack this. The kit included a sheet having unique code for registration of the product in Taiyo Yuden website to get the encrypted "Getting started guide". Hopefully, this could have been made opensource for anyone to get started and learn. All supported peripherals, tools were provided within to get going with the basic first design for anyone. To note, only one USB Type-B cable was available inbox though it needed two of them(one fo debugger and other for BLE Module). Anyways, it was manageable by soldering GPIO pins onboard to power up. Overall, it's good enough.
The price of KIT seems little higher comparatively. Although, a major part of the price goes to Segger Debugger and BLE module poses to be cheaper.
| {gallery}Taiyo Yuden BLE KIT |
|---|
Firmware expresses itself through hardware and without it, the system is void. For using the Taiyo Yuden BLE module, the following tools were used.
Module's operation stack is as shown above. There is a processor core in the base which is just like MCU can be barely operated by C programming. To operate Bluetooth Low Energy, a separate stack is placed above so called SoftDevice (SD) which performs authentication, crypto, connectivity and some backend operations for Bluetooth protocol. Over this, user interface applications lie through which one can directly interact with the core. The composition, structure and planning of operation stacks look excellent and works seamlessly.
The getting started process is quite simple and good documentations are provided by Taiyo Yuden. Initially, I tried running a blinky application only by accessing the MCU core(explained with a separate blog in detail). Here, I am going to show about serial communication test with BLE from the smartphone using the Nordic toolbox app.
In Segger Studio go to "File" >> "Open" to open sample project from nRF52 SDK at "<location>" >> "examples" >> "ble_app_uart" >> "PCA10040e" >> "s112" >> "ses" >> "ble_app_uart". Sample projects are made for Nordic development boards which supports Taiyo Yuden BLE kit too with some modifications since they have same nRF5281x core. Following are the images shown for this process and inside 'red box', sucessfully modified sections are shown.
| {gallery} Taiyo Yuden BLE Config |
|---|
![]() |
The above settings being done and built, BLE module spits out the network to which one can connect via the nRF toolbox moile app. This is a very good feature establishing security and reliability, unlike generic HC-05 Bluetooth module starts beaming signals once powered. One connected, seamless serial communication can be achieved with high transfer speed and bandwidth.
After this, terminal activates and messages can be sent through seamlessly. Any terminal softwrae like PuTTY, TeraTerm etc can be used. It also supports emojis ; ]]
The PCB design and quality are very good. Board mount antennae is beautifully carved(check right side of the image) and has good BLE range. The real BLE chipset is very tiny and seems promising!
To unleash the full potential and test in all perspectives, I have written a series of blogs with a variety of projects ranging from basics to using UART feature and making miniature control. Feel free to go through the following :
Projects |
|---|
First and basic test by running a blinky application. |
Gearing up by implementing a simple GPIO toggling application. |
Implemented custom sequence for controlling multiple GPIOs with UART interface. |
To summarize, it's great and poses vast applications for real world problems and increasing comforts.
The major issue which I had was with software suportability[SDK] as stated above. It was quite easy for me to overcome since the documentation was provided to some extent. But, for developing a solution for scratch or building a product, its gonna be quite hard to figure out everything with this device. Currently, Taiyo Yude BLE devices use Nordic Semiconductor nRF52 SDK as the standard one for development where a lot of modifications needs to be done in terms of memory mapping, GPIO configuration, Memory allocation etc. Hopefully, independent SDK giving full support to these devices comes out.
Rather, everything was easy to follow and develop with Taiyo Yuden BLE module and I highly recommended interested people to check this out.
All in all, my experience was excellent with Taiyo Yuden BLE KIT and would likely recommend this to people and also looking forward to use it in coming designs.
Links and References |
|---|
Product Page https://www.yuden.co.jp/or/product/category/module/lineup/eysnsnzww/ |
nRF52811 Product Page https://www.nordicsemi.com/Products/Low-power-short-range-wireless/nRF52811 |
Taiyo Yuden GitHub Page |
nRF52 SDK Download Page https://www.nordicsemi.com/Software-and-tools/Software/nRF5-SDK/Download#infotabs |
Segger Studio Download Page |
Getting Started Guide for nRF SDK https://www.nordicsemi.com/Software-and-tools/Software/nRF5-SDK/GetStarted |
Thanks to E14, Taiyo Yuden and all supporters for giving this opportunity to RoadTest.
Open for Comments / Improvements / Discussions / Interesting development ideas etc
Cheers!!!
Happy making.