Ok, it claims to be a 0.22Ω 3watt power sand resistor, with 3 legs. (so starting at the top and going clockwise, 1 at the top, 2 on the right, and 3 on the left)
My fluke 113 says no it's 0.38 Ω between 1 and 2, as well as between 1 and 3, and 0.59…
Link to files used in this tutorial: http://dl.dropbox.com/u/30557697/RaspberryPiTutorials/PiShooterV2.zip Instructions for unzipping files are at the start of Tutorial 6. The Raspberry Pi is a
My attempts to video tape myself soldering. Im sorry that the video isn't the best but I am still learning. I have to remind myself that I need to keep my hands under the camera all the time. I hope that others will learn from my mistakes.
Hello All, I am using Eagle 5.7, and I am trying to create a logo to be used in silk-screen or copper layer. What I have done so far is to use import-bmp.ulp to import a bitmapped version of the logo. I then want to trace it using polygons, in order to…
I have a classic gameboy which I am trying to restore and I cant find the solution elsewhere online. When I insert a game it displays a scrambled Nintendo logo. At first I thought it may be a bad cart reader so i took a working game and soldered it directly…
Microsoft has a brand-new logo to go with all the brand-spankin' new products it's got coming this fall. The new design uses the long-standing Windows logo as its starting point, but gone are the wavy edges of that older look. The graphic element of the…
Ubuntu has been in the news quite a lot recently what with the release of 12.04 “Precise Pangolin” last month, Dell deciding to ship the first Ultrabook with Canonical’s OS, and Mark Shuttleworth’s bid today to get Ubuntu on 5% of PCs by the end of next…
Hello everybody I want to know how to create Logo for a factory that I work for. As you can see on the attach, I want to convert this image to buttom or top layer to put on my boards. Is there any way to do it easily? or.. Do I have to do it drawing piece…
Hi Folks, ich benötige für ein Projekt eine lib mit Siemens Logo CPU und DM16. (s. Anhang). Das DM16 hat 8 Relaisausgänge. Der Kontaktspiegel mit 8 Ausgängen untereinander ist aber sehr unübersichtlich und braucht viel Platz. Leider habe ich es nicht…
I have demonstrated the bug in this video, please watch it in 1280x720 and full screen http://www.youtube.com/watch?v=odne9gdBqfY
This video is unavailable.
You don't have permission to edit metadata of this video.
I would like to know how to remove or hide the Raspberry logo showing during the startup with the option "Hold Shift to Recovery Mode". I know there are other discussions about removing RPi logos, but they are referred to the four raspberry logos that…