Intro This episode chronicles getting the Lora & Husky show live-connecting with the Crystal display. The Lora and husky hardware and software are fully functional, including a 3D printed chassis. This node views the scene with the Husky camera and display…
Arduino MKR WAN 1300 LCD For full blog see: https://www.element14.com/community/community/arduino/arduino-projects/blog/2018/11/18/loragelomkr-long-range-geo-locator-mkr
MKR WAN 1300 Unboxing for the full blog see: https://www.element14.com/community/community/arduino/arduino-projects/blog/2018/11/18/loragelomkr-long-range-geo-locator-mkr
arduino MKR WAN 1300 GPS for full blog see: https://www.element14.com/community/community/arduino/arduino-projects/blog/2018/11/18/loragelomkr-long-range-geo-locator-mkr
MKR WAN 1300 LoRa GPS system For full blog see: https://www.element14.com/community/community/arduino/arduino-projects/blog/2018/11/18/loragelomkr-long-range-geo-locator-mkr
RF (Radio Frequency) Enter Your Project for a chance to win a Spectrum Analyzer for the Most Innovative RF Project! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll In the Comments Below: Let Us Know Your Innovative Project…
Or, also known as: How I pretty much bricked, and then fixed a product I was roadtesting. The following story is something I encountered during my Roadtest of the MKR WAN 1300. (See roadtests.) I've mentioned the programming error I encountered in passing…
Another Project14 Challenge complete - sort of..... As always, some goals were met and some were not. I thought that I would summarize where I got to. Blog Post Index LoRa Experimental Environmental Sensors (LoRaXes) - Introduction LoRa Experimental Environmental…
I made all the changes needed to the case assembly and I trimmed down the proto PCB and wired the connections to the sensors.
Here is a picture of the completed assembly:
Not pretty, but looks like a prototype..... At the lower right, next to…
Well, I am running out of time to complete this project. All the usual excuses, out of town guests and other distractions. I am going to do well just to finalize all the construction by next week. I did a test print of the component mounting bracket …
I decided to do some initial RSSI testing at various locations inside my house and outside in the backyard to see how much loss I was getting due to the structure of my house. This is to get a baseline for further outdoor testing. There are two components…
The temperature sensor that I selected is the BME280. It measures humidity and barometric pressure in addition to temperature. The particular version that I'm using interfaces over I2C. There are other versions that will interface with I2C or SPI at the…
Now that I've gotten some runtime on my new 3D printer and used the new workflow with Cura - I'm ready to start printing the component mounting for the sensor case. Since I've decided to use the larger case, I can mount some of the components vertically…
I recently connected my Things Gateway to the Things Network and this Project14 challenge seemed like a good opportunity to do some experiments with the two MKR WAN 1300 boards that I received with the gateway.
I'd like to build a pair of portable…