Browse By Tags

  • Real time playback of digital audio signal from Cirrus Audio Card SPDIF input through Raspberry Pi USB DAC

    Dear Sirs, Is real time play back of digital audio signal recieved through the SPDIF input of the Cirrus Audio Card through an USB DAC connected to the Raspberry Pi possible? If yes, than what kind of OS version, drivers, software, patches or settings…
  • Cirrus Logic card as SPDIF DAC

    Hello, Can the Cirrus Logic audio card take an SPDIF input from an external source and play it on the analogue outputs? If so, is there likely to be much latency? Does the audio data have to pass through the Raspberry Pi or can this be handled by the…
  • Accessing SPDIF input pins

    Hi, we have two RIoT boards in our test setups now, along with other imx6 boards, and they are working great! We are able to use SPI, I2C, UART and other connections. On other boards we now also acitivated the SPDIF input of the imx. Sadly, there is no…
  • Wolfson: can't record with the SPDIF IN / impossible d'enregistrer avec la prise SPDIF IN

    FRANÇAIS: Bonjour, J'ai acheté et installé une carte son Wolfson sur mon Raspberry Pi B, puis installé le Master contenant les drivers et logiciels et fichiers de démonstrations sur ma carte SD. -La lecture de fichiers FLAC fonctionne très bien (avec…
  • Wolfson Audio Card - no SPDIF out.

    I'm on my 2nd Wolfson card as I sent the first back thinking it was broken. I just cannot get any output from SPDIF, not even with the example HD flacs. Lineout works fine. I'm using mplayer -ao alsa to play flacs. There are no errors in output. Same…
  • Streaming from cirrus logic audio card in Mono? and in Digital?

    Hi, I working on a raspberry-pi streaming project. So far I can stream from darkice from the analog input. I read and old post that says it is impossible to attribute the value [1] for the audio channels parameters in darkice.conf because the card cannot…
  • Cirrus Audio Multi-Ch Capture

    Hi, Is the Cirrus Audio Card (WM5102) able to capture (and pass along the AIF1 interface) multiple channel of audio? I am trying to capture simultaneously audio from the SPDIF input (2 channels) and from the Line In (2 channels). I cannot have the audio…
  • Cirrus Audio Board on RPI 2

    Hi All, Since there is till now no Kernel 3.18 with driver for the Cirrus Audio Board available did somebody managed to geth the SPDIF output working? Since the SPDIF interface is based on the Wolfson WM8804 is already comes with an build in module for…
  • Spdif Freq Input ?

    Hi every one, I'm in dev of an spdif recorder with the wolfson audio card ans raspberry pi to use it with an Neumann DMI-2 interface https://www.neumann.com/?lang=en&id=current_accessories&cid=db_current_accessories&dbid=193 All works perctely, but I…
  • Any galvanic isolation of the electrical SPDIF out?

    An impressive little board with great flexibility at this price point. Does anyone know if it has galvanic isolation of the electrical SPDIF out?