Artificial Intelligence and Machine Learning
  • Technologies
  • More
Artificial Intelligence and Machine Learning
Blog Developers Created a Compression Algorithm in the 1970s By Adding a Spell Checker to a Unix System Still Used Today
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Artificial Intelligence and Machine Learning to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 6 May 2025 7:33 PM Date Created
  • Views 2616 views
  • Likes 3 likes
  • Comments 2 comments
  • pdp
  • cabeatwell
  • spellcheck
  • ai
  • unix
  • innovation
Related
Recommended

Developers Created a Compression Algorithm in the 1970s By Adding a Spell Checker to a Unix System Still Used Today

Catwell
Catwell
6 May 2025

image

A PDP-11 machine. )Image Credit: Wikipedia)

Everyone’s familiar with spellchecking, a handy feature in browsers, text editors, and other software. The tool proved extremely challenging to install as systems lacked sufficient memory to support it at the time. But, a lossless compression algorithm, which is still used today, allowed it to be integrated into a system.

In 1975, AT&T programmers explored ways to use Unix for text processing. However, this required a working spellchecking tool. The easiest way to do this involves putting the dictionary into system memory, and the computer would then look each word up. It’s a tedious task that takes time, and during those years, computers had insufficient memory to handle it.

But, through compression, we can easily load a 250 kB file into 64 kB of RAM. However, this is more challenging than we think. To do this, you would need to use a PC with a superfast multicore processor and lots of RAM. You can create a 256 kB text file with 260,000 characters, compressing it via a compressor and the Lempel-Ziv-Markov chain algorithm to shrink the size to 257 bytes.

AT&T used PDP-11 systems (16-bit microcomputers), which are weaker as they feature less memory (64 kB to a few hundred kB) and processing power. Due to hardware constraints, it would be challenging for the PDP-11 systems to search through a 256 kB text file as the system may struggle to handle that task. It can handle a compressed 257-byte file.

Computer scientist Steve Johnson developed the first Unix-based, disk-backed spellchecking prototype. While functional, the system was slow and made mistakes. Douglas McIlroy developed an algorithm that decreased the amount of memory required to store dictionary words and introduced a data structure, allowing the entire dictionary to load into a few kB of memory. This algorithm only needed 14 bits per word, which meant a 30,000-word dictionary could fit in fewer than 52 kB of memory. Theoretically, the system only required at least 13.57 bits per word.    

A big part of the solution was Golomb coding, a lossless compression still used today in Rice coding, which is used in formats like FLAC, Apple Lossless, and Lossless JPEG.

Have a story tip? Message me at: http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • DAB
    DAB over 1 year ago

    The first computer I ever used was a PDP-11.

    I did a lot of cool programs in assembly language.

    Compared to what I have now, it was very slow with each instruction taking microseconds.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 1 year ago

    The first computer I ever used was a PDP-11.

    I did a lot of cool programs in assembly language.

    Compared to what I have now, it was very slow with each instruction taking microseconds.