Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog 14 bit ADC oversample example for the EasyL1105 MSPM0 board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 24 Sep 2025 3:43 PM Date Created
  • Views 1168 views
  • Likes 5 likes
  • Comments 7 comments
  • MSPM0L1105
  • MSPM0
  • easyL1105
  • mspm0_dma
Related
Recommended

14 bit ADC oversample example for the EasyL1105 MSPM0 board

Jan Cumps
Jan Cumps
24 Sep 2025
14 bit ADC oversample example for the EasyL1105 MSPM0 board

TI's SDK for the MSPM0 family has a set of examples. They are all targeting one of their LaunchPad dev kits. In this post, I'm porting another one to the EasyL1105.

The example, adc14_14bit_resolution, uses hardware to oversample the 12 bit onboard ADC. And DMA to retrieve 1024 samples. It goes in low power mode while sampling is happening. It's originally written for the LP-MSPM0L1117 LaunchPad. I'm porting it (just like I did in Port an SDK example to the EasyL1105 MSPM0 board).

What does it do?

The design uses the 12 bit ADC peripheral options to oversample to 14 bits:

image

From the readme:

ADC12 Hardware averaging is configured to accumulate 16 samples and shift right by 4 to achieve 14-bit effective resolution.

Use DMA to get 1024 samples - in low power mode. The selected input is ADC channel 2. On the EasyL1105, this is J2.9.

image

image

While ADC and DMA are doing their work in the background, we allow the controller to poll for completeness in a power saving mode:

        DL_ADC12_startConversion(ADC12_0_INST);

        while (false == gCheckADC) {
            __WFE();
        }

The WFE arm assembler instruction 

A usage for WFE is to put it into a spinlock loop. ... To save power, you can insert the WFE instruction into the loop so the CPUs instead of looping continuously will enter STANDBYWFE.

image

The gCheckADC flag gets set in the ADC interrupt handler, when DMA has finished loading 1024 samples:

void ADC12_0_INST_IRQHandler(void)
{
    switch (DL_ADC12_getPendingInterrupt(ADC12_0_INST)) {
        case DL_ADC12_IIDX_DMA_DONE:
            gCheckADC = true;
            break;
        default:
            break;
    }
}

image

The ccs project with source and config files is attached. Thank you for reading.

ccs project adapted to EasyL1105: 3704.adc12_14bit_resolution_EasyL1105_20250923.zip

Related posts

DMA specific

  • Sign in to reply
Parents
  • DAB
    DAB over 1 year ago

    OK Jan, you lost me.

    Taking sixteen 12 Bit samples and dividing them by four does not give you 14 Bit accuracy.

    That approach will reduce noise by 75 percent, but the basic measurement is still only good to 12 bits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 1 year ago

    OK Jan, you lost me.

    Taking sixteen 12 Bit samples and dividing them by four does not give you 14 Bit accuracy.

    That approach will reduce noise by 75 percent, but the basic measurement is still only good to 12 bits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to DAB

    I miswrote, it's shift right 4 bits