Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Using TVS Diode P6KE across relay coil but then also relay coil is getting damaged.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 340 subscribers
  • Views 4613 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Using TVS Diode P6KE across relay coil but then also relay coil is getting damaged.

e14 Contributor
e14 Contributor over 10 years ago

We are using TVS diode across 24V DC-100AMPs relay for automotive application but my relay coil is getting damaged.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor +1
    Unfortunately the schematic shows a relay and not what is connected on the load side, or how the 24v DC is sourced (ie switchmode supply, battery, etc). What is on the end of the 100A contacts.? ie a simple…
  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor +1
    That image helps.... There is no heating apparent from the contact as it seems to be a nice copper colour. The coil wire appears to have fused. For any inductive circuit the In-rush/ON current is very…
  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor +1
    We are trying to help.... If you can't provide a circuit then I'm afraid my anwers are limited to guessing ... Mark
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to artful_bodger

    Its not local, its costly.Its from reputed manufacturer.

    My thinking is that due to Contact it is getting damaged.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    If the coil is being energised by the alternator without any dc rectification then yep it'll generate a lot more heat and fail more rapidly

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor

    We are trying to help....

    If you can't provide a circuit then I'm afraid my anwers are limited to guessing ...

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to mcb1

    Coil is energized through Battery 24V.

     

    Circuit connection given above.

    Just directly connect one starter switch at one point .

    The starter switch is connected to batter +ve.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Is the load powered directly from the same +ve too? Is there anything on the load inductor wise that could cause a huge back surge when it's switched off, something like that could force through the coil to the ground connection damaging it as it goes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Actually Here load is motor ,battery is connected to This relay and engine.Relay contacts are used to connect alternator output to motors. through wires

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Currently i had gone with 40V diode ,it is not able to prevent the damage

    cn i reduce the volatge to 30V

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • artful_bodger
    artful_bodger over 10 years ago

    I'm with lucie tozer.  I think you've got a heating problem caused by peaks in the alternator output.

    You say the relay operates 3 hours with no load, but was that on a lab supply, or on the alternator?

    Stick a scope on there and have a look at the coil volts.  I can't think of a way the load could directly damage the coil.

    Once you know what the waveform looks like, you can send it to the manufacturer for help.

    A charged battery will be around 28V (you have a battery in circuit?), or a bit more, so a 30V diode may be a bit tight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor

    Hi Amol,

    My experience with situations like this indicate that the coil is getting too much current during energization. mcb1 is right in his assesment. Each time this over current occurs the wire that you show in the photo "heats up" as it is exposed in the air and the weakest link. The repeated heating of the wire causes it to change its temper and resistance and become more and more susceptible to failure. I would put a low resistance, perhaps 5 ohms, in series with the the circuit that feeds the coil. If the coil won't pull in with 5 ohms try 3 ohms. This will limit the energizing current and should prevent the failure you are seeing.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor

    Hi Amol,

    I thought of one other possibility for the cause of this problem. If for some reason the solenoid relay coil is not properly secured to the armature it will move during the actuation. This can cause a mechanical stress or a bending of the leads. Just like bending a wire back and forth will break it, repeated actuation with a loose coil will also break the leads.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>