Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Why is the Schottky diode being used in control circuit?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 1 answer
  • Subscribers 336 subscribers
  • Views 2028 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Why is the Schottky diode being used in control circuit?

Humaninsane
Humaninsane 5 months ago

imageWhy is the Schottky diode being used in control circuit? and why is the 470nF cap is added at that voltage divider output? how is the Cap value 470nF calculated?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett 5 months ago in reply to Humaninsane +3 suggested
    I think I can see what the ciruit is attempting: T103 switches T104 on and T104 connects R108 to the supply rail. R108 and R119 attenuate the signal by a factor of (180 + 10.2)/10.2. C111 makes a…
  • geralds
    geralds 5 months ago in reply to michaelkellett +2
    Hi simulation with Schottky diode: simulation without Schottky diode: The Schottky diode is important during switching off the transistors. Without Schottky it can produce very high…
  • geralds
    geralds 5 months ago in reply to Humaninsane +1
    Hi, I would say that the T103 is a simple switching transistor in a higher voltage-rated circuit. A BC846 would be too small at 60V. The microcontroller's output switches it on to measure the voltage…
Parents
  • michaelkellett
    0 michaelkellett 5 months ago

    I would need to know more about the function of the circuit to make an informed comment.

    The two transistors are high voltage parts (250V and 500V).

    What are the inductor connections and what is the working voltage on emitter of T104 ?

    D108 is only rated for 40V reverse voltage.

    I suspect that the diode is to protect T103 from negative voltages at TP131 - but without more information its only a guess. 

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dang74
    0 dang74 5 months ago in reply to michaelkellett
    michaelkellett said:
    D108 is only rated for 40V reverse voltage.

    Good catch.  Hopefully the input voltage is less than that... mind you when the NPN transistor is off the diode cathode is isolated from GND.

    [Edit] next to R118 there is a bit of text that says 36V... so I guess we are safe.

    In terms of operation....

    The only condition in which current runs through the Schottky is during the positive AC cycle and when the NPN is on.  Otherwise the voltage at the base of the PNP is the same as the emitter so the PNP remains off.

    When the NPN is turned on, the positive half of the cycle is allowed to pass through the PNP.  The voltage divided at its output would indeed be around 1.93V assuming 36V peak voltage.  The capacitor is of course used to smooth out the signal to essentially DC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ArminAIM
    0 ArminAIM 5 months ago in reply to dang74

    It seems that the 470nF is part of some sort of peak detector. I recently built one. They consist of a diode to rectify, resistor to ensure slow discharge and capacitor to store the charge so that the resulting measured voltage is all balanced and rectified. But I am not sure maybe I’m way off here so correct me if I’m wrong!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ArminAIM
    0 ArminAIM 5 months ago in reply to dang74

    It seems that the 470nF is part of some sort of peak detector. I recently built one. They consist of a diode to rectify, resistor to ensure slow discharge and capacitor to store the charge so that the resulting measured voltage is all balanced and rectified. But I am not sure maybe I’m way off here so correct me if I’m wrong!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dang74
    0 dang74 5 months ago in reply to ArminAIM

    You have it right.  I just used different words when I said smooth out the signal to DC.