FPGA
  • Technologies
  • More
FPGA
Blog Arty: talk to SPI EEPROM - part 2a: EEPROM State Machine and Initialise
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 25 Jun 2022 8:04 PM Date Created
  • Views 2026 views
  • Likes 7 likes
  • Comments 4 comments
  • summer of fpga
  • Spartan_Migration
Related
Recommended

Arty: talk to SPI EEPROM - part 2a: EEPROM State Machine and Initialise

Jan Cumps
Jan Cumps
25 Jun 2022

The 25LC256 SPI EEPROM needs some management, if you plan to write data to it. It's described in this app note. At startup, it's read-only. You need to enable write functionality and remove write protect. Once that's done, you can use the write functionality.
This is the sequence:
image
I need to send the 8 bit write-enable, then the 16 bit no-protection. Both should be wrapped inside a ~CS envelope.

I'm implementing the EEPROM VHDL as a state machine. Init at startup, then read, then wait for data and write. Once data is received and written, back to read. Because I'm managing the ~CS myself via bitbanging*, I'd like to keep each SPI sentence (a section wrapped inside a ~CS) as a state. So I split the init state in two:

  • initialise Write Enable
  • initialise No Protection

* The SPI module I selected doesn't support CS hold. It will hold CS low until the requested data size is sent. But that's a fixed size. The EEPROM has requirements to hold the CS until a activity is completed. In my case, that can be 1 byte for the WREN instruction, 2 bytes to write to a register, or 4 bytes to read/write data: instruction, 2 byte address, data. To get support for CS hold,  I can:

  • customise the current SPI IP I'm using - add an input parameter telling for how many bytes to hold the CS low,
  • look for an other IP, or
  • ignore that IP's CS, and bitbang the CS line low and then high in my own EEPROM VHDL module. It knows the EEPROM requirements.

I chose the 3rd option.

My state machine will look like this:

  1. init WREN, then next
  2. init NOPROT, then next
  3. READ data from address, then next
  4. wait for data and WRITE to address, then 3

Here's the design. I tried to implement 1 and 2. The others just contain comments of what I think they 'll need to do:

architecture Behavioral of eeprom is
  TYPE FSM IS(init_wren, init_noprot, accept, read); --state machine
  SIGNAL state : FSM;                             
  SIGNAL step : integer range 0 to 5;
  
begin

  PROCESS(clk, reset_n)
  BEGIN
    IF(reset_n = '0') THEN --reset everything
      state <= init_wren;     
      step <= 0;
      bitbang_cs_n <= '1';
      start <= '0';
    ELSIF(rising_edge(clk)) THEN
      case state is
                  
        when init_wren => -- init eeprom, enable writing
          if (step = 0) then -- send WREN cmd
            bitbang_cs_n <= '0';
            step <= 1; -- next step
            data_out <= "00000110"; -- WREN (0x06)
            start <= '1';
          elsif (step = 1) then -- wait for ack from spi
            if (busy = '1') then  -- wait for spi buzy
              step <= 2;
            end if;
          elsif (step = 2) then -- finalise WREN
            if not (busy = '1') then  -- wait until spi no longer buzy
              -- finished					 
              start <= '0';
              state <= init_noprot;        
              step <= 0; 
              bitbang_cs_n <= '1';
            end if;
          end if;

        when init_noprot => -- init eeprom, no write protect
          if (step = 0) then -- write status register (0x01)
            bitbang_cs_n <= '0';
            step <= 1; -- next step
            data_out <= "00000001"; -- WRSR (0x01)
            start <= '1';
          elsif (step = 1) then -- wait for ack from spi
            if (busy = '1') then  -- wait for spi buzy
              step <= 2;
            end if;
          elsif (step = 2) then -- finalise WRSR
            if not (busy = '1') then  -- wait until spi no longer buzy
              -- finished					 
              start <= '0';
              step <= 3; 
            end if;
          elsif (step = 3) then -- finalise WRSR
              step <= 4; -- next step
              data_out <= "00000000"; -- NOPROT (0x00)
              start <= '1';
          elsif (step = 4) then -- wait for ack from spi
            if (busy = '1') then  -- wait for spi buzy
              step <= 5;
            end if;
          elsif (step = 5) then -- finalise NOPROT
            if not (busy = '1') then  -- wait until spi no longer buzy
              -- finished					 
              start <= '0';
              state <= read;        
              step <= 0; 
              bitbang_cs_n <= '1';
            end if;
          end if;

        when read =>
          -- todo read from address
          -- todo READ cmd
          -- todo send address
          -- todo receive data
          
          -- finished					 
          state <= accept;        
          step <= 0;         

        WHEN accept =>
 		  IF not (data_in (3 downto 0) = "0000") THEN
			-- todo write to address
          -- todo WRITE cmd
          -- todo send address
          -- todo send data
			
			-- finished
			state <= read;
            step <= 0;         
          END IF;
          
      END CASE;
    END IF;
  END PROCESS; 

end Behavioral;

I think I'll have an issue with my CS bitbanging, as currently implemented. The state machine runs on a fast clock. The time between setting CS high and back low, between states, may be too short for the 25LC256. I know how to deal with that, but want to see if it's a real issue first.

edit: this works. See the comments below for the steps from fail to success...

image

checkpoints:

  • CS low
  • send 0x06
  • CS high
  • min 350 ns before next step: 9 µs (I check this specifically, because I'm bitbanging this signal. All others controlled bt the SPI IP).
  • CS low
  • send 0x01
  • send 0x00
  • CS high
  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    Success: same sequence as in the application note: "0x06" - "0x01 0x00" with the two last bytes clubbed together in a CS envelope

    image

    The CS bump is 9 µs. That's within the specs:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago

    Progress: Some data. 

    image

    I kept the START signal active longer (until the SPI lifted the BUSY signal).
    It's still not the correct conversation, but promising. This is what's expected:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    Including the busy signal. It seems to be Okay:
    image

    Now over to find out why:

    • data is not clocked out
    • state machine doesn't go to next state: init_noprot
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago

    Only a little bit of success:

    image

    ~CS works. Clock gets clocked, but I don't see the initial conversation happening. I'll need to restudy my code. Maybe bring the SPI IP's busy signal external for checking...