FPGA
  • Technologies
  • More
FPGA
Blog Discussion with Choices of Design for the Arty S7 - The Blinky Project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fyaocn
  • Date Created: 20 Jun 2022 5:30 AM Date Created
  • Views 1171 views
  • Likes 6 likes
  • Comments 0 comments
Related
Recommended

Discussion with Choices of Design for the Arty S7 - The Blinky Project

fyaocn
fyaocn
20 Jun 2022

Build a project with the Arty S7-The Blinky Project

1. How many ways to Build one start-up Project ?

With reference to previous comparation between Spartan-6 and Spartan-7, more design choice are available. This blog tries to enlighten as many as choice to complete the job.

5

2. About Arty-S7

Before start, a glance on this web page can Programmable Logic - Digilent Reference give clues on where  Spartan-7 is on Digilent Xilinx FPGA family tree, with  256 MB DDR3L, 16 MB QSPI Flash,  2,700 Kb BRAM resources. It is good start point for FPGA exploration as Arty S7 - Digilent Reference.

image

image

This reference page is important for Hardware definition.

image

3. Prepare the  software in Windows 10

 It is better to use Vitis selection after  Xilinx_Unified_2022.1_0420_0327_Win64 is started in Windows 10. Refer to Installing Vivado, Vitis, and Digilent Board Files - Digilent Reference

image

Install the board is easy now, just press refresh button and find the Arty-S7 board, the hardware definition files shall be installed automatically.

image

Then start the Vivado to build the first Project, to blink the leds.

4. Choices of Design and Build one FPGA Project 

4.1 Design Baremetal with basic Logic Gates in Block Design in VIvado

4.2 Design Baremetal with IP integrator in Vivado

image

image

4.3 Design Baremetal with Verilog , System Verilog or VHDL in Vivado

  • Set port in constrain file of .xdc

image

create the verilog file blink.v

image

with port set according to that of .xdc

image

edit the verilog file

image

Run synthesis

image

Run  implementation

image

Create bitstream

image

Open hardware manager to connect the Arty-S7 

image

image

Program the Device  with blink.bit file then run the blink project.

image

Refer to Getting Started with Vivado for Hardware-Only Designs - Digilent Reference for details.

4.4 Designing with C++ in MicroBlaze core, Vitis

4.5 Desiging with kinds of MicroCore like ARM-M1, RISC-V or MIPS

5. Please leave your idea on this discuss Choices of Design and Build one FPGA Project on Digilent Arty-S7 - Forum - FPGA - element14 Community To correct me if there is anything not right.

Reference:

1. Programmable Logic - Digilent Reference

2. Arty S7 Reference Manual - Digilent Reference

3. Installing Vivado, Vitis, and Digilent Board Files - Digilent Reference

4. Choices of Design and Build one FPGA Project on Digilent Arty-S7 - Forum - FPGA - element14 Community

5. Arm DesignStart FPGA Cortex-M1 Environmental Monitor - Digilent Projects (digilentinc.com)

6. Arm DesignStart FPGA Cortex-M3-Based Robot - Digilent Projects (digilentinc.com)

7. GitHub - OpenXiangShan/XiangShan: Open-source high-performance RISC-V processor