FPGA
  • Technologies
  • More
FPGA
Blog Cheap Entry into FPGA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelkellett
  • Date Created: 3 May 2015 4:17 PM Date Created
  • Views 2737 views
  • Likes 10 likes
  • Comments 9 comments
  • cyclone
  • fpga
  • altera
Related
Recommended

Cheap Entry into FPGA

michaelkellett
michaelkellett
3 May 2015

There's been quite  a lot of talk in the FPGA group about cheap ways to get started so a couple of weeks ago I decided to forsake the professional setup I use for real work and try one of the cheapest routes I could find. The idea was to try something as general purpose as possible and to keep clear of as much proprietary hardware and software as possible. That basically means using a simple board with the FPGA and very little else on it and using the FPGA manufacturer's free software.

 

All the FPGA manufacturers offer development boards and some of the simple ones from Lattice and Altera are quite cheap. Xilinx and MicroSemi don't get down to quite the same price level. There are third party boards at just about any level and the cheapest I can find with a real FPGA are based on Altera's Cyclone2 device.

There are several vendors for these on Aliexpress - this one is typical : ALTERA FPGA Cyslonell EP2C5T144 Minimum System Learning Board Development Board-in Other Electronic Components from Elec…

You'll pay about £10 with free shipping.

I bought mine in a bundle with a programmer from Etang Electronics on Amazon for £32.58 for the lot including shipping.

 

It looks like this:

 

image

 

And the good news is that it all works !

 

The Cyclone2 is a rather old design and although Altera still recommend it for new designs it isn't supported by the latest version of their design software. So when you download the software to develop code for it make sure to get version 13.0sp1. The part on the board is  a real FPGA with hardware multipliers, some embedded memory blocks and about 4000 logic elements. You get a voltage regulator, a 50MHz oscillator, a switch and three LEDs.

 

I've never used Altera's design software before so it took a little while to get round the quirks. There are one or two places where it seems to need to be told stuff it must already know (like where to find the simulator that was installed with it !) and it can generate test bench files but gives them an odd filename extension which you end up changing. There is a lot if support material on the web.

 

You get a free version of ModelSim for simulation and I found this to be the most difficult part - I expect mainly because I use a paid for version of a different simulator and have done for the last 10 years.

There is a free open source  VHDL simulator (GHDL) but it's reputation is not very good - so if you go this route you are stuck with ModelSim.

 

These boards are down at Arduino price levels so perfectly affordable for building in to projects.

 

If any one is interested I'll post some actual code that does something and if any one has an idea of a project they fancy using this board I'll be happy to discuss it.

 

MK

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 11 years ago +6
    Hi Michael, Thank you for using your expertise to look at the entry level hardware and software. I enjoyed reading your post. John
  • dougw
    dougw over 9 years ago in reply to jw0752 +4
    An interesting topic... I used to only rarely click Like or Helpful because I thought it would help promote better quality contributions if I only rewarded the highest quality input. I've changed though…
  • volly
    volly over 9 years ago in reply to jw0752 +4
    jw0752 Hi John, I do respect your point and opinion on this matter. Thank you if you mean well, and I am sure you do. While your statements and that of dougw might be true, admirable and even likeable…
Parents
  • volly
    volly over 9 years ago

    michaelkellett

     

    Thanks. I am so hooked!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to volly

    Hi Yunus,

     

    Just out of curiosity, how was my comment on this piece helpful? The reason I ask is that sometimes we get people who join and then just chase points. While this gets the person lots of points it at the same time causes the people they are trying to impress to think poorly of them. I have seen that you are truly interested and that you have made some good contributions. I also consider you a new friend so I did not want this to happen to you. The points do not matter in the long term only the respect of your fellow members. I look forward to your great contributions to this site.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 9 years ago in reply to jw0752

    An interesting topic... I used to only rarely click Like or Helpful because I thought it would help promote better quality contributions if I only rewarded the highest quality input. I've changed though, not to get more points but to encourage more participation. I now generally use the basic rule if someone made some effort to write it down and I found it interesting enough to actually read it, it gets a like (unless I really don't like it) - to encourage and reward this level of effort. It takes a little more work to click on Like all the time, but I think it does have a positive effect. I know members like Michael are not concerned with points, but I am not about to discriminate and exclude anyone.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to dougw

    Hi Doug,

    I agree to some extent and I do use a LIKE more often when I want to say thank you or acknowledge someones effort. For me however the HELPFUL means that some knowledge has actually been passed. If I have learned something new or a question that I have had has been answered then I feel that the helpful is warranted. Your post to me is a good example. I feel that it deserves a LIKE but nothing in it is something new about electronics for me so it will not get a HELPFUL. It is also obviously the case that not everyone else has to agree or use the same conventions. I mentioned it to Yunus as he has a lot of enthusiasm and this may be misread as points chasing by some of the guys.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jw0752

    Good discussion guys.

     

    Unfortunately LIKE has been inherited from Facebook (and maybe other social media).

    It does have the advantage of visibility about who likes it.

     

    On the other hand helpful is an unknown (except in the inbox).

     

    I'd prefer that both gave points only to the other person, and therefor the 'points collectors' have no benefit.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 9 years ago in reply to jw0752

    Good discussion guys.

     

    Unfortunately LIKE has been inherited from Facebook (and maybe other social media).

    It does have the advantage of visibility about who likes it.

     

    On the other hand helpful is an unknown (except in the inbox).

     

    I'd prefer that both gave points only to the other person, and therefor the 'points collectors' have no benefit.

     

     

    Mark