FPGA
  • Technologies
  • More
FPGA
Blog Comparison between Spartan-6 and Spartan-7 FPGAs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 1 Jun 2022 5:27 PM Date Created
  • Views 9920 views
  • Likes 8 likes
  • Comments 0 comments
  • Xilinx Vivado
  • xilinx ise
  • xilinx sdk
  • spartan-7
  • xilinx fpga
  • Spartan_Migration
  • xilinx vitis
  • spartan-6
Related
Recommended

Comparison between Spartan-6 and Spartan-7 FPGAs

ralphjy
ralphjy
1 Jun 2022

The Spartan-6 was introduced by Xilinx in 2009 and the follow on Spartan-7 in 2015. As semiconductor fabs move to newer process nodes older processes become less cost effective and production volumes decrease. Due to current shortages of Spartan-6 parts, Xilinx is encouraging migration of designs to the newer Series 7 FPGAs.

Xilinx has done a great job of documenting differences between the Spartan-6 and Spartan-7 FPGAs in order facilitate that migration. The two best references I've seen are the white paper and webinar, both done with Adam Taylor from Andiuvo Engineering.

Migrating S6 to 7 Series.pdf

Webinar Mastering the Migration Journey from Spartan-6 FPGAs

I'll try to highlight what I learned from those resources.

Hardware differences

A significant change is that the Series 7 FPGAs are built with the next generation process node moving down from 45nm to 28nm. This enables higher performance and higher circuit density and lower power. The Spartan-7 has 2X the relative performance per watt than the Spartan-6 as shown in the chart below. The chart also shows improved memory speed from DDR3-800 to DDR3-1066.

The Spartan-7 does have some tradeoffs in a smaller Max I/O count (400 vs 576) and the lack of transceiver cores (Gb SerDes and PCIe). If these features are required, then the design needs to be implemented using Artix-7 FPGAs.

image

There are also a number of significant architectural changes. These are listed in the following table.

image

Toolchain differences

There are also significant improvements in the development toolchain between Spartan-6 and Spartan-7.

The Spartan-6 uses Xilinx ISE for hardware development and Xilinx SDK for software development.  The Spartan-7 devices are using the newer Vivado tool for hardware and Vitis for software.  There is a huge improvement in design efficiency gained by using these new tools.  Vivado allows working with pure RTL designs, but it also leverages a large IP library managed using the Vivado IP integrator.  On the software side, Vitis is a unified software platform that provides a high level framework with open-source libraries that have been optimized for Xilinx FPGAs. 

Summary

Spartan-6 devices are nearing end-of-life (EOL) and should not be considered for new designs, but the newer generation Spartan-7 device capabilities and toolchain should allow the design migration from legacy parts.  The specific IP and IO requirement utilized in the Spartan-6 design could require using a different 7 Series part other than the Spartan-7.

For new designs, the Spartan-7 is a clear choice due to higher performance, power efficiency, and improved toolchain (with exceptions requiring other 7 Series parts).