FPGA
  • Technologies
  • More
FPGA
Blog Current Project, with Altera MAX10
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelkellett
  • Date Created: 4 Nov 2017 5:12 PM Date Created
  • Views 668 views
  • Likes 4 likes
  • Comments 2 comments
  • fpga
Related
Recommended

Current Project, with Altera MAX10

michaelkellett
michaelkellett
4 Nov 2017

This is the project I've been working on recently. Just assembled the first prototype. I've only populated 2 of the 8 analogue input sections, some values in filters may change and I don't need to waste expensive parts by building all 8 channels just yet. The signals go into an 8 channel simultaneous sampling 24 bit ADC which will run at about 256k samples per channel per second. The FPGA, an Altera MAX10M16, controls the ADC and does the heavy digital signal processing work. It has a little 128kbyte serial RAM from Microchip for extra buffering and talks to the uP via SPI and some handshake lines.

 

The processor (STM32F407) has an Ethernet interface connected via a Microchip PHY and USB connectivity via  an FTDI USB/serial converter.

 

I can't say what the two blocks of circuit driving the D connectors do.

 

The power supply stuff along the bottom edge is not populated for a sad reason - I checked up on part availability before I did the design but foolishly only tried to order the components once the layout was finished and the board ordered (so as to be as quick as possible). Alas, when I came to order the LT8640 chips that work the power supplies Farnell had sold out and offering delivery of more in December. No one else had any and I couldn't get a delivery date from any one else either. I ordered 25 form Farnell but they told me  a day later that LT had put the delivery date out to September 2018. I was rather expecting this and had already started work on a little PSU board that will piggy back on the main board where the 8640s were meant to be. The moral of all this is that you should secure the critical parts before you lay out the board - I've got too used to parts being readily available.

 

I'll try to find time to blog a bit about the Altera MAX 10s because they seem well suited to small volume applications. This one runs from a single 3.3V supply and has on chip flash so it's a lot easier on support chips than many other devices.

 

image

MK

  • Sign in to reply

Top Comments

  • dougw
    dougw over 8 years ago +2
    Yeah - we also are getting nailed by nasty delivery delays. Between Analog Devices buying Linear Tech and Analog Devices moving a bunch of parts to a new plant and big outfits soaking up and stockpiling…
Parents
  • jc2048
    jc2048 over 8 years ago

    Thanks for the warning about the Linear supply times.

     

    Interesting project you've got on the go there; look forward to the FPGA blogging.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 8 years ago

    Thanks for the warning about the Linear supply times.

     

    Interesting project you've got on the go there; look forward to the FPGA blogging.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data