FPGA
  • Technologies
  • More
FPGA
Blog Entering The World Of FPGA's with a DEO-NANO P0082 - Part 1
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 27 Jul 2017 6:20 PM Date Created
  • Views 5340 views
  • Likes 15 likes
  • Comments 16 comments
  • p0082
  • terasic
  • enterfpga
  • p0082(terasic)
  • deo nano
Related
Recommended

Entering The World Of FPGA's with a DEO-NANO P0082 - Part 1

e14 Contributor
e14 Contributor
27 Jul 2017

image

 

Recently I was selected to roadtest the terasIC DEO-NANO P0082 fpga development kit. My application was based around reviewing the P0082 for suitability as an entry level device to simplify the process of people wanting to explore fpga development for the first time.

 

As part of that roadtest application I offered to post regular blogs here in the fgpa group on element14 documenting my progress, this first post centered around the unboxing and first impressions.

 

 

 

 

 

 

 

 

 

 

 

 

 

 

image

 

The Box Contains:

            - P0082 development board

            - Mini USB cable

            - Quick start guide

            - Brochures for other products

 

I always like getting brochures for other products!!

 

 

 

 

 

 

 

 

 

 

 

 

 

imageimage

 

Quick start guide

 

Page 1 has a picture of the P0082 development board with labels to highlight the specific components.

Page 2 contains a brief introduction and a list of relevant software you will need to install to develope with the P0082.

Page 3 is an overview of the pre-loaded demonstration and links of where to download further demonstrations.

Page 4 looks at a control panel demonstration and a system builder tool to enable quick development on the P0082 (I'd imagine a project setup wizard).

 

imageimageimage

 

The P0082 development board looks well made, comes with a clear acrylic protective top cover and has standoffs to raise the bottom of the board from the surface its stood on which is a nice touch. The main component of the board is an Altera Cyclone 4. From what I understand at the moment, the Altera fpga loses all of it's configuration when power is removed and re-configures itself using an external EEPROM. To the left hand side of the board there is an I2C EEPROM so I'm assuming that this is where your compiled program (is that what you call it?) is downloaded from your computer onto ready for the fpga to read upon next power up.

 

Positive Comments

 

The development kit looks reasonably well presented, the quickstart guide is easy to follow and gives me confidence that the product is a worthy contender as an introductory device to the world of fpga's

 

Negative comments

 

One of the pins for the external power header is slightly bent, this coupled with the box looking rather worn and the software cd's that are supposed to be included are missing leads me to think this is a pre-used kit. Keep in mind though that this product was sent as a roadtest product and not one that has been purchased as new. Luckily the software packages can be downloaded easily enough so the missing cd's aren't a huge problem. Fingers crossed the board does function, I'll find out in due time!!

(edit) *after a quick power-up test, the P0082 is working fine and preloaded with the flashing led demo.

 

 

image

 

* Pictures taken with my new general purpose camera Canon EOS 750D

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 9 years ago in reply to michaelkellett +2
    Thanks! Yes I just found out this morning that the "image" was stored on an EPCS device when I was trying to find the driver to connect it to the computer and came across the technical docs for it!! The…
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to jc2048 +2
    Thanks, theres some great advice there! Yes I have an oscilloscope to check things out with, one of the things I'll probably need advice with is how to get the image data into the fpga.
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to msimon +2
    Hi Mehmet, Yes Ive used the programmer already, what Im talking about here is my eventual project where I intend to take some image data (from a picture) and use the fpga to display that onto an LED matrix…
  • jc2048
    jc2048 over 9 years ago in reply to e14 Contributor

    I'd call it a 'bitstream' too (I've worked with Xilinx FPGAs in the past). 'Image' is ok in my book as well - it describes what is going on much better than the word program.

     

    Bit stream is good because it's a stream of bits being loaded into shift registers on the device. When all the bits are in the correct place, they get latched into place, taking over from the default settings and controlling the various elements of the FPGA (routing connections, etc).

     

    One thing that's useful to remember, if you're designing hardware to go around an FPGA, is that that process takes time [a considerable time, in electronic terms, if you're used to logic that just starts instantly] and until the bits get latched the FPGA will hold the I/O pins in a high impedance state. If you use the FPGA to generate chip selects to external devices, or that kind of thing, you may need to consider carefully what happens before the FPGA gets going to avoid conflicts [usually just a few carefully placed pull-ups or pull-downs will do].

     

    I can remember one design that I did that incorporated registers that an external processor could write to in order to set up various parameters. It didn't work when I tried it with a simple test program to load the registers, even though I could see on a 'scope the right data being written across. After spending a while looking at all the wrong things, in the way that you do sometimes, I thought to look at the signal that showed when the configuration was complete and realised that the processor was pushing the data across a couple of hundred milliseconds before the FPGA was finished with its configuration.

     

    An LED tile is a good project. LED displays lend themselves well to debugging designs - it makes for fast progress being able to see the mistakes in front of your face. Do you have an oscilloscope to look at waveforms?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 9 years ago in reply to DAB

    DAB wrote:

     

    I look forward to seeing your experience with the board.

     

    I am very curious to see how easy the software is to use from a newbie perspective.

    Lucie, I am also interested in your experience as a new FPGA designer.  I've been in this game since the 90s, back when FPGA architectures and software were a whole lot simpler so I was able to climb the learning curve gradually.  My impression is that nowadays a new FPGA user is faced with "The Cliffs of Insanity" when it comes to vendor tools and languages such as VHDL and Verilog.  So I look forward to your comments.

     

    One of the best talks I've ever heard on FPGA's in Duane Benson's Design West / ESC 2013 talk called “FPGAs: I know nothing... yet”.  Duane was highly knowledgeable about microprocessors and microcontrollers when he first tried to learn about FPGAs -- it was, shall we say, "interesting".

     

    Here's an interesting element14 thread on this general topic: Barriers to designing with FPGAs?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to michaelkellett

    Thanks! Yes I just found out this morning that the "image" was stored on an EPCS device when I was trying to find the driver to connect it to the computer and came across the technical docs for it!!

     

    The quick start guide says that the board comes pre-loaded with a bit stream to demonstrate the board but I'll probably stick to calling the result of the compiler an image like you, it sounds right.

     

    I'm gonna spend some time trying to get a basic working knowledge of the board first and then move onto using it to drive a 32x32 rgb led matrix as a first main project. Ive just tested out some of the demo's which install by running a batch file, I supposed its time to have a read of the full user manual and see if I can move forwards from there! image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 9 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

    I don't know what to call the code like thing that FPGAs have so I call it an image so as not to mix it up with programmes for micros.

    Xilinx usually calls it a "bitstream", which is the terminology I generally use, e.g., Taming the Wild Bitstream.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago

    You haven't got it quite right re. the boot up process:

     

    Your board has  a small (2k) I2C EEPROM but this is far too tiny to store the boot up image for the FPGA - it has as an ECPS64 8Mbyte Flash chip for that. You are right that this FPGA (like many others) is RAM based so needs to copy the image from somewhere non volatile on power up. I don't know what to call the code like thing that FPGAs have so I call it an image so as not to mix it up with programmes for micros.

     

    I try not to talk about writing software for FPGAs  - after all VHDL and Verilog are both officially hardware description languages but it does sound a bit pompous to say I spent my morning describing hardware !

     

    Do you have a project in mind for the Nano ?

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>